7.4.2. List of createProject Options

Note that the available options can vary depending on the Code Composer Studio™ version used. For the list of options available for your specific Code Composer Studio version, run the command with the '-ccs.help' option:

ccs-server-cli -noSplash -workspace "<workspace_dir>" -application com.ti.ccs.apps.createProject -ccs.help

Full List of createProject Options:

-ccs.projectSpec '<file>'
        The project-spec defining the project(s) to be created.
        See the <ccs-install-root>/ccs/eclipse/plugins/com.ti.ccs.project.templates/schema/projectSpec.xsd file for details.

-ccs.name <name>
        The name of the new project.

-ccs.location '<dir>'
        The filesystem location of the project, if it is
        to be created outside of workspace (optional).

-ccs.outputType (executable | staticLibrary)
        The output-type (optional).
        Defaults to 'executable'.

-ccs.device <id>
        The device-variant ID.
        A list of all available device-variant IDs will be
        printed if this argument is missing or not recognized.

-ccs.endianness <name>
        The device endianness (optional).
        Defaults to device-specific setting, if defined.
        A list of all applicable endianness types will be
        printed if this argument is not recognized.

-ccs.toolChain (TI | TICLANG | GNU)
        Compiler tool-chain (optional).
        Defaults to 'TI'.

-ccs.toolVersion <version>
        Compiler version (optional).
        Defaults to highest applicable version.

-ccs.outputFormat (COFF | ELF)
        The output-format (optional).
        Defaults to device-specific setting, if defined, or 'COFF'.

-ccs.products '[<id>[:<version>];]+'
        List of products to enable (optional).

-ccs.cmd '<file>'
        Linker command file to be physically copied into the project (optional).
        Defaults to device-specific setting, if defined.

-ccs.rts '<file>'
        Runtime support library (optional).
        Defaults to device-specific setting, if defined.

-ccs.configurations [<name> ]+
        Space-separated list of build-configurations to create (optional).
        Defaults to 'Debug Release'.

-ccs.defaultConfiguration <name>
        Name of one build-configuration which would be made active each time this project is imported into workspace.

-ccs.references [<name> ]+
        Space-separated list of project-references to add to created project (optional).

-ccs.artifactName <name>
        Name of the build-artifact (optional).
        Defaults to the name of the project.

-ccs.artifactExtension <ext>
        Extension of the build-artifact (optional).
        Defaults to 'out' or 'lib', depending on '-ccs.outputType'.

-ccs.listBuildOptions
        Prints a list of all applicable build-options (optional).
        Does not actually create the project.

-ccs.setCompilerOptions '<options>' [@prepend] [@files ['<path>' ]+] [@folders ['<path>' ]+] [@configurations [<name> ]+]
        Space-separated list of build-options to set on the created project's compiler tool (optional)
        (use backslash '\' to escape all double-quotes in <options>).
        Optionally, force the value for any list-type options to be prepended to current value.
        Optionally, specify lists of files/folders (project-relative paths) to set these options on.
        Optionally, specify a list of build-configurations in which these options are to be set.

-ccs.setLinkerOptions '<options>' [@prepend] [@configurations [<name> ]+]
        Similar to -ccs.setCompilerOptions

-ccs.setHexOptions '<options>' [@prepend] [@configurations [<name> ]+]
        Similar to -ccs.setCompilerOptions. Hex tool needs to be separately enabled using -ccs.enableHexTool.

-ccs.setObjcopyOptions '<options>' [@prepend] [@configurations [<name> ]+]
        Similar to -ccs.setCompilerOptions. Objcopy tool needs to be separately enabled using -ccs.enableObjcopyTool.

-ccs.setSysConfigOptions '<options>' [@prepend] [@configurations [<name> ]+]
        Similar to -ccs.setCompilerOptions. SysConfig tool needs to be separately enabled using -ccs.enableSysConfigTool.

-ccs.enableHexTool
        Enable the Hex tool with its default build-options (optional).
        Defaults to 'false'.

-ccs.enableObjcopyTool
        Enable the Objcopy tool with its default build-options (optional).
        Defaults to 'false'.

-ccs.enableSysConfigTool
        Enable the SysConfig tool with its default build-options (optional).
        Defaults to 'false'.

-ccs.setPreBuildStep '<command>' [@configurations [<name> ]+]
        Command to be used as a pre-build step (optional)
        (use backslash '\' to escape all double-quotes in <command>).
        Optionally, specify a list of build-configurations in which this build-step is to be set.

-ccs.setPostBuildStep '<command>' [@configurations [<name> ]+]
        Command to be used as a post-build step (optional)
        (use backslash '\' to escape all double-quotes in <command>).
        Optionally, specify a list of build-configurations in which this build-step is to be set.

-ccs.copyFile '<file>' [@dir '<dir>'] [@configurations [<name> ]+]
        Copies the given file/directory into the project upon creation (optional).
        Optionally, specify a project-relative directory as the file's destination.
        Optionally, specify a list of build-configurations in which this file is to be used.

-ccs.linkFile '<file>' [@dir '<dir>' [@virtual]] [@configurations [<name> ]+]
        Links the given file/directory into the project upon creation (optional).
        Optionally, specify a project-relative directory as the file's destination.
        Optionally, specify whether the destination directory should be created as virtual.
        Optionally, specify a list of build-configurations in which this file is to be used.

-ccs.definePathVariable <name> <value> [@scope (global|project)]
        Defines the given path-variable for resolving portable linked file paths (optional)
        (also defines a global build-macro with the same name and value).
        Optionally, specify the scope (defaults to 'global').

-ccs.defineBuildVariable <name> <value> [@type (string|dir|file)] [@scope (global|project|configuration)] [@configurations [<name> ]+]
        Defines the given build-variable (optional).
        Optionally, specify the type (defaults to 'string').
        Optionally, specify the scope (defaults to 'global').
        Optionally, specify a list of build-configurations in which this build-variable is to be defined
        (applies only when scope is 'configuration').

-ccs.autoGenerateMakefiles (true|false)
        Turns automatic makefile-generation on/off (optional).
        Defaults to 'true'.

-ccs.buildLocation '<path>'
        Absolute or project-relative path to folder to be used as the build-directory (optional).
        Applies only when the '-ccs.autoGenerateMakefiles' flag is set to 'false'.
        Defaults to project root-directory.

-ccs.buildCommand '<path>'
        Absolute path to an alternative build utility (optional).
        Defaults to the gmake utility that is shipped with CCS.

-ccs.buildCommandFlags '<flags>'
        List of flags to override the default build-command flags (optional).

-ccs.buildTarget <name>
        Name of the target to run during an incremental build (optional).
        Defaults to 'all'.

-ccs.cleanTarget <name>
        Name of the target to run during a clean build (optional).
        Defaults to 'clean'.

-ccs.template <id>
        ID of the project-template to use when generating the new project (optional).
        A list of all applicable template IDs will be
        printed if this argument is not recognized.

-ccs.ignoreDefaultDeviceSettings
        Iff 'true' ignores any default settings specified by the selected device.

-ccs.ignoreDefaultCCSSettings
        Iff 'true' ignores any non-essential default settings made by CCS.

-ccs.overwrite (full | keep)
        Forces overwrite of existing file-system resources (optional).
        A 'full' overwrite would delete and recreate the entire existing project folder.
        A 'keep' overwrite would keep all existing filesystem project contents
        (applies only when workspace project does not exist).

-ccs.autoBuild
        Performs an incremental build on the imported/created project (optional).

-ccs.kind <id>
        The project kind ID (optional).
        [Deprecated] - use -ccs.outputType

-ccs.listBuildOptionIDs
        Prints a list of all applicable build-option IDs (optional).
        Does not actually create the project.
        [Deprecated] - use -ccs.listBuildOptions

-ccs.setBuildOption <id> '<value>' [@prepend] [@configurations [<name> ]+]
        Sets the given build-option on the created project (optional).
        (use the wildcard '*' to match multiple characters in <id> and enum <value>'s).
        Optionally, force the value for any list-type options to be prepended to current value.
        Optionally, specify a list of build-configurations in which this option is to be set.
        [Deprecated] - use -ccs.setCompilerOptions/-ccs.setLinkerOptions

-ccs.defaultImportDestination '<dir>'
        Default import-destination. This is the workspace where user-projects will be created/imported by default.

-ccs.args '<file>'
        File containing any extra arguments (optional).

-ccs.help
        Print this help message.

DSP/BIOSv5.x support:
                -bios.version <version>
                        DSP/BIOSv5.x tools version.

RTSC support:
                -rtsc.enableRtsc
                        Enable RTSC support.

                -rtsc.xdcVersion <version>
                        XDCtools version (optional).
                        Defaults to highest available version, when '-rtsc.enableRtsc' is specified.

                -rtsc.target <id>
                        RTSC target (optional).
                        Will be auto-set by default.

                -rtsc.platform <id>
                        RTSC platform (optional).
                        Will be left blank by default.

                -rtsc.buildProfile <profile>
                        RTSC build-profile (optional).
                        Defaults to 'whole_program'.

                -rtsc.products '[<id>[:<version>];]+'
                        List of RTSC products to enable (optional). [Deprecated] - use the '-ccs.products' flag instead.

                -rtsc.setConfiguroOptions '<options>'
                        Space-separated list of options to set on the created project's Configuro tool (optional)
                        (use backslash '\' to escape quotes in <options>).

                -rtsc.configurationOnly
                        Generate a reusable RTSC Configuration project (optional).