7.9.8.83. GEL_SrcStepInto()ΒΆ

Steps into source code.

Syntax

GEL_SrcStepInto()

Parameters

count(optional) specifies the number of times the command is to be repeated. If no count is specified, executes a single assembly instruction.

Description

Executes the next available instruction in C or assembly source code then halts. If an action enters an area with no source code, the debugger continues stepping until source code (somewhere) is reached. Repeats count times.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Related Topics

GEL_AsmStepInto

GEL_AsmStepOver

GEL_SrcStepOver