7.9.8.73. GEL_Run()ΒΆ
Runs code.
Syntax
GEL_Run( ["Condition"] );
Parameters
Condition: (optional) specifies the condition that must be satisfied while the target is executing. Once the execution reaches a breakpoint and the condition is evaluated to be false, the Code Composer Studio debugger stops at that address. The condition must be enclosed in quotation marks.
Description
This function starts executing code on the target. If a condition is specified, the run function becomes a conditional run statement. That is, execution continues while the statement is true. The statement is evaluated at each breakpoint that is encountered.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_Run();
GEL_Run("A != B");
Related Topics