7.9.8.111. OnResetDetected()ΒΆ
GEL callback that occurs when a reset is detected in the system.
Syntax
OnResetDetected();
Parameters
None
Description
This callback is called whenever a reset is detected in the system other than the default reset (typically called Reset CPU). More specifically, it is called once a reset is detected and the target later halts. The reset occurs when the target executing code performs a reset, or when invoked from the advanced reset menu or GEL function.
The difference between OnReset() and OnResetDetected() is that OnReset() is only triggered when Reset CPU has been selected, while OnResetDetected() is triggered when any type of reset occurs. Thus, OnResetDetected() is a super function of OnReset().
Related Topics