7.9.2.1. Legacy unsupported functions¶
The following GEL Built-In functions are not supported. The GEL will recognize these functions, however, no operation will be performed when they are called.
GEL_CloseWindow GEL_Exit GEL_OpenMemoryWindow GEL_OpenWindow GEL_ProjectAddSubProj GEL_ProjectBuild GEL_ProjectBuildConfi g GEL_ProjectClose GEL_ProjectCreateCopy Config |
GEL_ProjectCreateDefa ultConfig GEL_ProjectLoad GEL_ProjectRebuildAll GEL_ProjectRebuildAll Config GEL_ProjectRemoveConf ig GEL_ProjectRemoveSubP roj GEL_ProjectSave GEL_ProjectSetActive GEL_ProjectSetActiveC onfig |
GEL_ProjectSetSubProj ConfigSel GEL_SrcDirAdd GEL_SrcDirRemoveAll GEL_StopTransferToFil e GEL_TransferToFile GEL_TransferToFileCon fg GEL_WatchAdd GEL_WatchDel GEL_WatchReset |
The following GEL Built-In functions are only supported in the Windows platform.