<!-- Start of markdown source --> ## Overview The TI Cloud Agent is a small application that is required for flashing and debugging hardware devices from Texas Instruments tools. This application is used by both cloud and desktop tools to manage the communication between the host computer and the TI hardware devices. Despite the name, it is not a cloud-based application and runs locally on the user's machine. [[b NOTE - CLOUD BASED TOOLS A browser extension, called the **TI Cloud Agent Bridge**, must also be installed separately to enable the browser to communicate with the main application. ]] ## Requirements ### OS * Please see [System Requirements](https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs/ccs_overview.html#operating-system) ### Permissions The user account which will use TI Cloud Agent must have the ability to install the TI Cloud Agent with the required elevated (administrator) privileges. ## Troubleshooting ### TI Cloud Agent Installation [[b NOTE - DESKTOP TOOLS Desktop tools such as Code Composer Studio IDE (offline desktop version) and UniFlash (offline desktop versions) come with their own version of TI Cloud Agent which is installed as part of the main installer. Hence no additial steps are required to install TI Cloud Agent when using these tools. ]] Please ensure you have followed all the instructions on the **TI Cloud Agent Installation** dialog. You should only have to perform each step once. ![](./images/TICloudAgentInstallation.png) If you are still having issues please check the following: * Verify your browser version is supported and up to date * **Chrome**: Click on Chrome menu icon (the three dots next to your profile picture) in the top right and select **Settings** then **Extensions**. Find **TICloudAgent Bridge** and ensure **Enabled** is checked. Do not use incognito mode, or select **Allow in incognito** in the same location as above. * **Firefox**: Click on the menu icon in the top right and select **Add-ons** and then the **Extensions** tab. Find **TICloudAgent Bridge** and click on **Enable** if present. Do not use private browsing. Open **about:config** in a new tab. Select **I'll be careful**. Type **browser.privatebrowsing.autostart** in the search box, and disable the option if enabled. * Make sure Windows short filename generation is enabled On Windows systems, short filename generation must be enabled during the installation. Otherwise an error like the below will occur: ![](./images/ticloudagent_shortfilename.jpg) You can check by running the following command from from a command window: ```dos fsutil 8dot3name query ``` Here are a couple of Microsoft articles on the subject for reference: [here](https://support.microsoft.com/en-us/help/121007/how-to-disable-8-3-file-name-creation-on-ntfs-partitions) and <a href="https://docs.microsoft.com/en-us/previous-versions/windows/it-pro/windows-server-2012-R2-and-2012/ff621566(v=ws.11)">here</a>. If disabled: re-enable it (at least temporarily), delete the <tt>C:\Users\\[userId]\TICloudAgent</tt> and the <tt>C:\Users\[userId]\AppData\Local\Texas Instruments</tt> folders, and retry the installation. ### Overriding TI Cloud Agent Proxy Settings Cloud agent attempts to automatically detect and configure the local proxy settings. If automatic detection fails, it may be necessary to manually override the proxy settings. This can be done by opening the <tt>[Home]\TICloudAgent\util\proxy.js</tt> file and setting **exports.proxy** to your local proxy. For example: ```js exports.proxy = "http://user:password@example_host.com:80"; ``` ### Linux Library Dependencies When the TI Cloud Agent installer starts, it will check for the presence of the required system libraries. Please ensure these libraries are present before proceeding. [[y NOTE Only 64-bit Linux distributions are supported by TI Cloud Agent. ]] A common issue is a missing dependency on **libudev.so.0**. This library may not be available on some Linux distributions. A workaround for Cloud Agent is to symlink **libudev.so.0** to **libudev.so.1**. The process of installing dependencies for the desktop Code Composer Studio installs is also relevant. For more information refer to [here](https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs/ccs_installation.html#system-check). ### TI Cloud Agent Startup The below error can occur if you the user account trying to use TI Cloud Agent wasn't the account used to install it on the PC. <tt> Could not launch TI Cloud Agent: Failed to start TICloudAgent: Specified native messaging host not found.. Please perform the actions listed below and try your operation again. </tt> <pre> </pre> A common scenario when this occurs is that the TI Cloud Agent was installed on a PC using a separate administrator account since the standard user accounts on the PC do not have the ability to run the installer with the required elevated (administrator) privileges. However, TI Cloud Agent is a per user install. Hence, the user account will not see the install from the local administrator account. One workaround (on Windows) is to edit the Windows registry and add an entry for the user to see the administrator install. That would require duplicating <tt>HKEY_CURRENT_USER\Software\Google\Chrome\NativeMessagingHosts\com.ti.cloudagent</tt> from the local administrator account. ## Support Please submit TI Cloud Agent logs when reporting issues on the [E2E Forums](https://e2e.ti.com/). ### Logging #### Linux and MacOS Edit the <tt>~/TICloudAgent/ticloudagent.sh</tt> script, and uncomment lines 4-6. Restart your browser and reproduce the problem. The log will be located at <tt>/tmp/my_ticld.log</tt>. [[y NOTE - DESKTOP TOOLS For issues with TI Cloud Agent when using CCS IDE desktop, use the following *.sh file instead: <tt>[CCS INSTALL DIR]/ccs/ccs_base/cloudagent/ticloudagent.sh</tt>. Then restart CCS. ]] #### Windows Edit the <tt>C:\Users\\[your ID]\TICloudAgent\ticloudagent.bat</tt> script, and uncomment lines 4-6. Restart your browser and reproduce the problem. The log will be located at <tt>C:\temp\my_ticld.log</tt>. [[y NOTE - DESKTOP TOOLS For issues with TI Cloud Agent when using CCS IDE desktop, modify the following *.bat file instead: <tt>[CCS INSTALL DIR]\ccs\ccs_base\cloudagent\ticloudagent.bat</tt>. Then restart CCS. ]] <!-- End of markdown source --> <div id="footer"></div>