The GEL expression to evaluate
The value resulting from the evaluation of the expression, if numerical or a string.
Will throw if the evaluation of the expression fails.
// Adds 8 to the address of the main symbol, returns a BigInt
let result = session.expressions.evaluate("main + 8");
// Returns a (floating point) number
let result = session.expressions.evaluate("1.0 / 2");
// Call a GEL function (assuming that this function is defined in a loaded GEL script)
session.expressions.evaluate('userDefinedGelFunction()');
Evaluates a GEL expression and returns the resulting value, if numerical or a string. All standard rules for GEL expressions apply. If the result of evaluating the expression is an integral value, a BigInt will be returned. If the value is a floating point value, a standard Javascript number will be returned. For any other value, like a reference to a c++ object, we return without a value.