Either an expression that evaluates to the location or a source file. The source file can be specified as the full path to the file at compilation time, or as just the file name. In the latter case, the breakpoint will be set in the first source file with a matching name.
Optionalline: numberThe line number. If provided, the first argument must be a source file.
An index identifying the breakpoint created
Will throw if breakpoint location cannot be resolved.
// Adds a breakpoint at 0x2400
let id = session.breakpoints.add(0x2400n);
// Adds a breakpoint at symbol 'main'
let id = session.breakpoints.add("main");
// Adds a breakpoint at an offset from symbol 'main'
let id = session.breakpoints.add("main + 0x8");
// Adds a breakpoint at line 24 of main.c
let id = session.breakpoints.add("C:/my_project/source/main.c", 24);
// or if we know there is only one main.c
let id = session.breakpoints.add("main.c", 24);
Add a breakpoint based on properties that have been set in advance. A set of breakpoint properties can be created using createProperties
The index identifying the set of breakpoint properties
An index identifying the breakpoint created
Creates a new set of breakpoint properties. A breakpoint can later be created from this set of properties using addWithProperties. Only one breakpoint can be added with each set of properties. Properties must be configured before calling addWithProperties.
Optionaltype: numberThe type of breakpoint to create properties for. 0 for a software breakpoint, 1 for a hardware breakpoint (if supported). Defaults to a software breakpoint.
An index identifying the set of properties
Get a detailed list of all breakpoint properties currently available in the specified set of properties. Configuring some properties can cause other properties to become available or become unavailable.
The index identifying the set of breakpoint properties. This index is obtained from createProperties.
A list of objects which detail each breakpoint property
let id = session.breakpoints.createProperties();
let properties = session.breakpoints.getDetailedProperties(id);
// print details of properties
for (const prop of properties) {
console.log(`${prop.id}:`);
console.log(` type: ${prop.type}`);
console.log(` description: ${prop.description}`);
console.log(` value: ${prop.value}`);
if (prop.allowedValues) {
console.log(` allowedValues: ${JSON.stringify(prop.allowedValues)}`);
}
if (prop.allowedRange) {
console.log(` allowedRange: [${prop.allowedRange.min}, ${prop.allowedRange.max}]`);
}
console.log("");
}
Get the value of a specific breakpoint property
The index identifying the set of breakpoint properties. This index is obtained from createProperties.
The identifier for the desired property
The value of the property
Will throw if the property does not exist
// Get the value of the Skip Count property. This is an integral value
let skipCount = session.breakpoints.getProperty(id, "Debugger Response.Skip Count");
// Get the breakpoint's location
let location = session.breakpoints.getProperty(id, "Hardware Configuration.Location");
// location might be an integral value (e.g. 0x1000n)
// it might also be a string if the location is a symbolic expression (e.g. "main + 0x8") or
// a source-based location (e.g. "C:/my_project/Debug/my_project.out@C:/my_project/main.c, line 12")
Set the value of a specific breakpoint property. You can only configure properties before they are used to add a breakpoint.
The index identifying the set of breakpoint properties. This index is obtained from createProperties.
The identifier for the desired property
The new value of the property
Will throw if the property does not exist, the provided value cannot be set on the property, or if a breakpoint has already been added with this set of properties.
// Set the Skip Count property to 5
session.breakpoints.setProperty(id, "Debugger Response.Skip Count", 5);
// Set the location to a symbolic expression
session.breakpoints.setProperty(id, "Hardware Configuration.Location", "main + 0x8");
Set the value of a location property to a source file and line number
The index identifying the set of breakpoint properties. This index is obtained from createProperties.
Like for add this can be either the full path to the file at compilation time, or as just the file name. In the latter case, the breakpoint will be set in the first source file with a matching name.
The line number
Will throw if the property does not exist, is not a location property, or if a breakpoint has already been added with this set of properties.
// Set the location property to line 24 of our project's main.c file
session.breakpoints.setPropertySourceLocation(id, "Hardware Configuration.Location", "C:/my_project/source/main.c", 24);
// or if we know there is only one main.c
session.breakpoints.setPropertySourceLocation(id, "Hardware Configuration.Location", "main.c", 24);
Adds a breakpoint at the specified location. The location can be an address, a symbolic expression, or a source file and line number