Overview
---
JavaScript is the default scripting language supported by [DSS](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html). But because DSS is implemented as a set of Java APIs, it works quite nicely out of the box with Java. While the provided DSS examples are mostly for JavaScript, the DSS Java API documentation shows examples of API calls with Java code.
Prerequisites
---
At a minimum, a Java compiler (javac) and a Java Runtime Environment (JRE) are needed to build and run the DSS Java application. While CCS comes with a JRE, it does not come with a JDK (which provides a Java compiler). A JDK can be downloaded from the [Sun Java SE download site](https://java.sun.com/javase/downloads/index.jsp). If a Java IDE (such as [Eclipse](https://www.eclipse.org/)) is being used to develop the DSS Java application, then a Java compiler is already available.
[[b Note:
You must ensure that your JDK is compatible with the version of CCS you have installed. Consult the table below to determine if you need a 32-bit or 64-bit JDK. A compatible JDK or JRE will also be required to run compiled programs.
| OS |
Requires 32-bit JDK |
Requires 64-bit JDK |
| Windows |
Up to CCS v8.x |
CCS v9 and above |
| MacOS |
None |
All |
| Linux |
Up to CCS v6.1.3 |
CCS v6.2.0 and above |
]]
Creating and Running a DSS Java Program
---
Create a new Java source file in an editor. If a Java IDE is being used, create a new Java project and add your new Java source file to the project. Refer to the [documentation](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html#dss-api) for the available APIs.
### Example source
The following example code snippets are from a straight port of the 'Breakpoints.js' example which is [included with DSS](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html#examples).
First, you must import the all necessary DSS packages.
```java
// Import all DSS packages for the Debug Server
import com.ti.ccstudio.scripting.environment.*;
import com.ti.debug.engine.scripting.*;
```
The first action done by the `main()` method is to create a scripting instance:
```java
...
public class DssBreakpointsExample {
public static void main(String[] args)
{
// Create our scripting environment object - which is the main entry point into any script and
// the factory for creating other Scriptable servers and Sessions
ScriptingEnvironment scriptEnv = ScriptingEnvironment.instance();
...
```
Next, the debug server instance is created and a debug session is started. The calls are wrapped in a 'try-catch' block since most DSS APIs can throw exceptions.
```java
...
DebugServer debugServer = null;
DebugSession debugSession = null;
try {
// Get the Debug Server and start a Debug Session
debugServer = (DebugServer) env.getServer("DebugServer.1");
debugServer.setConfig("../msp430f5529/msp430f5529.ccxml");
debugSession = debugServer.openSession(".*");
} catch (ScriptingException e) {
scriptEnv.traceWrite("ERROR");
e.printStackTrace();
}
...
```
Finally, let's look at a snippet in which a breakpoint is set and the program is run.
```java
...
try {
rnd = debugSession.symbol.getAddress("ReadNextData");
rndBP = debugSession.breakpoint.add(rnd);
// Run the program until execution is halted (should hit the breakpoint)
debugSession.target.run();
...
```
To see what the rest of the functionality of the example is, refer to the Breakpoints.js JavaScript example that ships with DSS. As an exercise, try to do a complete port of it yourself! The file should be saved as DssBreakpointsExample.java.
### Compiling the Source Code
To build your code using the Java compiler, the dss.jar file must be in the classpath. You can do this either by placing it in your `CLASSPATH` environment variable, or by using the **-classpath** (or **-cp**) option. The JAR file can be found in the following location:
<CCS_DIR>/ccs_base/DebugServer/packages/ti/dss/java/dss.jar
where <CCS_DIR> is the location of the CCS installation on your machine (for CCS 8 on Windows it might be C:/ti/ccsv8/).
For example, the following command will build the DssBreakpointsExample.java from the command line (using CCS 8 on Windows)
```diff
javac -cp "C:/ti/ccsv8/ccs_base/DebugServer/ti/dss/java/dss.jar" DssBreakpointsExample.java
```
This will generate the DssBreakpointsExample.class file. Note that the example above assumes that the bin subfolder of the JDK installation is in the system `PATH`, so that `javac` can be called from anywhere.
### Running the Program
Once the class file has been generated, the application can be run. Before running, you must ensure that the dss.jar is in the classpath. As when compiling, you can either add it to your `CLASSPATH` environment variable or use the **-classpath** (or **-cp**) option. For example, to run the 'DssBreakpointsExample' compiled above, (with CCS 8 on Windows):
```diff
java -cp ".;C:/ti/ccsv8/ccs_base/DebugServer/ti/dss/java/dss.jar" DssBreakpointsExample
```
Make sure the instance of Java running your program is from a JDK or JRE that is compatible with your version of CCS.
### Creating a JAR file from Eclipse
{{b This section assumes you are using [standard Eclipse](https://www.eclipse.org/). }}
In your project's properties, add the dss.jar file to the build path. This is also a good time to check that your project is using the correct JDK.
To export your project as a JAR file, the dependent JAR files must be referenced from their original location. For this reason, Eclipse's option to export as a 'Runable Jar File' will not work. Instead you should choose to export as a 'JAR file' and provide your own MANIFEST.MF file. A basic manifest file for our `DssBreakpointsExample` project might look like this (the location of your CCS installation might differ):
```diff
Manifest-Version: 1.0
Class-Path: . file:///C:/ti/ccsv8/ccs_base/DebugServer/packages/ti/dss/java/dss.jar
Main-Class: DssBreakpointsExample
```
When exporting as a JAR file, choose the option to **use existing manifest from workspace** and select your manifest file.

Now you should be able to run your JAR file:
```diff
java -jar DssBreakpointsExample.jar
```