#Overview
When working in a team environment, there may be cases where the desired version of Simplelink SDK is in a Git repository that each user checks out as needed.
This document describes how to set up CCS to use a SimpleLink SDK that is in a local Git repository.
#Location and Discovery
In this environment, the assumption is that the Simplelink SDK is available in the user's local Git repository.
In order for CCS to use a specific version of SDK during project build, it needs to first discover that version as an installed product.
CCS determines the list of installed products by searching the **Product discovery path**. To see which versions of products are installed go to menu **Window → Preferences → Code Composer Studio → Products**. The paths searched by default are added to the **Product discovery path** (highlighted in yellow) and the products installed to those paths are listed under **Installed products**.

In a typical use-case, SDKs are installed from [Resource Explorer](ccs_resource_explorer.html) (either desktop or online) into the default location (c:\ti). In this case they will be automatically discovered by CCS.
However, if the SDK is in a directory that CCS does not automatically search, as is likely the case for a local Git repository, the directory needs to be added to the **Product discovery path**.
To add the location of the SDK to the list of discovery paths:
- Go to menu **Window → Preferences → Code Composer Studio → Products**.
- Click the **Add** button next to **Product discovery path** and browse to the Git directory where the SDK is located.
For example, if the SDK is in Git directory C:\git\sdk\simplelink_cc13x2_sdk_1_60_00_29, you can browse all the way down to that sub-directory if you need just that version to be discovered, or you can browse to C:\git\sdk if there are multiple versions within that directory. In this example there are two versions of SDK in the C:\git\sdk directory.

Once the new path has been added, CCS will rescan the discovery paths and refresh the **Product discovery path** dialog. If there are multiple versions of SDK located in that directory, they will all be discovered and will appear in the list of **Installed products**. In this example both versions of SDK are discovered.

## Same version in different locations
If you previously had a version of SDK installed to one of the default paths, say C:\ti, then the same version will not be discovered again from the Git directory.
For example, if SDK version 1.60.0.29 is already discovered from C:\ti, then after adding the path to C:\git\sdk (which contains both 1.60.0.29 and 2.10.0.48) only 2.10.0.48 is picked up from C:\git\sdk.

In this case, you would need to remove the previously discovered version. To do this, uncheck the discovery path for that product (C:\ti). CCS will rescan the discovery paths and refresh the **Installed products** list to pick up the SDK from the Git directory.

#Selection
Any product that is installed into CCS can be selected as the version to use when building a project.
To change the version of SDK used for the build:
- Right-click on the project in **Project Explorer** view and select **Properties**.
- Click on **General** in left pane.
- Go to **Products** tab.
- Select the desired version of SDK from the list of versions provided.
The version selected here will be used during project build.
Note that if the project is an application project that is dependent on a separate kernel project, the SDK version will need to be modified in the kernel project as shown below.

Now when you Rebuild the project it will use the selected version of SDK from the Git directory.
This [article](../training/quicktips/ccsv7_update_simplelink_sdk.html) describes in bit more detail the process of changing the version of SimpleLink SDK for both single project and separate kernel project scenarios.