Release Notes — CCStudio™ IDE v21.1.0

Service release

General Information

These release notes contain important information about CCStudio™ IDE v21.1.0 that may not be included in other product documentation. Please review this document before using this release.

CCStudio IDE v21.1.0 is a service release. For a summary of changes, see the v21.1.0 What’s New section below.

System Requirements

ⓘ Note

CCStudio IDE is a 64-bit application and will not run on 32-bit operating systems.

Windows
  • Windows 11 64-bit
  • Windows 10 64-bit
Linux
  • Ubuntu 26.04 64-bit
  • Ubuntu 24.04 64-bit
  • Ubuntu 22.04 64-bit
macOS
  • macOS 14 Sonoma
  • macOS 15 Sequoia
  • macOS 26 Tahoe
ⓘ Note

For more details on platform-specific requirements and installation instructions, refer to the CCStudio IDE User’s Guide.

CCStudio IDE v21.1.0 — What’s New

New Features
Issue Summary
EXT_EP-13395 Watch view: Add an option to remove expressions when importing expressions from .json

Some suggestions: Support a command in the .json file which will clear the existing expressions when the .json file is imported. Similar to expRemoveAll() command supported on CCS eclipse. Add a checkbox to the import menu which allows expressions to be cleared.  The latter option will allow the user the most control.

EXT_EP-13494 Memory allocation view does not auto-update when manually loaded xml/map file changes
EXT_EP-13514 Support expression values when exporting/importing for arrays and structs

The Watch view has the option to import/export expression names from/to a JSON text file. This request is to also support expression values. Allow the user the option to include the values on export. Also allow the user to choose if they wish to import the names and also write the associated values stored in the JSON file. If there are no values in the JSON file then only the names will be imported.

Bug Fixes
Issue Summary
EXT_EP-13651 Arm GCC 9.2.1 AArch64 package is bad on Linux

The Arm GCC 9.2.1 AArch64 package for Linux is broken. Compiling works but linking does not. This is because there is an issue with a soft link.

Previous Releases

Full release notes for earlier versions are available as individual documents. Each page includes a complete What’s New summary, known issues, and a link to the bug-fix tracker for that release.

📄 View previous release notes
Version Type Highlights Release Notes
v21.0.1 Feature Service release, includes Mac ARM support View notes
v21.0.0 Feature Improvements to our AI integrations; New System project graphic editor; python scripting support View notes
v20.5.1 Feature Fixes to AI Integration features released in CCS v20.5.0 View notes
v20.5.0 Feature AI Integration features: getting started UI, MCP servers, graph improvements for FFT, build performance improvements, scripting improvements View notes
v20.4.1 Service Debugger fixes for M33 breakpoints, daisy-chain hardware breakpoints, and full verification mismatch View notes
v20.4.0 Feature Theia IDE core v1.64.1; improved project wizard; macOS 26 support; IDE & debug enhancements; Energia support removed View notes
v20.3.1 Service Secure Debug Manager fix (Windows); MSPM33 macOS flash loader; Arm Clang v4.0.4.LTS; J-Link v8.7.0; device support updates View notes
v20.3.0 Feature Graph view; Python scripting; ARM Advanced Features; new device support (CC35xx, MSPM33, UCD3138R); SysConfig v1.25; C6000 compiler v8.5.0.LTS View notes
v20.2.0 Feature Theia IDE core v1.58; AI/code assistant support; debug view improvements; assembly syntax highlighting; JRE v21; SysConfig v1.24 View notes
v20.1.1 Service Watch/Variable view enhancements; clangd support improvements; CC13x4 program load fix; Windows IDE update fix View notes
v20.1.0 Feature IDE feature improvements; macOS Arm native startup; XDS110 firmware fixes; device support updates (AM62L, xWRL68xx, MSPM0C110x); TI ARM Clang v4.0.2 View notes
v20.0.0 Feature First full-featured release based on Theia IDE; replaces the Eclipse-based v12.x release; new views (Modules, Stack Usage, Memory Map, GEL); broad device family coverage View notes

All Open Issues

The following JIRA query returns all open issues across the CCStudio IDE product areas, including Theia IDE, debug and trace, Resource Explorer, and SysConfig:

Components

For details on all components included in this release, please review the manifest: