Release Notes for Code Composer Studio™ v20.2.0
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™.The release notes are divided into five sections:
Contents
CCS v20 is TI’s next generation Integrated Development Environment (IDE) based on Theia IDE framework. CCS v20.2.0 uses a modified version of Theia-IDE. (https://theia-ide.org/)
For additional information and support, please go to:
https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs_20.2.0/index.html
Please note that Code Composer Studio is a 64bit application and thus will not run on 32bit operating systems.
Supported distributions include:
Code Composer Studio will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Versions Supported
Each Code Composer Studio release is validated against a set of macOS releases. This release was validated with:
MacOS Debug Probe Support
MacOS does not include support for XDS560v2.
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCS_20.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio:1. Run ccs_setup_20.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The offline installer is now distributed as disk images (.dmg files)
1. Right-click on CCS_20.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio:1. Run ccs_setup_20.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_linux_host_support.html
before installing CCS on Linux. It contains important information on
installing CCS on different Linux distributions, including CCS dependencies that may need to be installed first.
Before installing CCS, the tarball file in which the CCS Installer is distributed must first be extracted:untar CCS_20.x.x.xxxxx_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCS_20.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS as root. However, it is preferred that you first install CCS as a normal user and then install the drivers as root.
To install Code Composer Studio as a normal user and emulation drivers as root:1. Run ccs_setup_1.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio as root:
1. Run ccs_setup_1.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
· Click to view the list of bug fixes for this release: Link
· v20.1.1 is a maintenance release based on v20.1.0, with the following updates:
· Click to view the list of bug fixes for this release: Link
· IDE features improvements (Projects, Memory View, Watch View, Breakpoints)
· Startup improvement on macOS version with Arm® processors
o Note: the Theia IDE component is now compiled for Arm® processors for performance improvements (x86 IDE package is still included to support Intel based Macs). But the backend components are still x86 based, so Rosetta is still required.
· Various bug fixes and improvements to the XDS110 firmware
· Device Support Updates
o added AM62L support
o added xWRL68xx support
o added MSPM0C110x support
o various improvements to LPCS flash library
o various improvements and bug fixes for F28 and F29 devices
· Compiler Updates
o TI ARM Clang v4.0.2 (more info: https://www.ti.com/tool/download/ARM-CGT-CLANG)
· SysConfig v1.23 supporting the latest devices, features improvements, bug fixes (more info: https://www.ti.com/tool/download/SYSCONFIG)
· Updated to latest J-Link support package (v8.12.4)
· Various enhancements and bug fixes
· Click to view the list of bug fixes for this release: Link
· v20.0.2 is a maintenance release based on v20.0.1, with the following updates:
· Click to view the list of bug fixes for this release: Link
· v20.0.1 is a maintenance release based on v20.0.0, with the following updates:
· Click to view the list of bug fixes for this release: Link
· v20.0.0 is the first full-featured version of CCS based on the Theia IDE. No further feature releases are planned for CCS v12.x.
· New Theia-based IDE:
· Currently no support for CC32xx.
· Use of Trace data files is not operational on Linux
· Click to view the list of bug fixes for this release: Link
Click to view the list of open issues related to CCS: Link
|
ARM Clang Compiler Tools |
v4.0.3.LTS |
|
Automotive Processor Device Support |
v1.1.18 |
|
Automotive Processor Feature Metadata |
v1.1.18 |
|
BlackHawk Emulator Drivers |
v9.0.0.002 |
|
C2000 Device Support |
v6.26.1.0 |
|
C2000 Emulation Flash |
v1.0.0.5 |
|
C2000_FEATURE_METADATA |
v6.26.1.0 |
|
C2800 Compiler Tools |
v22.6.2.LTS |
|
C29 Compiler Tools |
v1.0.0.LTS |
|
C29 Feature Metadata |
v1.2.16.0 |
|
C29 Device Support |
v1.2.16.0 |
|
C6000 Compiler Tools |
v8.3.13 |
|
C6000 Device Support |
v1.1.7 |
|
C7000 Compiler Tools |
v5.0.0.LTS |
|
CC26xx Device Support |
v3.21.3.57 |
|
CC3220 Device Support |
v1.0.5 |
|
CC323X Device Support |
v1.0.5 |
|
CC32xx Device Support |
v1.0.8 |
|
CC32xx Driver Support |
v1.0.8 |
|
CCS Server |
v20.2.0.202505162334 |
|
CCS Theia Installer Dependencies |
v1.0.0.20170130000000 |
|
CCS Utilities |
v1.0.2.20250509 |
|
Debug Server |
v20.2.0.3756 |
|
Debug Server Flash |
v20.2.0.3756 |
|
Hercules Device Support |
v6.0.9 |
|
IDE_METADATA |
v1.8.0 |
|
InstallBuilder |
v24.3.0 |
|
LPCS_FEATURE_METADATA |
v3.21.3.57 |
|
MMWAVE_FEATURE_METADATA |
v1.7.19 |
|
MSP430 Build Header Support |
v11.1.0.20211104 |
|
MSP430 Compiler Tools |
v21.6.1.LTS |
|
MSP430 Debug Support |
v11.1.0.20211104 |
|
MSP430 Device Support |
v11.1.0.20211104 |
|
MSP430 GCC Build Header Support |
v11.1.0.20211104 |
|
MSP432 Debug Support |
v8.2.3.0 |
|
MSP432 Device Support |
v8.2.2.0 |
|
MSPM0 Support |
v1.15.00.04 |
|
MSPM0_FEATURE_METADATA |
v1.15.00.04 |
|
MSVC 2015+ Redistributable |
v14.38.33135 |
|
Main CCS Theia Installer |
v20.2.0.20250523114933 |
|
Mmwave Radar Device Support |
v1.7.19 |
|
Node.js |
v18.16.0 |
|
OMAPL Device Support |
v1.1.2 |
|
PGA Device Support |
v1.0.2 |
|
SEGGER J-Link |
v8.34.0 |
|
SEGGER J-Link USB Driver |
v1.0.1.0 |
|
Shared Device Support |
v1.1.7 |
|
Signal Processing MCU Feature Metadata |
v1.1.0 |
|
Signal Processing MCU Device Support |
v1.1.0 |
|
Sitara Device Support |
v1.6.10 |
|
Sitara Feature Metadata |
v1.6.10 |
|
Sitara MCU Device Support |
v1.4.8 |
|
Sitara MCU Feature Metadata |
v1.4.8 |
|
SysConfig |
v1.24.0.4110 |
|
TI Cloud Agent |
v0.5.5246 |
|
TI Emulators |
v20.2.0.3536 |
|
TIREX Desktop |
v4.20.0.202411191616 |
|
TM4C Device Support |
v2.1.1.15071 |
|
TM4E Device Support |
v2.1.1.15071 |
|
TargetDB Default Props |
v12.3.0.N202303010900 |
|
Theia |
v20.2.0.20250523114933 |
|
Tiva/Stellaris ICDI Debug Probe |
v2.1.3.15 |
|
UCD Digital Power Controllers |
v1.1.5 |
|
YAROV |
v2.0.2 |
|
|
|
Windows 10 and Windows 11 are all trademarks and/or registered trademarks of Microsoft Corporation.
OSX, macOS are trademarks of Apple.
MSPM0, MSP430, GUI Composer, C2000, Code Composer Studio, XDS110 are trademarks
of Texas Instruments.
Ubuntu is a trademark of Canonical.
J-Link is a trademark of Segger.
© Copyright 2024