Release Notes — CCStudio™ IDE v21.0.1

Service release

General Information

These release notes contain important information about CCStudio™ IDE v21.0.1 that may not be included in other product documentation. Please review this document before using this release.

CCStudio IDE v21.0.1 is a service release. For a summary of changes, see the v21.0.1 What’s New section below.

System Requirements

ⓘ Note

CCStudio IDE is a 64-bit application and will not run on 32-bit operating systems.

Windows
  • Windows 11 64-bit
  • Windows 10 64-bit
Linux
  • Ubuntu 26.04 64-bit
  • Ubuntu 24.04 64-bit
  • Ubuntu 22.04 64-bit
macOS
  • macOS 14 Sonoma
  • macOS 15 Sequoia
  • macOS 26 Tahoe
ⓘ Note

For more details on platform-specific requirements and installation instructions, refer to the CCStudio IDE User’s Guide.

CCStudio IDE v21.0.1 — What’s New

New Features
Issue Summary
EXT_EP-12257 Need ability to specify where to save Target Configuration file (ccxml)

When creating a target configuration file there should be the ability to browse to where you want to save the file. It only saves to the default location. CCSv12 and earlier could specify the location.

EXT_EP-12966 Option to export all messages in the Problems view to a log file

Open to export all messages in the Problems view to a log file, or at least the ability to "Select All" like what was available in CCS Eclipse. Note that it is possible to multi select lines by selecting a line and then holding down SHIFT button and then selecting another line to select all the lines in between. Then use CTRL+C and CTRL+V to copy and paste. However this doesn't work well with many lines so it is not a viable workaround.

EXT_EP-13051 Support expression values when exporting/importing to/from JSON text file

The Watch view has the option to import/export expression names from/to a JSON text file. This request is to also support expression values. Allow the user the option to include the values on export. Also allow the user to choose if they wish to import the names and also write the associated values stored in the JSON file. If there are no values in the JSON file then only the names will be imported.

EXT_EP-13259 Read, reset, configure profile clock Tool API

Need tool call API to read, reset, enable, disable profile clock.

Bug Fixes

Previous Releases

Full release notes for earlier versions are available as individual documents. Each page includes a complete What’s New summary, known issues, and a link to the bug-fix tracker for that release.

📄 View previous release notes
Version Type Highlights Release Notes
v21.0.0 Feature Improvements to our AI integrations; New System project graphic editor; python scripting support View notes
v20.5.1 Feature Fixes to AI Integration features released in CCS v20.5.0 View notes
v20.5.0 Feature AI Integration features: getting started UI, MCP servers, graph improvements for FFT, build performance improvements, scripting improvements View notes
v20.4.1 Service Debugger fixes for M33 breakpoints, daisy-chain hardware breakpoints, and full verification mismatch View notes
v20.4.0 Feature Theia IDE core v1.64.1; improved project wizard; macOS 26 support; IDE & debug enhancements; Energia support removed View notes
v20.3.1 Service Secure Debug Manager fix (Windows); MSPM33 macOS flash loader; Arm Clang v4.0.4.LTS; J-Link v8.7.0; device support updates View notes
v20.3.0 Feature Graph view; Python scripting; ARM Advanced Features; new device support (CC35xx, MSPM33, UCD3138R); SysConfig v1.25; C6000 compiler v8.5.0.LTS View notes
v20.2.0 Feature Theia IDE core v1.58; AI/code assistant support; debug view improvements; assembly syntax highlighting; JRE v21; SysConfig v1.24 View notes
v20.1.1 Service Watch/Variable view enhancements; clangd support improvements; CC13x4 program load fix; Windows IDE update fix View notes
v20.1.0 Feature IDE feature improvements; macOS Arm native startup; XDS110 firmware fixes; device support updates (AM62L, xWRL68xx, MSPM0C110x); TI ARM Clang v4.0.2 View notes
v20.0.0 Feature First full-featured release based on Theia IDE; replaces the Eclipse-based v12.x release; new views (Modules, Stack Usage, Memory Map, GEL); broad device family coverage View notes

All Open Issues

The following JIRA query returns all open issues across the CCStudio IDE product areas, including Theia IDE, debug and trace, Resource Explorer, and SysConfig:

Components

For details on all components included in this release, please review the manifest: