2.4.4. Saturation in C¶
To perform efficient saturation in C on the C28x, use the ternary ?: operator.
Using if results in the following code with -O3:
C Source |
Generated Assembly |
|---|---|
int saturate(int sum, int max, int min)
{
if( sum > max )
sum = max;
if( sum < min )
sum = min;
return sum;
}
|
||saturate||:
MOVZ AR6,AL
MOV AL,AR4
CMP AH,AR6
MOV AR6,AH,LT
CMP AL,AR6
MOV AR6,AL,GT
MOV AL,AR6
LRETR
|
Using ?: generates the much more efficient MAX/MIN instructions:
C Source |
Generated Assembly |
|---|---|
int saturate_opt(int sum, int max, int min)
{
sum = (sum > max) ? max : sum;
sum = (sum < min) ? min : sum;
return sum;
}
|
||saturate_opt||:
MIN AL,AH
MAX AL,AR4
LRETR
|