2.4.2. Grouping global variables¶
Group global variables into structures can potentially enable the compiler to generate efficient direct addressing using the DP and minimize the number of updates to the DP between variable accesses.
Table 2.3 illustrates grouping global variables into fields in a struct.
Global variables |
Global variables grouped into a struct |
|---|---|
int16_t global0;
int16_t global1;
int16_t global2;
int16_t global3;
int16_t global4;
int16_t global5[32];
int16_t foo()
{
return global0 + global1 + global2 +
global3 + global4 + global5[0];
}
|
typedef struct {
int16_t global0;
int16_t global1;
int16_t global2;
int16_t global3;
int16_t global4;
int16_t global5[32];
} Globals;
Globals g;
int16_t bar()
{
return g.global0 + g.global1 + g.global2 +
g.global3 + g.global4 + g.global5[0];
}
|
Table 2.4 illustrates the improvement in the generated assembly from grouping global variables - there are fewer updates to the DP between accesses - 3 vs. 1 for the 5 accesses.
||foo||:
MOVW DP,#||global0||
MOV AL,@||global0||
MOVW DP,#||global5||
ADD AL,@||global5||
MOVW DP,#||global1||
ADD AL,@||global1||
ADD AL,@||global2||
ADD AL,@||global3||
ADD AL,@||global4||
LRETR
|
||bar||:
MOVW DP,#||g||+1
MOV AL,@||g||+1
ADD AL,@||g||
ADD AL,@||g||+2
ADD AL,@||g||+3
ADD AL,@||g||+4
ADD AL,@||g||+5
LRETR
|
Refer to TMS320C28x Optimizing C/C++ Compiler User’s Guide, Section 3.11, Data Page (DP) Pointer Load Optimization for details.