7.12. CDD_DMA

7.12.1. Types

Base type

Type Name

Brief

enum

Cdd_Dma_EmulationModeType

Emulation control type.

enum

Cdd_Dma_PriorityType

Channel priority selection type.

enum

Cdd_Dma_InstanceType

DMA instance type.

enum

Cdd_Dma_ChannelType

DMA Channel type.

enum

Cdd_Dma_MpuRegionType

DMA MPU Region type.

enum

Cdd_Dma_ChannelWrDataSizeType

Write data size mode bit type.

enum

Cdd_Dma_ChannelDataSizeType

Data size mode bit type.

enum

Cdd_Dma_ContinuousModeEnableType

Continuous mode type.

enum

Cdd_Dma_OneshotModeEnableType

Oneshot mode type.

enum

Cdd_Dma_ChIntEnableType

Channel interrupt generation enable type.

enum

Cdd_Dma_ChIntModeType

Channel interrupt generation mode type.

enum

Cdd_Dma_OvrflowIntEnableType

Overflow interrupt type.

enum

Cdd_Dma_PeriEvtTrigEnableType

Peripheral event trigger enable type.

enum

Cdd_Dma_OverflowStatusType

Overflow status type.

enum

Cdd_Dma_RunStatusType

Run status type.

enum

Cdd_Dma_BurstStatusType

Burst status type.

enum

Cdd_Dma_TransferStatusType

Transfer status type.

enum

Cdd_Dma_PeriEvtTrigStatusType

Peripheral event trigger status type.

enum

Cdd_Dma_MpuRegionAccessType

MPU region access type.

enum

Cdd_Dma_ChannelPriority

Channel priority type.

enum

Cdd_Dma_PeriEvtTriggerSrcType

Peripheral event trigger source select type.

typedef void(*)(uint8 Channel_Index)

Cdd_Dma_NotifyType

Channel notification callback function pointer.

typedef uint16

Cdd_Dma_MpuChmaskType

MPU Region channel mask parameter.

7.12.1.1. enum Cdd_Dma_EmulationModeType

Enumerator

Value

Description

CDD_DMA_EMULATION_STOP

The DMA completes the current read-write operation, then halts.

CDD_DMA_EMULATION_FREE_RUN

The DMA continues running during an emulation halt.

Brief: Emulation control type.

7.12.1.2. enum Cdd_Dma_PriorityType

Enumerator

Value

Description

CDD_DMA_PRIORITY_ROUND_ROBIN

The round-robin priority scheme.

CDD_DMA_PRIORITY_SOFTWARE_CONFIG

Software configurable priority for channels.

Brief: Channel priority selection type.

7.12.1.3. enum Cdd_Dma_InstanceType

Enumerator

Value

Description

CDD_DMA1

0

CDD_DMA2

1

Brief: DMA instance type.

7.12.1.4. enum Cdd_Dma_ChannelType

Enumerator

Value

Description

CDD_DMA_CH1

0

CDD_DMA_CH2

1

CDD_DMA_CH3

2

CDD_DMA_CH4

3

CDD_DMA_CH5

4

CDD_DMA_CH6

5

CDD_DMA_CH7

6

CDD_DMA_CH8

7

CDD_DMA_CH9

8

CDD_DMA_CH10

9

Brief: DMA Channel type.

7.12.1.5. enum Cdd_Dma_MpuRegionType

Enumerator

Value

Description

CDD_DMA_MPUR1

0

RTDMA MPU Region 1.

CDD_DMA_MPUR2

1

RTDMA MPU Region 2.

CDD_DMA_MPUR3

2

RTDMA MPU Region 3.

CDD_DMA_MPUR4

3

RTDMA MPU Region 4.

CDD_DMA_MPUR5

4

RTDMA MPU Region 5.

CDD_DMA_MPUR6

5

RTDMA MPU Region 6.

CDD_DMA_MPUR7

6

RTDMA MPU Region 7.

CDD_DMA_MPUR8

7

RTDMA MPU Region 8.

CDD_DMA_MPUR9

8

RTDMA MPU Region 9.

CDD_DMA_MPUR10

9

RTDMA MPU Region 10.

CDD_DMA_MPUR11

10

RTDMA MPU Region 11.

CDD_DMA_MPUR12

11

RTDMA MPU Region 12.

CDD_DMA_MPUR13

12

RTDMA MPU Region 13.

CDD_DMA_MPUR14

13

RTDMA MPU Region 14.

CDD_DMA_MPUR15

14

RTDMA MPU Region 15.

CDD_DMA_MPUR16

15

RTDMA MPU Region 16.

Brief: DMA MPU Region type.

7.12.1.6. enum Cdd_Dma_ChannelWrDataSizeType

Enumerator

Value

Description

CDD_DMA_CHANNEL_WR_DATASIZE_MODE_8

=

    0x0U| DMA channel transfers 8 bits of data on write port per read/write operation.   |

| CDD_DMA_CHANNEL_WR_DATASIZE_MODE_16 | = 0x100000U| DMA channel transfers 16 bits of data on write port per read/write operation. | | CDD_DMA_CHANNEL_WR_DATASIZE_MODE_32 | = 0x200000U| DMA channel transfers 32 bits of data on write port per read/write operation. | | CDD_DMA_CHANNEL_WR_DATASIZE_MODE_64 | = 0x300000U| DMA channel transfers 64 bits of data on write port per read/write operation. |

Brief: Write data size mode bit type.

7.12.1.7. enum Cdd_Dma_ChannelDataSizeType

Enumerator

Value

Description

CDD_DMA_CHANNEL_DATASIZE_MODE_8

=

    0x0U| DMA channel transfers 8 bits of data per read/write operation.   |

| CDD_DMA_CHANNEL_DATASIZE_MODE_16 | = 0x20000U| DMA channel transfers 16 bits of data per read/write operation. | | CDD_DMA_CHANNEL_DATASIZE_MODE_32 | = 0x40000U| DMA channel transfers 32 bits of data per read/write operation. | | CDD_DMA_CHANNEL_DATASIZE_MODE_64 | = 0x60000U| DMA channel transfers 64 bits of data per read/write operation. |

Brief: Data size mode bit type.

7.12.1.8. enum Cdd_Dma_ContinuousModeEnableType

Enumerator

Value

Description

CDD_DMA_CONTINUOUS_MODE_DISABLED

Continuous mode disabled.

CDD_DMA_CONTINUOUS_MODE_ENABLED

Continuous mode enabled.

Brief: Continuous mode type.

7.12.1.9. enum Cdd_Dma_OneshotModeEnableType

Enumerator

Value

Description

CDD_DMA_ONESHOT_MODE_DISABLED

Oneshot mode disabled.

CDD_DMA_ONESHOT_MODE_ENABLED

Oneshot mode enabled.

Brief: Oneshot mode type.

7.12.1.10. enum Cdd_Dma_ChIntEnableType

Enumerator

Value

Description

CDD_DMA_CHANNEL_INTERRUPT_DISABLED

Channel interrupt generation mode disabled.

CDD_DMA_CHANNEL_INTERRUPT_ENABLED

Channel interrupt generation mode enabled.

Brief: Channel interrupt generation enable type.

7.12.1.11. enum Cdd_Dma_ChIntModeType

Enumerator

Value

Description

CDD_DMA_INT_BEG_OF_TRANSFER

Generate interrupt at beginning of new transfer.

CDD_DMA_INT_END_OF_TRANSFER

Generate interrupt at end of transfer.

Brief: Channel interrupt generation mode type.

7.12.1.12. enum Cdd_Dma_OvrflowIntEnableType

Enumerator

Value

Description

CDD_DMA_OVERFLOW_INTERRUPT_DISABLED

Overflow interrupt disabled.

CDD_DMA_OVERFLOW_INTERRUPT_ENABLED

Overflow interrupt enabled.

Brief: Overflow interrupt type.

7.12.1.13. enum Cdd_Dma_PeriEvtTrigEnableType

Enumerator

Value

Description

CDD_DMA_PERI_EVT_TRIG_DISABLED

Peripheral event trigger disabled.

CDD_DMA_PERI_EVT_TRIG_ENABLED

Peripheral event trigger enabled.

Brief: Peripheral event trigger enable type.

7.12.1.14. enum Cdd_Dma_OverflowStatusType

Enumerator

Value

Description

CDD_DMA_OVERFLOW_NOT_DETECTED

No overflow detected.

CDD_DMA_OVERFLOW_DETECTED

Overflow detected i.e. peripheral event trigger was received while PERINTFLG was already set.

Brief: Overflow status type.

7.12.1.15. enum Cdd_Dma_RunStatusType

Enumerator

Value

Description

CDD_DMA_CHANNEL_NOT_RUNNING

DMA channel is ready to respond to peripheral event triggers - no ongoing transfer.

CDD_DMA_CHANNEL_RUNNING

DMA channel is busy.

Brief: Run status type.

7.12.1.16. enum Cdd_Dma_BurstStatusType

Enumerator

Value

Description

CDD_DMA_NO_BURST_ACTIVITY_ONGOING

Burst is completed i.e. BURST_COUNT has reached zero.

CDD_DMA_BURST_ACTIVITY_ONGOING

Burst is in progress.

Brief: Burst status type.

7.12.1.17. enum Cdd_Dma_TransferStatusType

Enumerator

Value

Description

CDD_DMA_NO_TRANSFER_ACTIVITY_ONGOING

Transfer is completed i.e. TRANSFER_COUNT has reached zero.

CDD_DMA_TRANSFER_ACTIVITY_ONGOING

Transfer is in progress.

Brief: Transfer status type.

7.12.1.18. enum Cdd_Dma_PeriEvtTrigStatusType

Enumerator

Value

Description

CDD_DMA_WAITING_FOR_EVT_TRIG

Wating for peripheral event trigger.

CDD_DMA_PENDING_EVT_TRIG

Peripheral event trigger has arrived.

Brief: Peripheral event trigger status type.

7.12.1.19. enum Cdd_Dma_MpuRegionAccessType

Enumerator

Value

Description

CDD_DMA_NO_ACCESS

No access to the region.

CDD_DMA_READ_ACCESS

Only read access.

CDD_DMA_READ_WRITE_ACCESS

Both read and write access.

Brief: MPU region access type.

7.12.1.20. enum Cdd_Dma_ChannelPriority

Enumerator

Value

Description

CDD_DMA_CHPRIORITY0

Priority 0.

CDD_DMA_CHPRIORITY1

Priority 1.

CDD_DMA_CHPRIORITY2

Priority 2.

CDD_DMA_CHPRIORITY3

Priority 3.

Brief: Channel priority type.

7.12.1.21. enum Cdd_Dma_PeriEvtTriggerSrcType

Enumerator

Value

Description

CDD_DMA_TRIGGER_SOFTWARE

0

TRIGGER SOFTWARE.

CDD_DMA_TRIGGER_ADCA1

1

TRIGGER ADCA1.

CDD_DMA_TRIGGER_ADCA2

2

TRIGGER ADCA2.

CDD_DMA_TRIGGER_ADCA3

3

TRIGGER ADCA3.

CDD_DMA_TRIGGER_ADCA4

4

TRIGGER ADCA4.

CDD_DMA_TRIGGER_ADCAEVT

5

TRIGGER ADCAEVT.

CDD_DMA_TRIGGER_ADCB1

6

TRIGGER ADCB1.

CDD_DMA_TRIGGER_ADCB2

7

TRIGGER ADCB2.

CDD_DMA_TRIGGER_ADCB3

8

TRIGGER ADCB3.

CDD_DMA_TRIGGER_ADCB4

9

TRIGGER ADCB4.

CDD_DMA_TRIGGER_ADCBEVT

10

TRIGGER ADCBEVT.

CDD_DMA_TRIGGER_ADCC1

11

TRIGGER ADCC1.

CDD_DMA_TRIGGER_ADCC2

12

TRIGGER ADCC2.

CDD_DMA_TRIGGER_ADCC3

13

TRIGGER ADCC3.

CDD_DMA_TRIGGER_ADCC4

14

TRIGGER ADCC4.

CDD_DMA_TRIGGER_ADCCEVT

15

TRIGGER ADCCEVT.

CDD_DMA_TRIGGER_ADCD1

16

TRIGGER ADCD1.

CDD_DMA_TRIGGER_ADCD2

17

TRIGGER ADCD2.

CDD_DMA_TRIGGER_ADCD3

18

TRIGGER ADCD3.

CDD_DMA_TRIGGER_ADCD4

19

TRIGGER ADCD4.

CDD_DMA_TRIGGER_ADCDEVT

20

TRIGGER ADCDEVT.

CDD_DMA_TRIGGER_ADCE1

21

TRIGGER ADCE1.

CDD_DMA_TRIGGER_ADCE2

22

TRIGGER ADCE2.

CDD_DMA_TRIGGER_ADCE3

23

TRIGGER ADCE3.

CDD_DMA_TRIGGER_ADCE4

24

TRIGGER ADCE4.

CDD_DMA_TRIGGER_ADCEEVT

25

TRIGGER ADCEEVT.

CDD_DMA_TRIGGER_CPU1_XINT1

31

TRIGGER CPU1 XINT1.

CDD_DMA_TRIGGER_CPU1_XINT2

32

TRIGGER CPU1 XINT2.

CDD_DMA_TRIGGER_CPU1_XINT3

33

TRIGGER CPU1 XINT3.

CDD_DMA_TRIGGER_CPU1_XINT4

34

TRIGGER CPU1 XINT4.

CDD_DMA_TRIGGER_CPU1_XINT5

35

TRIGGER CPU1 XINT5.

CDD_DMA_TRIGGER_CPU2_XINT1

36

TRIGGER CPU2 XINT1.

CDD_DMA_TRIGGER_CPU2_XINT2

37

TRIGGER CPU2 XINT2.

CDD_DMA_TRIGGER_CPU2_XINT3

38

TRIGGER CPU2 XINT3.

CDD_DMA_TRIGGER_CPU2_XINT4

39

TRIGGER CPU2 XINT4.

CDD_DMA_TRIGGER_CPU2_XINT5

40

TRIGGER CPU2 XINT5.

CDD_DMA_TRIGGER_CPU3_XINT1

41

TRIGGER CPU3 XINT1.

CDD_DMA_TRIGGER_CPU3_XINT2

42

TRIGGER CPU3 XINT2.

CDD_DMA_TRIGGER_CPU3_XINT3

43

TRIGGER CPU3 XINT3.

CDD_DMA_TRIGGER_CPU3_XINT4

44

TRIGGER CPU3 XINT4.

CDD_DMA_TRIGGER_CPU3_XINT5

45

TRIGGER CPU3 XINT5.

CDD_DMA_TRIGGER_EPWM1SOCA

46

TRIGGER EPWM1SOCA.

CDD_DMA_TRIGGER_EPWM1SOCB

47

TRIGGER EPWM1SOCB.

CDD_DMA_TRIGGER_EPWM2SOCA

48

TRIGGER EPWM2SOCA.

CDD_DMA_TRIGGER_EPWM2SOCB

49

TRIGGER EPWM2SOCB.

CDD_DMA_TRIGGER_EPWM3SOCA

50

TRIGGER EPWM3SOCA.

CDD_DMA_TRIGGER_EPWM3SOCB

51

TRIGGER EPWM3SOCB.

CDD_DMA_TRIGGER_EPWM4SOCA

52

TRIGGER EPWM4SOCA.

CDD_DMA_TRIGGER_EPWM4SOCB

53

TRIGGER EPWM4SOCB.

CDD_DMA_TRIGGER_EPWM5SOCA

54

TRIGGER EPWM5SOCA.

CDD_DMA_TRIGGER_EPWM5SOCB

55

TRIGGER EPWM5SOCB.

CDD_DMA_TRIGGER_EPWM6SOCA

56

TRIGGER EPWM6SOCA.

CDD_DMA_TRIGGER_EPWM6SOCB

57

TRIGGER EPWM6SOCB.

CDD_DMA_TRIGGER_EPWM7SOCA

58

TRIGGER EPWM7SOCA.

CDD_DMA_TRIGGER_EPWM7SOCB

59

TRIGGER EPWM7SOCB.

CDD_DMA_TRIGGER_EPWM8SOCA

60

TRIGGER EPWM8SOCA.

CDD_DMA_TRIGGER_EPWM8SOCB

61

TRIGGER EPWM8SOCB.

CDD_DMA_TRIGGER_EPWM9SOCA

62

TRIGGER EPWM9SOCA.

CDD_DMA_TRIGGER_EPWM9SOCB

63

TRIGGER EPWM9SOCB.

CDD_DMA_TRIGGER_EPWM10SOCA

64

TRIGGER EPWM10SOCA.

CDD_DMA_TRIGGER_EPWM10SOCB

65

TRIGGER EPWM10SOCB.

CDD_DMA_TRIGGER_EPWM11SOCA

66

TRIGGER EPWM11SOCA.

CDD_DMA_TRIGGER_EPWM11SOCB

67

TRIGGER EPWM11SOCB.

CDD_DMA_TRIGGER_EPWM12SOCA

68

TRIGGER EPWM12SOCA.

CDD_DMA_TRIGGER_EPWM12SOCB

69

TRIGGER EPWM12SOCB.

CDD_DMA_TRIGGER_EPWM13SOCA

70

TRIGGER EPWM13SOCA.

CDD_DMA_TRIGGER_EPWM13SOCB

71

TRIGGER EPWM13SOCB.

CDD_DMA_TRIGGER_EPWM14SOCA

72

TRIGGER EPWM14SOCA.

CDD_DMA_TRIGGER_EPWM14SOCB

73

TRIGGER EPWM14SOCB.

CDD_DMA_TRIGGER_EPWM15SOCA

74

TRIGGER EPWM15SOCA.

CDD_DMA_TRIGGER_EPWM15SOCB

75

TRIGGER EPWM15SOCB.

CDD_DMA_TRIGGER_EPWM16SOCA

76

TRIGGER EPWM16SOCA.

CDD_DMA_TRIGGER_EPWM16SOCB

77

TRIGGER EPWM16SOCB.

CDD_DMA_TRIGGER_EPWM17SOCA

78

TRIGGER EPWM17SOCA.

CDD_DMA_TRIGGER_EPWM17SOCB

79

TRIGGER EPWM17SOCB.

CDD_DMA_TRIGGER_EPWM18SOCA

80

TRIGGER EPWM18SOCA.

CDD_DMA_TRIGGER_EPWM18SOCB

81

TRIGGER EPWM18SOCB.

CDD_DMA_TRIGGER_TINT0

94

TRIGGER CPU1 TINT0.

CDD_DMA_TRIGGER_TINT1

95

TRIGGER CPU1 TINT1.

CDD_DMA_TRIGGER_TINT2

96

TRIGGER CPU1 TINT2.

CDD_DMA_TRIGGER_CPU2_TINT0

97

TRIGGER CPU2 TINT0.

CDD_DMA_TRIGGER_CPU2_TINT1

98

TRIGGER CPU2 TINT1.

CDD_DMA_TRIGGER_CPU2_TINT2

99

TRIGGER CPU2 TINT2.

CDD_DMA_TRIGGER_CPU3_TINT0

100

TRIGGER CPU3 TINT0.

CDD_DMA_TRIGGER_CPU3_TINT1

101

TRIGGER CPU3 TINT1.

CDD_DMA_TRIGGER_CPU3_TINT2

102

TRIGGER CPU3 TINT2.

CDD_DMA_TRIGGER_ECAP1

112

TRIGGER ECAP1.

CDD_DMA_TRIGGER_ECAP2

113

TRIGGER ECAP2.

CDD_DMA_TRIGGER_ECAP3

114

TRIGGER ECAP3.

CDD_DMA_TRIGGER_ECAP4

115

TRIGGER ECAP4.

CDD_DMA_TRIGGER_ECAP5

116

TRIGGER ECAP5.

CDD_DMA_TRIGGER_ECAP6

117

TRIGGER ECAP6.

CDD_DMA_TRIGGER_LINATX

120

TRIGGER LINATX.

CDD_DMA_TRIGGER_LINARX

121

TRIGGER LINARX.

CDD_DMA_TRIGGER_LINBTX

122

TRIGGER LINBTX.

CDD_DMA_TRIGGER_LINBRX

123

TRIGGER LINBRX.

CDD_DMA_TRIGGER_SYNC

124

TRIGGER SYNC.

CDD_DMA_TRIGGER_SPIATX

125

TRIGGER SPIATX.

CDD_DMA_TRIGGER_SPIARX

126

TRIGGER SPIARX.

CDD_DMA_TRIGGER_SPIBTX

127

TRIGGER SPIBTX.

CDD_DMA_TRIGGER_SPIBRX

128

TRIGGER SPIBRX.

CDD_DMA_TRIGGER_SPICTX

129

TRIGGER SPICTX.

CDD_DMA_TRIGGER_SPICRX

130

TRIGGER SPICRX.

CDD_DMA_TRIGGER_SPIDTX

131

TRIGGER SPIDTX.

CDD_DMA_TRIGGER_SPIDRX

132

TRIGGER SPIDRX.

CDD_DMA_TRIGGER_SPIETX

133

TRIGGER SPIETX.

CDD_DMA_TRIGGER_SPIERX

134

TRIGGER SPIERX.

CDD_DMA_TRIGGER_CLB1INT

135

TRIGGER CLB1INT.

CDD_DMA_TRIGGER_CLB2INT

136

TRIGGER CLB2INT.

CDD_DMA_TRIGGER_CLB3INT

137

TRIGGER CLB3INT.

CDD_DMA_TRIGGER_CLB4INT

138

TRIGGER CLB4INT.

CDD_DMA_TRIGGER_CLB5INT

139

TRIGGER CLB5INT.

CDD_DMA_TRIGGER_CLB6INT

140

TRIGGER CLB6INT.

CDD_DMA_TRIGGER_FSITXA

143

TRIGGER FSITXA.

CDD_DMA_TRIGGER_FSIRXA

144

TRIGGER FSIRXA.

CDD_DMA_TRIGGER_FSIA_DATA_TAG_MATCH

145

TRIGGER FSIA DATA TAG MATCH.

CDD_DMA_TRIGGER_FSIA_PING_TAG_MATCH

146

TRIGGER FSIA PING TAG MATCH.

CDD_DMA_TRIGGER_FSIRXB

148

TRIGGER FSIRXB.

CDD_DMA_TRIGGER_FSITXB

147

TRIGGER FSITXB.

CDD_DMA_TRIGGER_FSIB_DATA_TAG_MATCH

149

TRIGGER FSIB DATA TAG MATCH.

CDD_DMA_TRIGGER_FSIB_PING_TAG_MATCH

150

TRIGGER FSIB PING TAG MATCH.

CDD_DMA_TRIGGER_FSIRXC

152

TRIGGER FSIRXC.

CDD_DMA_TRIGGER_FSITXC

151

TRIGGER FSITXC.

CDD_DMA_TRIGGER_FSIC_DATA_TAG_MATCH

153

TRIGGER FSIC DATA TAG MATCH.

CDD_DMA_TRIGGER_FSIC_PING_TAG_MATCH

154

TRIGGER FSIC PING TAG MATCH.

CDD_DMA_TRIGGER_FSITXD

155

TRIGGER FSITXD.

CDD_DMA_TRIGGER_FSIRXD

156

TRIGGER FSIRXD.

CDD_DMA_TRIGGER_FSID_DATA_TAG_MATCH

157

TRIGGER FSID DATA TAG MATCH.

CDD_DMA_TRIGGER_FSID_PING_TAG_MATCH

158

TRIGGER FSID PING TAG MATCH.

CDD_DMA_TRIGGER_CPU1_DLT

161

TRIGGER CPU1 DLT.

CDD_DMA_TRIGGER_CPU3_DLT

163

TRIGGER CPU3 DLT.

CDD_DMA_TRIGGER_CPU2_DLT

162

TRIGGER CPU2 DLT.

CDD_DMA_TRIGGER_UARTARX

167

TRIGGER UARTARX.

CDD_DMA_TRIGGER_UARTATX

168

TRIGGER UARTATX.

CDD_DMA_TRIGGER_UARTBTX

169

TRIGGER UARTBTX.

CDD_DMA_TRIGGER_UARTBRX

170

TRIGGER UARTBRX.

CDD_DMA_TRIGGER_UARTCTX

171

TRIGGER UARTCTX.

CDD_DMA_TRIGGER_UARTCRX

172

TRIGGER UARTCRX.

CDD_DMA_TRIGGER_UARTDTX

173

TRIGGER UARTDTX.

CDD_DMA_TRIGGER_UARTDRX

174

TRIGGER UARTDRX.

CDD_DMA_TRIGGER_UARTETX

175

TRIGGER UARTETX.

CDD_DMA_TRIGGER_UARTERX

176

TRIGGER UARTERX.

CDD_DMA_TRIGGER_UARTFTX

177

TRIGGER UARTFTX.

CDD_DMA_TRIGGER_UARTFRX

178

TRIGGER UARTFRX.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_S_CTXIN_REQ

179

TRIGGER DTHE SHA DMA S CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_S_DATAIN_REQ

180

TRIGGER DTHE SHA DMA S DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_S_CTXOUT_REQ

181

TRIGGER DTHE SHA DMA S CTXOUT REQ.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_P_CTXIN_REQ

182

TRIGGER DTHE SHA DMA P CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_P_DATAIN_REQ

183

TRIGGER DTHE SHA DMA P DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_SHA_DMA_P_CTXOUT_REQ

184

TRIGGER DTHE SHA DMA P CTXOUT REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_S_CTXIN_REQ

185

TRIGGER DTHE AES DMA S CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_S_DATAIN_REQ

186

TRIGGER DTHE AES DMA S DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_S_DATAOUT_REQ

187

TRIGGER DTHE AES DMA S DATAOUT REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_S_CTXOUT_REQ

188

TRIGGER DTHE AES DMA S CTXOUT REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_P_CTXIN_REQ

189

TRIGGER DTHE AES DMA P CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_P_DATAIN_REQ

190

TRIGGER DTHE AES DMA P DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_P_DATAOUT_REQ

191

TRIGGER DTHE AES DMA P DATAOUT REQ.

CDD_DMA_TRIGGER_DTHE_AES_DMA_P_CTXOUT_REQ

192

TRIGGER DTHE AES DMA P CTXOUT REQ.

CDD_DMA_TRIGGER_DTHE_SM3_CTXIN_REQ

193

TRIGGER DTHE SM3 CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_SM3_DATAIN_REQ

194

TRIGGER DTHE SM3 DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_SM3_CTXOUT_REQ

195

TRIGGER DTHE SM3 CTXOUT REQ.

CDD_DMA_TRIGGER_DTHE_SM4_CTXIN_REQ

196

TRIGGER DTHE SM4 CTXIN REQ.

CDD_DMA_TRIGGER_DTHE_SM4_DATAIN_REQ

197

TRIGGER DTHE SM4 DATAIN REQ.

CDD_DMA_TRIGGER_DTHE_SM4_DATAOUT_REQ

198

TRIGGER DTHE SM4 DATAOUT REQ.

CDD_DMA_TRIGGER_DTHE_SM4_CTXOUT_REQ

199

TRIGGER DTHE SM4 CTXOUT REQ.

CDD_DMA_TRIGGER_EPG

200

TRIGGER EPG.

CDD_DMA_TRIGGER_SDFM1FLT1

201

TRIGGER SDFM1FLT1.

CDD_DMA_TRIGGER_SDFM1FLT2

202

TRIGGER SDFM1FLT2.

CDD_DMA_TRIGGER_SDFM1FLT3

203

TRIGGER SDFM1FLT3.

CDD_DMA_TRIGGER_SDFM1FLT4

204

TRIGGER SDFM1FLT4.

CDD_DMA_TRIGGER_SDFM2FLT1

205

TRIGGER SDFM2FLT1.

CDD_DMA_TRIGGER_SDFM2FLT2

206

TRIGGER SDFM2FLT2.

CDD_DMA_TRIGGER_SDFM2FLT3

207

TRIGGER SDFM2FLT3.

CDD_DMA_TRIGGER_SDFM2FLT4

208

TRIGGER SDFM2FLT4.

CDD_DMA_TRIGGER_SDFM3FLT1

209

TRIGGER SDFM3FLT1.

CDD_DMA_TRIGGER_SDFM3FLT2

210

TRIGGER SDFM3FLT2.

CDD_DMA_TRIGGER_SDFM3FLT3

211

TRIGGER SDFM3FLT3.

CDD_DMA_TRIGGER_SDFM3FLT4

212

TRIGGER SDFM3FLT4.

CDD_DMA_TRIGGER_SDFM4FLT1

213

TRIGGER SDFM4FLT1.

CDD_DMA_TRIGGER_SDFM4FLT2

214

TRIGGER SDFM4FLT2.

CDD_DMA_TRIGGER_SDFM4FLT3

215

TRIGGER SDFM4FLT3.

CDD_DMA_TRIGGER_SDFM4FLT4

216

TRIGGER SDFM4FLT4.

CDD_DMA_TRIGGER_SENT1

217

TRIGGER SENT1.

CDD_DMA_TRIGGER_SENT2

218

TRIGGER SENT2.

CDD_DMA_TRIGGER_SENT3

219

TRIGGER SENT3.

CDD_DMA_TRIGGER_SENT4

220

TRIGGER SENT4.

CDD_DMA_TRIGGER_SENT5

221

TRIGGER SENT5.

CDD_DMA_TRIGGER_SENT6

222

TRIGGER SENT6.

CDD_DMA_TRIGGER_WADI1

223

TRIGGER WADI1.

CDD_DMA_TRIGGER_WADI2

224

TRIGGER WADI2.

CDD_DMA_TRIGGER_RTDMA_CH1INT

240

TRIGGER RTDMA CH1INT.

CDD_DMA_TRIGGER_RTDMA_CH2INT

241

TRIGGER RTDMA CH2INT.

CDD_DMA_TRIGGER_RTDMA_CH3INT

242

TRIGGER RTDMA CH3INT.

CDD_DMA_TRIGGER_RTDMA_CH4INT

243

TRIGGER RTDMA CH4INT.

CDD_DMA_TRIGGER_RTDMA_CH5INT

244

TRIGGER RTDMA CH5INT.

CDD_DMA_TRIGGER_RTDMA_CH6INT

245

TRIGGER RTDMA CH6INT.

CDD_DMA_TRIGGER_RTDMA_CH7INT

246

TRIGGER RTDMA CH7INT.

CDD_DMA_TRIGGER_RTDMA_CH8INT

247

TRIGGER RTDMA CH8INT.

CDD_DMA_TRIGGER_RTDMA_CH9INT

248

TRIGGER RTDMA CH9INT.

CDD_DMA_TRIGGER_RTDMA_CH10INT

249

TRIGGER RTDMA CH10INT.

Brief: Peripheral event trigger source select type.

7.12.1.22. typedef Cdd_Dma_NotifyType

typedef void(* Cdd_Dma_NotifyType) (uint8 Channel_Index);

Brief: Channel notification callback function pointer.

7.12.1.23. typedef Cdd_Dma_MpuChmaskType

typedef uint16 Cdd_Dma_MpuChmaskType;

Brief: MPU Region channel mask parameter.

7.12.2. Structures

Name

Brief

Cdd_Dma_ChannelStatus

DMA Channel status structure.

Cdd_Dma_ChannelParamsType

DMA Channel properties.

Cdd_Dma_TransferSizeType

Burst and Transfer size parameter.

Cdd_Dma_TransferSrcStepType

Source burst step and transfer step parameter.

Cdd_Dma_TransferDestStepType

Destination burst step and transfer step parameter.

Cdd_Dma_TransferSrcWrapType

Source wrap size, wrap step and beginning address parameter.

Cdd_Dma_TransferDestWrapType

Destination wrap size, wrap step and beginning address parameter.

Cdd_Dma_TransferParamsType

DMA transfer properties.

Cdd_Dma_MpuRegionCfgType

DMA MPU Region configuration structure.

Cdd_Dma_HwInstanceCfgType

CDD DMA config type.

Cdd_Dma_ChannelCfgType

CDD DMA channel config type.

Cdd_Dma_ConfigType

CDD DMA config type.

Cdd_Dma_PeriodicReadBackDataType

CDD_DMA periodic readback type.

7.12.3. Defines

Name

Brief

CDD_DMA_SW_MAJOR_VERSION

Driver Implementation Major Version.

CDD_DMA_SW_MINOR_VERSION

Driver Implementation Minor Version.

CDD_DMA_SW_PATCH_VERSION

Driver Implementation Patch Version.

CDD_DMA_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CDD_DMA Driver.

CDD_DMA_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CDD_DMA Driver.

CDD_DMA_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CDD_DMA Driver.

CDD_DMA_VENDOR_ID

Texas Instruments Vendor ID.

CDD_DMA_MODULE_ID

CDD DMA Driver Module ID.

CDD_DMA_INSTANCE_ID

CDD DMA Instance ID.

CDD_DMA_E_UNINIT

API service used without module initialization.

CDD_DMA_E_ALREADY_INITIALIZED

API called for reinitialization of already initialized DMA driver.

CDD_DMA_E_INIT_FAILED

Initialization API failed.

CDD_DMA_E_PARAM_POINTER

API service called with invalid parameter pointer.

CDD_DMA_E_PARAM_VALUE

API service called with invalid parameter value.

CDD_DMA_E_BUSY

API service called during ongoing process.

CDD_DMA_E_PERIPHERAL_EVENT_TRIGGER_DISABLED

API service called to force or clear peripheral event trigger when peripheral event trigger is disabled.

CDD_DMA_E_PERIPHERAL_EVENT_TRIGGER_ENABLED

API service called to enable peripheral event trigger when peripheral event trigger is already enabled.

CDD_DMA_E_ALREADY_RUNNING

API service called to start a channel when the channel is already running.

CDD_DMA_E_ALREADY_HALTED

API service called to halt a channel when the channel already halted.

CDD_DMA_E_DMACFG_COMMITTED

API service called to modify DMA configurable properties when DMA configurable properties are committed.

CDD_DMA_E_CHCFG_COMMITTED

API service called to modify DMA channel properties when DMA channel properties are committed.

CDD_DMA_E_MPUR_COMMITTED

API service called to modify DMA MPU region properties when DMA MPU region properties are committed.

CDD_DMA_E_MPUCFG_COMMITTED

API service called to enable or disable MPU when DMA MPU configuration are committed.

CDD_DMA_E_NO_OVERFLOW

API service called to clear error flag when no overflow is detected.

CDD_DMA_E_NO_TRIGGER

API service called to clear peripheral event trigger when no event trigger exists.

CDD_DMA_SID_GET_VERSION_INFO

Cdd_Dma_GetVersionInfo() API Service ID.

CDD_DMA_SID_INIT

Cdd_Dma_Init() API Service ID.

CDD_DMA_SID_DEINIT

Cdd_Dma_DeInit() API Service ID.

CDD_DMA_SID_SET_CHANNEL_PROPERTIES

Cdd_Dma_SetChannelProperties() API Service ID.

CDD_DMA_SID_SET_TRANSFER_PROPERTIES

Cdd_Dma_SetTransferProperties() API Service ID.

CDD_DMA_SID_SET_TRANSFER_SIZE

Cdd_Dma_SetTransferSize() API Service ID.

CDD_DMA_SID_SET_TRANSFER_SRC_PROPERTIES

Cdd_Dma_SetTransferSrcProperties() API Service ID.

CDD_DMA_SID_SET_TRANSFER_DEST_PROPERTIES

Cdd_Dma_SetTransferDestProperties() API Service ID.

CDD_DMA_SID_SET_TRANSFER_SRC_ADDRESS

Cdd_Dma_SetTransferSrcAddress() API Service ID.

CDD_DMA_SID_SET_TRANSFER_DEST_ADDRESS

Cdd_Dma_SetTransferDestAddress() API Service ID.

CDD_DMA_SID_SET_TRANSFER_WRAP_SRC_PROPERTIES

Cdd_Dma_SetTransferWrapSrcProperties() API Service ID.

CDD_DMA_SID_SET_TRANSFER_WRAP_DEST_PROPERTIES

Cdd_Dma_SetTransferWrapDestProperties() API Service ID.

CDD_DMA_SID_ENABLE_PERIPHERAL_EVENT_TRIGGER

Cdd_Dma_EnablePeripheralEventTrigger() API Service ID.

CDD_DMA_SID_DISABLE_PERIPHERAL_EVENT_TRIGGER

Cdd_Dma_DisablePeripheralEventTrigger() API Service ID.

CDD_DMA_SID_SET_PERIPHERAL_EVENT_TRIGGER_SOURCE

Cdd_Dma_SetPeripheralEventTriggerSource() API Service ID.

CDD_DMA_SID_START_CHANNEL_TRANSFER

Cdd_Dma_StartChannelTransfer() API Service ID.

CDD_DMA_SID_STOP_CHANNEL_TRANSFER

Cdd_Dma_StopChannelTransfer() API Service ID.

CDD_DMA_SID_FORCE_PERIPHERAL_EVENT_TRIGGER

Cdd_Dma_ForcePeripheralEventTrigger() API Service ID.

CDD_DMA_SID_CLEAR_PERIPHERAL_EVENT_TRIGGER

Cdd_Dma_ClearPeripheralEventTrigger() API Service ID.

CDD_DMA_SID_TRIGGER_SOFT_RESET

Cdd_Dma_TriggerSoftReset() API Service ID.

CDD_DMA_SID_SET_CHANNEL_PRIORITY

Cdd_Dma_SetChannelPriority() API Service ID.

CDD_DMA_SID_GET_CHANNEL_STATUS

Cdd_Dma_GetChannelStatus() API Service ID.

CDD_DMA_SID_CLEAR_ERROR_FLAG

Cdd_Dma_ClearErrorFlag() API Service ID.

CDD_DMA_SID_SET_CHANNEL_COMMIT

Cdd_Dma_SetChannelCommit() API Service ID.

CDD_DMA_SID_SET_DMACFG_COMMIT

Cdd_Dma_SetDmaCfgCommit() API Service ID.

CDD_DMA_SID_SET_MPUR_COMMIT

Cdd_Dma_SetMpuRegionCommit() API Service ID.

CDD_DMA_SID_SET_MPUCFG_COMMIT

Cdd_Dma_SetMpuCfgCommit() API Service ID.

CDD_DMA_SID_GET_CHANNEL_PRIORITY

Cdd_Dma_GetChannelPriority() API Service ID.

CDD_DMA_SID_PERIODIC_READBACK

Cdd_Dma_PeriodicReadback() API Service ID.

7.12.4. Functions

Return type

Function Name

Brief

void

Cdd_Dma_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr)

Service to provide the version information of Cdd Dma module.

void

Cdd_Dma_Init(const Cdd_Dma_ConfigType * ConfigPtr)

Service to initialize CDD DMA driver.

void

Cdd_Dma_DeInit(void )

Service to deinitialize CDD DMA driver.

Std_ReturnType

Cdd_Dma_SetChannelProperties(uint8 ChannelId, Cdd_Dma_ChannelParamsType ChannelProperties)

Service to set the channel properties of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferProperties(uint8 ChannelId, Cdd_Dma_TransferParamsType TransferProperties)

Service to set the transfer properties of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferSize(uint8 ChannelId, uint16 BurstSize, uint32 TransferSize)

Service to set the burst size and transfer size of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferSrcProperties(uint8 ChannelId, sint16 SrcBurstStep, sint16 SrcTransferStep)

Service to set the transfer source properties : source burst step, source transfer step of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferDestProperties(uint8 ChannelId, sint16 DestBurstStep, sint16 DestTransferStep)

Service to set the transfer destination properties : destination burst step, destination transfer step of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferSrcAddress(uint8 ChannelId, uint32 SrcAddress)

Service to set the transfer source address of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferDestAddress(uint8 ChannelId, uint32 DestAddress)

Service to set the transfer destination address of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferWrapSrcProperties(uint8 ChannelId, uint32 SrcWrapSize, sint16 SrcWrapStep, uint32 SrcBegAddress)

Service to set the transfer source wrap properties of a DMA channel.

Std_ReturnType

Cdd_Dma_SetTransferWrapDestProperties(uint8 ChannelId, uint32 DestWrapSize, sint16 DestWrapStep, uint32 DestBegAddress)

Service to set the transfer destination wrap properties of a DMA channel.

Std_ReturnType

Cdd_Dma_EnablePeripheralEventTrigger(uint8 ChannelId)

Service to enable peripheral event triggers of a DMA channel.

Std_ReturnType

Cdd_Dma_DisablePeripheralEventTrigger(uint8 ChannelId)

Service to disable peripheral event triggers of a DMA channel.

Std_ReturnType

Cdd_Dma_SetPeripheralEventTriggerSource(uint8 ChannelId, Cdd_Dma_PeriEvtTriggerSrcType PeripheralEventTrigSrc)

Service to set the peripheral event trigger source for a DMA channel.

Std_ReturnType

Cdd_Dma_StartChannelTransfer(uint8 ChannelId)

Service to start or enable a DMA channel.

Std_ReturnType

Cdd_Dma_StopChannelTransfer(uint8 ChannelId)

Service to stop or disable a DMA channel.

Std_ReturnType

Cdd_Dma_ForcePeripheralEventTrigger(uint8 ChannelId)

Service to force the peripheral event trigger for the channel.

Std_ReturnType

Cdd_Dma_ClearPeripheralEventTrigger(uint8 ChannelId)

Service to clear the peripheral event trigger for the channel.

Std_ReturnType

Cdd_Dma_TriggerSoftReset(uint8 ChannelId)

Service to trigger a soft reset for the channel.

Std_ReturnType

Cdd_Dma_SetChannelPriority(uint8 ChannelId, Cdd_Dma_ChannelPriority Priority)

Service to set channel priority.

Std_ReturnType

Cdd_Dma_GetChannelPriority(uint8 ChannelId, Cdd_Dma_ChannelPriority * Priority)

Service to get channel priority.

void

Cdd_Dma_GetChannelStatus(uint8 ChannelId, Cdd_Dma_ChannelStatus * ChannelStatus)

Service to get the channel status : peripheral event trigger status, transfer status, burst status, run status and overflow status.

Std_ReturnType

Cdd_Dma_ClearErrorFlag(uint8 ChannelId)

Service to clear the overflow error flag for a DMA channel.

Std_ReturnType

Cdd_Dma_SetDmaCfgCommit(uint8 HwInstanceId)

Service to commit DMA configurable properties such as priority scheme, channel priority and emulation mode for a specific instance.

Std_ReturnType

Cdd_Dma_SetChannelCommit(uint8 ChannelId)

Service to commit DMA channel configurations for a specific channel.

Std_ReturnType

Cdd_Dma_SetMpuCfgCommit(uint8 HwInstanceId)

Service to commit Mpu configuration: MPUEN for a specific instance.

Std_ReturnType

Cdd_Dma_SetMpuRegionCommit(uint16 MpuRegionId)

Service to commit Mpu Region configurations for a specific MPU region.

void

Cdd_Dma_PeriodicReadback(uint8 ChannelId, Cdd_Dma_PeriodicReadBackDataType * ReadBackRegisterdata)

Service to read all the statically configured registers for periodic readback.

7.12.4.1. function Cdd_Dma_GetVersionInfo

void Cdd_Dma_GetVersionInfo(
    Std_VersionInfoType * VersionInfoPtr
)

Brief: Service to provide the version information of Cdd Dma module.

Parameters:

  • VersionInfoPtr is the pointer to CDD DMA driver version information.

Returns:

  • None

Return: None

Precondition: This API is available only if CDD_DMA_GET_VERSION_INFO_API is STD_ON

Postcondition: None

7.12.4.2. function Cdd_Dma_Init

void Cdd_Dma_Init(
    const Cdd_Dma_ConfigType * ConfigPtr
)

Brief: Service to initialize CDD DMA driver.

Parameters:

  • ConfigPtr is the NULL pointer for pre compile variant from plugin

Return: None

Precondition: Preconditions - Driver not already initialized

Postcondition: Postconditions - Driver in initialized state

7.12.4.3. function Cdd_Dma_DeInit

void Cdd_Dma_DeInit(
    void 
)

Brief: Service to deinitialize CDD DMA driver.

Return: None

Precondition: None

Postcondition: None

7.12.4.4. function Cdd_Dma_SetChannelProperties

Std_ReturnType Cdd_Dma_SetChannelProperties(
    uint8 ChannelId,
    Cdd_Dma_ChannelParamsType ChannelProperties
)

Brief: Service to set the channel properties of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the channel properties are configured

  • ChannelProperties Structure of type Cdd_Dma_ChannelParamsType which contains the channel properties to be set.

Returns:

  • E_OK Successfully set channel properties

  • E_NOT_OK Failed to set channel properties

Return: Status of setting channel properties

Precondition: None

Postcondition: None

7.12.4.5. function Cdd_Dma_SetTransferProperties

Std_ReturnType Cdd_Dma_SetTransferProperties(
    uint8 ChannelId,
    Cdd_Dma_TransferParamsType TransferProperties
)

Brief: Service to set the transfer properties of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the transfer properties are configured

  • TransferProperties Structure of type Cdd_Dma_TransferParamsType which contains the transfer properties to be set

Returns:

  • E_OK Successfully set transfer properties

  • E_NOT_OK Failed to set transfer properties

Return: Status of setting transfer properties

Precondition: None

Postcondition: None

7.12.4.6. function Cdd_Dma_SetTransferSize

Std_ReturnType Cdd_Dma_SetTransferSize(
    uint8 ChannelId,
    uint16 BurstSize,
    uint32 TransferSize
)

Brief: Service to set the burst size and transfer size of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the transfer size properties are configured

  • BurstSize Number of words transferred per burst

  • TransferSize Total number of bursts in the transfer

Returns:

  • E_OK Successfully set burst size and transfer size

  • E_NOT_OK Failed to set burst size and transfer size

Return: Status of setting burst size and transfer size

Precondition: None

Postcondition: None

7.12.4.7. function Cdd_Dma_SetTransferSrcProperties

Std_ReturnType Cdd_Dma_SetTransferSrcProperties(
    uint8 ChannelId,
    sint16 SrcBurstStep,
    sint16 SrcTransferStep
)

Brief: Service to set the transfer source properties : source burst step, source transfer step of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the source burst step and source transfer step properties are configured

  • SrcBurstStep Source burst step

  • SrcTransferStep Source transfer step

Returns:

  • E_OK Successfully set transfer source properties

  • E_NOT_OK Failed to set transfer source properties

Return: Status of setting transfer source properties : source burst step, source transfer step

Precondition: None

Postcondition: None

7.12.4.8. function Cdd_Dma_SetTransferDestProperties

Std_ReturnType Cdd_Dma_SetTransferDestProperties(
    uint8 ChannelId,
    sint16 DestBurstStep,
    sint16 DestTransferStep
)

Brief: Service to set the transfer destination properties : destination burst step, destination transfer step of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the destination burst step and destination transfer step properties are configured

  • DestBurstStep Destination burst step

  • DestTransferStep Destination transfer step

Returns:

  • E_OK Successfully set transfer destination properties

  • E_NOT_OK Failed to set transfer destination properties

Return: Status of setting transfer destination properties : destination burst step, destination transfer step

Precondition: None

Postcondition: None

7.12.4.9. function Cdd_Dma_SetTransferSrcAddress

Std_ReturnType Cdd_Dma_SetTransferSrcAddress(
    uint8 ChannelId,
    uint32 SrcAddress
)

Brief: Service to set the transfer source address of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the source address is configured

  • SrcAddress Transfer source address

Returns:

  • E_OK Successfully set transfer source address.

  • E_NOT_OK Failed to set source address.

Return: Status of setting transfer source address

Precondition: None

Postcondition: None

7.12.4.10. function Cdd_Dma_SetTransferDestAddress

Std_ReturnType Cdd_Dma_SetTransferDestAddress(
    uint8 ChannelId,
    uint32 DestAddress
)

Brief: Service to set the transfer destination address of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the destination address is configured

  • DestAddress Transfer destination address

Returns:

  • E_OK Successfully set transfer destination address

  • E_NOT_OK Failed to set destination address

Return: Status of setting transfer destination address

Precondition: None

Postcondition: None

7.12.4.11. function Cdd_Dma_SetTransferWrapSrcProperties

Std_ReturnType Cdd_Dma_SetTransferWrapSrcProperties(
    uint8 ChannelId,
    uint32 SrcWrapSize,
    sint16 SrcWrapStep,
    uint32 SrcBegAddress
)

Brief: Service to set the transfer source wrap properties of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the source wrap properties are configured

  • SrcWrapSize Source wrap size

  • SrcWrapStep Source wrap step

  • SrcBegAddress Source beginning address

Returns:

  • E_OK Successfully set source wrap properties

  • E_NOT_OK Failed to set source wrap properties

Return: Status of setting source wrap properties

Precondition: None

Postcondition: None

7.12.4.12. function Cdd_Dma_SetTransferWrapDestProperties

Std_ReturnType Cdd_Dma_SetTransferWrapDestProperties(
    uint8 ChannelId,
    uint32 DestWrapSize,
    sint16 DestWrapStep,
    uint32 DestBegAddress
)

Brief: Service to set the transfer destination wrap properties of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the destination wrap properties are configured

  • DestWrapSize Destination wrap size

  • DestWrapStep Destination wrap step

  • DestBegAddress Destination beginning address

Returns:

  • E_OK Successfully set destination wrap properties

  • E_NOT_OK Failed to set destination wrap properties

Return: Status of setting destination wrap properties

Precondition: None

Postcondition: None

7.12.4.13. function Cdd_Dma_EnablePeripheralEventTrigger

Std_ReturnType Cdd_Dma_EnablePeripheralEventTrigger(
    uint8 ChannelId
)

Brief: Service to enable peripheral event triggers of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which trigger shall be enabled

Returns:

  • E_OK Successfully enabled peripheral event trigger

  • E_NOT_OK Failed to enable peripheral event trigger

Return: Status of peripheral event trigger enabling

Precondition: None

Postcondition: None

7.12.4.14. function Cdd_Dma_DisablePeripheralEventTrigger

Std_ReturnType Cdd_Dma_DisablePeripheralEventTrigger(
    uint8 ChannelId
)

Brief: Service to disable peripheral event triggers of a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which trigger shall be disabled

Returns:

  • E_OK Successfully disabled peripheral event trigger

  • E_NOT_OK Failed to disabled peripheral event trigger

Return: Status of peripheral event trigger disabling

Precondition: None

Postcondition: None

7.12.4.15. function Cdd_Dma_SetPeripheralEventTriggerSource

Std_ReturnType Cdd_Dma_SetPeripheralEventTriggerSource(
    uint8 ChannelId,
    Cdd_Dma_PeriEvtTriggerSrcType PeripheralEventTrigSrc
)

Brief: Service to set the peripheral event trigger source for a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which trigger source shall be set

  • PeripheralEventTrigSrc : Peripheral event trigger source value

Returns:

  • E_OK Successfully set peripheral event trigger source

  • E_NOT_OK Failed to set peripheral event trigger source

Return: Status of setting peripheral event trigger source

Precondition: None

Postcondition: None

7.12.4.16. function Cdd_Dma_StartChannelTransfer

Std_ReturnType Cdd_Dma_StartChannelTransfer(
    uint8 ChannelId
)

Brief: Service to start or enable a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel which shall be enabled

Returns:

  • E_OK Successfully enabled the DMA channel

  • E_NOT_OK Failed to enable the DMA channel

Return: Status of enabling the DMA channel

Precondition: None

Postcondition: None

7.12.4.17. function Cdd_Dma_StopChannelTransfer

Std_ReturnType Cdd_Dma_StopChannelTransfer(
    uint8 ChannelId
)

Brief: Service to stop or disable a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which transfer shall be stopped

Returns:

  • E_OK Successfully disabled the DMA channel

  • E_NOT_OK Failed to disable the DMA channel

Return: Status of stoping the DMA channel

Precondition: None

Postcondition: None

7.12.4.18. function Cdd_Dma_ForcePeripheralEventTrigger

Std_ReturnType Cdd_Dma_ForcePeripheralEventTrigger(
    uint8 ChannelId
)

Brief: Service to force the peripheral event trigger for the channel.

Parameters:

  • ChannelId : Symbolic name of the DMA channel for which trigger shall be forced

Returns:

  • E_OK Successfully forced trigger for the DMA channel

  • E_NOT_OK Failed to force trigger for the DMA channel

Return: Status of forcing DMA channel trigger

Precondition: None

Postcondition: None

7.12.4.19. function Cdd_Dma_ClearPeripheralEventTrigger

Std_ReturnType Cdd_Dma_ClearPeripheralEventTrigger(
    uint8 ChannelId
)

Brief: Service to clear the peripheral event trigger for the channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which trigger shall be cleared

Returns:

  • E_OK Successfully cleared trigger for the DMA channel

  • E_NOT_OK Failed to clear trigger for the DMA channel

Return: Status of clearing DMA channel trigger

Precondition: None

Postcondition: None

7.12.4.20. function Cdd_Dma_TriggerSoftReset

Std_ReturnType Cdd_Dma_TriggerSoftReset(
    uint8 ChannelId
)

Brief: Service to trigger a soft reset for the channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which for which soft trigger shall be triggered

Returns:

  • E_OK Successfully triggered soft reset for the DMA channel

  • E_NOT_OK Failed to trigger soft reset for the DMA channel

Return: Status of trigerring soft reset

Precondition: None

Postcondition: None

7.12.4.21. function Cdd_Dma_SetChannelPriority

Std_ReturnType Cdd_Dma_SetChannelPriority(
    uint8 ChannelId,
    Cdd_Dma_ChannelPriority Priority
)

Brief: Service to set channel priority.

Parameters:

  • ChannelId : Symbolic name of the channel for which priority shall be set

  • Priority : Channel priority to be assigned

Returns:

  • E_OK Successfully set channel priority for the DMA channel

  • E_NOT_OK Failed to set channel priority for the DMA channel

Return: Status of setting channel priority

Precondition: None

Postcondition: None

7.12.4.22. function Cdd_Dma_GetChannelPriority

Std_ReturnType Cdd_Dma_GetChannelPriority(
    uint8 ChannelId,
    Cdd_Dma_ChannelPriority * Priority
)

Brief: Service to get channel priority.

Parameters:

  • ChannelId : Symbolic name of the channel for which priority shall be read

  • Priority : Pointer to memory location where the channel priority will be stored

Returns:

  • E_OK Successfully read channel priority

  • E_NOT_OK Failed to read channel priority

Return: Status of reading channel priority

Precondition: None

Postcondition: None

7.12.4.23. function Cdd_Dma_GetChannelStatus

void Cdd_Dma_GetChannelStatus(
    uint8 ChannelId,
    Cdd_Dma_ChannelStatus * ChannelStatus
)

Brief: Service to get the channel status : peripheral event trigger status, transfer status, burst status, run status and overflow status.

Parameters:

  • ChannelId : Symbolic name of the channel for which the status shall be read

  • ChannelStatus : Pointer to the structure of type Cdd_Dma_ChannelStatus where the channel status will be copied

Return: None

Precondition: None

Postcondition: None

7.12.4.24. function Cdd_Dma_ClearErrorFlag

Std_ReturnType Cdd_Dma_ClearErrorFlag(
    uint8 ChannelId
)

Brief: Service to clear the overflow error flag for a DMA channel.

Parameters:

  • ChannelId : Symbolic name of the channel for which the overflow error needs to be cleared

Returns:

  • E_OK Successfully cleared overflow error flag

  • E_NOT_OK Failed to clear overflow error flag

Return: Status of clearing the overflow error flag

Precondition: None

Postcondition: None

7.12.4.25. function Cdd_Dma_SetDmaCfgCommit

Std_ReturnType Cdd_Dma_SetDmaCfgCommit(
    uint8 HwInstanceId
)

Brief: Service to commit DMA configurable properties such as priority scheme, channel priority and emulation mode for a specific instance.

Parameters:

  • HwInstanceId Symbolic name of the DMA hardware instance

Returns:

  • E_OK Successfully commited DMA configurations

  • E_NOT_OK Failed to commit DMA configurations

Return: Status of commiting DMA configurations

Precondition: None

Postcondition: None

7.12.4.26. function Cdd_Dma_SetChannelCommit

Std_ReturnType Cdd_Dma_SetChannelCommit(
    uint8 ChannelId
)

Brief: Service to commit DMA channel configurations for a specific channel.

Parameters:

  • ChannelId Symbolic name of the DMA channel

Returns:

  • E_OK Successfully commited DMA channel configurations

  • E_NOT_OK Failed to commit DMA channel configurations

Return: Status of commiting DMA channel configurations

Precondition: None

Postcondition: None

7.12.4.27. function Cdd_Dma_SetMpuCfgCommit

Std_ReturnType Cdd_Dma_SetMpuCfgCommit(
    uint8 HwInstanceId
)

Brief: Service to commit Mpu configuration: MPUEN for a specific instance.

Parameters:

  • HwInstanceId Symbolic name of the DMA hardware instance

Returns:

  • E_OK Successfully commited Mpu configuration

  • E_NOT_OK Failed to commit Mpu configuration

Return: Status of commiting Mpu configuration

Precondition: None

Postcondition: None

7.12.4.28. function Cdd_Dma_SetMpuRegionCommit

Std_ReturnType Cdd_Dma_SetMpuRegionCommit(
    uint16 MpuRegionId
)

Brief: Service to commit Mpu Region configurations for a specific MPU region.

Parameters:

  • MpuRegionId Symbolic name of the DMA MPU region

Returns:

  • E_OK Successfully commited Mpu Region configuration

  • E_NOT_OK Failed to commit Mpu Region configuration

Return: Status of commiting Mpu Region configuration

Precondition: None

Postcondition: None

7.12.4.29. function Cdd_Dma_PeriodicReadback

void Cdd_Dma_PeriodicReadback(
    uint8 ChannelId,
    Cdd_Dma_PeriodicReadBackDataType * ReadBackRegisterdata
)

Brief: Service to read all the statically configured registers for periodic readback.

Parameters:

  • ChannelId Symbolic name of the DMA channel

  • ReadBackRegisterdata Pointer to the read back registers structure

Returns:

  • None

Return: None

Precondition: None

Postcondition: None