7.6. MCU

7.6.1. Types

Base type

Type Name

Brief

enum

Mcu_ASysCtlLockType

Bitmask type for ASysCtl LOCK register (ASYSCTL_O_LOCK).

enum

Mcu_PllStatusType

This is a status value returned by the function Mcu_GetPllStatus of the MCU module.

enum

Mcu_ResetType

This is the type of the reset enumerator containing the subset of reset types.

enum

Mcu_RamStateType

This is a status value returned by the function Mcu_GetRamState of the MCU module.

enum

Mcu_ClkSourceIdType

Type of the clock sources.

enum

Mcu_CpuTimerClkSrc

The following are clock sources available for Cpu Timer module.

enum

Mcu_MCanClkSrc

The following are clock sources available for MCAN module.

enum

Mcu_MCANClkDivider

The following are dividers available for MCAN module.

enum

Mcu_MCANInstance

The following are instances available for MCAN module.

enum

Mcu_ExternalClockOutClkSrc

The following are clock sources available for XCLKOUT module.

enum

Mcu_ExternalClockOutDiv

The following are dividers available for XCLKOUT.

enum

Mcu_EthercatClockDiv

The following are dividers available for Ethercat clock.

enum

Mcu_EthercatPhyClk

The following are values available to set enable/disable for EthcatPhyClock.

enum

Mcu_HsmClockDiv

The following are dividers available for HSM clock.

enum

Mcu_EPWMClkDivider

The following are dividers available for EPWM clock.

enum

Mcu_EMIFClkDivider

The following are dividers available for EMIF clock.

enum

Mcu_LINClkDivider

The following are dividers available for LIN clock.

enum

Mcu_LINInstance

The following are instances available for LIN module.

enum

Mcu_LowPowerModeType

List of low power modes.

enum

Mcu_ASysCtlTestNodeType

typedef uint8

Mcu_ClockType

This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock.

typedef uint32

Mcu_RawResetType

This type specifies the identification (ID) for a RAW reset status returned by Mcu_GetResetRawValue.

typedef uint8

Mcu_ModeType

This type specifies the identification (ID) for a MCU low power mode used in Mcu_SetMode.

typedef uint8

Mcu_RamSectionType

This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection.

typedef const Mcu_RamSectionConfigType *

Mcu_RamConfigPtrType

typedef const Mcu_PeripheralClkRegConfigType *

Mcu_PeripheralClkRegConfigPtrType

typedef const Mcu_PeripheralResetRegConfigType *

Mcu_PeripheralResetRegConfigPtrType

typedef const Mcu_MCanClkConfigType *

Mcu_MCanClkConfigPtrType

typedef const Mcu_LinClkConfigType *

Mcu_LinClkConfigPtrType

typedef const Mcu_ClockConfigType *

Mcu_ClockConfigPtrType

typedef const Mcu_ModeConfigType *

Mcu_ModeConfigPtrType

7.6.1.1. enum Mcu_ASysCtlLockType

Enumerator

Value

Description

MCU_ASYSCTL_LOCK_TSNSCTL

0x001U

Lock TSNSCTL register (Temperature Sensor Control)

MCU_ASYSCTL_LOCK_ANAREFCTL

0x002U

Lock ANAREFCTL register (Analog Reference Control)

MCU_ASYSCTL_LOCK_VMONCTL

0x004U

Lock VMONCTL register (Voltage Monitor Control)

MCU_ASYSCTL_LOCK_CMPHPMXSEL

0x020U

Lock CMPHPMXSEL register (CMPSS HP positive mux CMP1-CMP10)

MCU_ASYSCTL_LOCK_CMPLPMXSEL

0x040U

Lock CMPLPMXSEL register (CMPSS LP positive mux CMP1-CMP10)

MCU_ASYSCTL_LOCK_CMPHNMXSEL

0x080U

Lock CMPHNMXSEL register (CMPSS HN negative mux)

MCU_ASYSCTL_LOCK_CMPLNMXSEL

0x100U

Lock CMPLNMXSEL register (CMPSS LN negative mux)

MCU_ASYSCTL_LOCK_VREGCTL

0x200U

Lock VREGCTL register (Voltage Regulator Control)

MCU_ASYSCTL_LOCK_CMPHPMXSEL1

0x800U

Lock CMPHPMXSEL1 register (CMPSS HP positive mux CMP11-CMP12)

MCU_ASYSCTL_LOCK_CMPLPMXSEL1

0x1000U

Lock CMPLPMXSEL1 register (CMPSS LP positive mux CMP11-CMP12)

Brief: Bitmask type for ASysCtl LOCK register (ASYSCTL_O_LOCK).

Values can be OR-combined to lock multiple registers in a single call. Each bit corresponds to one register lock in the ASYSCTL_O_LOCK register.

Warning: These enum values MUST match the hardware register bit definitions in hw_asysctl.h (ASYSCTL_LOCK_*). The implementation relies on direct casting without bit translation to minimize cyclomatic complexity and meet HIS metrics requirements.

7.6.1.2. enum Mcu_PllStatusType

Enumerator

Value

Description

MCU_PLL_LOCKED

0U

PLL status Locked.

MCU_PLL_UNLOCKED

1U

PLL status Unlocked.

MCU_PLL_STATUS_UNDEFINED

2U

PLL status undefined.

Brief: This is a status value returned by the function Mcu_GetPllStatus of the MCU module.

7.6.1.3. enum Mcu_ResetType

Enumerator

Value

Description

MCU_POWER_ON_RESET

0U

Power On reset.

MCU_EXTERNAL_RESET

1U

External reset.

MCU_ESM_NMI_WATCHDOG_RESET

2U

NMI Watchdog reset.

MCU_WATCHDOG_RESET

3U

Watchdog reset

MCU_SW_RESET

4U

Simulation of external reset

MCU_ESM_RESET

5U

ESM reset

MCU_RESET_UNDEFINED

6U

UNDEFINED reset

Brief: This is the type of the reset enumerator containing the subset of reset types.

7.6.1.4. enum Mcu_RamStateType

Enumerator

Value

Description

MCU_RAMSTATE_INVALID

0U

Ram state status invalid

MCU_RAMSTATE_VALID

1U

Ram state status valid

Brief: This is a status value returned by the function Mcu_GetRamState of the MCU module.

7.6.1.5. enum Mcu_ClkSourceIdType

Enumerator

Value

Description

MCU_CLKSRC_OSC2

0x00

Internal Oscillator 2

MCU_CLKSRC_XTAL

0x01

External XTAL

MCU_CLKSRC_XTAL_SE

0x11

External XTAL Single-ended mode

MCU_CLKSRC_OSC1

0x02

Internal Oscillator 1

Brief: Type of the clock sources.

7.6.1.6. enum Mcu_CpuTimerClkSrc

Enumerator

Value

Description

MCU_CPUTIMERCLKSRC_SYSCLK

0U

SYSCLK (default on reset)

MCU_CPUTIMERCLKSRC_INTOSC1

1U

Internal Oscillator 1

MCU_CPUTIMERCLKSRC_INTOSC2

2U

Internal Oscillator 2

MCU_CPUTIMERCLKSRC_XTAL

3U

External Oscillator (XTAL)

MCU_CPUTIMERCLKSRC_MAX

Brief: The following are clock sources available for Cpu Timer module.

7.6.1.7. enum Mcu_MCanClkSrc

Enumerator

Value

Description

MCU_MCANCLKSRC_PERxSYSCLK

0U

SYSCLK (default on reset)

MCU_MCANCLKSRC_AUXCLKIN

2U

SYSCLK (default on reset)

MCU_MCANCLKSRC_PLLRAWCLK

3U

Raw PLL Clock

MCU_MCANCLKSRC_MAX

Brief: The following are clock sources available for MCAN module.

7.6.1.8. enum Mcu_MCANClkDivider

Enumerator

Value

Description

MCU_MCANCLK_DIV_1

0x0

MCAN clock = MCAN clock source / 1.

MCU_MCANCLK_DIV_2

0x1

MCAN clock = MCAN clock source / 2.

MCU_MCANCLK_DIV_3

0x2

MCAN clock = MCAN clock source / 3.

MCU_MCANCLK_DIV_4

0x3

MCAN clock = MCAN clock source / 4.

MCU_MCANCLK_DIV_5

0x4

MCAN clock = MCAN clock source / 5.

MCU_MCANCLK_DIV_6

0x5

MCAN clock = MCAN clock source / 6.

MCU_MCANCLK_DIV_7

0x6

MCAN clock = MCAN clock source / 7.

MCU_MCANCLK_DIV_8

0x7

MCAN clock = MCAN clock source / 8.

MCU_MCANCLK_DIV_9

0x8

MCAN clock = MCAN clock source / 9.

MCU_MCANCLK_DIV_10

0x9

MCAN clock = MCAN clock source / 10.

MCU_MCANCLK_DIV_11

0xA

MCAN clock = MCAN clock source / 11.

MCU_MCANCLK_DIV_12

0xB

MCAN clock = MCAN clock source / 12.

MCU_MCANCLK_DIV_13

0xC

MCAN clock = MCAN clock source / 13.

MCU_MCANCLK_DIV_14

0xD

MCAN clock = MCAN clock source / 14.

MCU_MCANCLK_DIV_15

0xE

MCAN clock = MCAN clock source / 15.

MCU_MCANCLK_DIV_16

0xF

MCAN clock = MCAN clock source / 16.

MCU_MCANCLK_DIV_17

0x10

MCAN clock = MCAN clock source / 17.

MCU_MCANCLK_DIV_18

0x11

MCAN clock = MCAN clock source / 18.

MCU_MCANCLK_DIV_19

0x12

MCAN clock = MCAN clock source / 19.

MCU_MCANCLK_DIV_20

0x13

MCAN clock = MCAN clock source / 20.

Brief: The following are dividers available for MCAN module.

7.6.1.9. enum Mcu_MCANInstance

Enumerator

Value

Description

MCU_MCAN_A

0U

MCAN Instance A.

MCU_MCAN_B

1U

MCAN Instance B.

MCU_MCAN_C

2U

MCAN Instance C.

MCU_MCAN_D

3U

MCAN Instance D.

MCU_MCAN_E

4U

MCAN Instance E.

MCU_MCAN_F

5U

MCAN Instance F.

Brief: The following are instances available for MCAN module.

7.6.1.10. enum Mcu_ExternalClockOutClkSrc

Enumerator

Value

Description

MCU_XCLKOUTSRC_PLLSYS

0U

PLL System Clock post SYSCLKDIV

MCU_XCLKOUTSRC_CPU1CLK

1U

CPU1.CLOCK

MCU_XCLKOUTSRC_CPU2CLK

2U

CPU2.CLOCK

MCU_XCLKOUTSRC_CPU3CLK

3U

CPU3.CLOCK

MCU_XCLKOUTSRC_INTOSC1

5U

Internal Oscillator 1

MCU_XCLKOUTSRC_INTOSC2

6U

Internal Oscillator 2

MCU_XCLKOUTSRC_XTALOSC

7U

External Oscillator

Brief: The following are clock sources available for XCLKOUT module.

7.6.1.11. enum Mcu_ExternalClockOutDiv

Enumerator

Value

Description

MCU_XCLKOUT_DIV_1

0U

divided by 1

MCU_XCLKOUT_DIV_2

1U

divided by 2

MCU_XCLKOUT_DIV_4

2U

divided by 4

MCU_XCLKOUT_DIV_8

3U

divided by 8

Brief: The following are dividers available for XCLKOUT.

7.6.1.12. enum Mcu_EthercatClockDiv

Enumerator

Value

Description

MCU_ECATCLKOUT_DIV_1

0U

divided by 1

MCU_ECATCLKOUT_DIV_2

1U

divided by 2

MCU_ECATCLKOUT_DIV_3

2U

divided by 3

MCU_ECATCLKOUT_DIV_4

3U

divided by 4

MCU_ECATCLKOUT_DIV_5

4U

divided by 5

MCU_ECATCLKOUT_DIV_6

5U

divided by 6

MCU_ECATCLKOUT_DIV_7

6U

divided by 7

MCU_ECATCLKOUT_DIV_8

7U

divided by 8

Brief: The following are dividers available for Ethercat clock.

7.6.1.13. enum Mcu_EthercatPhyClk

Enumerator

Value

Description

MCU_ECAT_PHYCLK_ENABLE

0x100U

Enable value 0x100.

MCU_ECAT_PHYCLK_DISABLE

0U

Disable value 0.

Brief: The following are values available to set enable/disable for EthcatPhyClock.

7.6.1.14. enum Mcu_HsmClockDiv

Enumerator

Value

Description

MCU_HSMCLK_DIV_1

0U

divided by 1

MCU_HSMCLK_DIV_2

1U

divided by 2

MCU_HSMCLK_DIV_4

2U

divided by 4

MCU_HSMCLK_DIV_8

3U

divided by 8

MCU_HSMCLK_DIV_16

4U

divided by 16

Brief: The following are dividers available for HSM clock.

7.6.1.15. enum Mcu_EPWMClkDivider

Enumerator

Value

Description

MCU_EPWMCLK_DIV_1

0U

EPWMCLK = PLLSYSCLK / 1.

MCU_EPWMCLK_DIV_2

1U

EPWMCLK = PLLSYSCLK / 2.

Brief: The following are dividers available for EPWM clock.

7.6.1.16. enum Mcu_EMIFClkDivider

Enumerator

Value

Description

MCU_EMIFCLK_DIV_1

0U

EMIF1CLK = PLLSYSCLK / 1.

MCU_EMIFCLK_DIV_2

1U

EMIF1CLK = PLLSYSCLK / 2.

MCU_EMIFCLK_DIV_4

2U

EMIF1CLK = PLLSYSCLK / 4.

Brief: The following are dividers available for EMIF clock.

7.6.1.17. enum Mcu_LINClkDivider

Enumerator

Value

Description

MCU_LINCLK_DIV_1

0U

LINCLK = PLLSYSCLK / 1.

MCU_LINCLK_DIV_2

1U

LINCLK = PLLSYSCLK / 2.

MCU_LINCLK_DIV_4

2U

LINCLK = PLLSYSCLK / 4.

Brief: The following are dividers available for LIN clock.

7.6.1.18. enum Mcu_LINInstance

Enumerator

Value

Description

MCU_LIN_A

0U

LIN Instance A.

MCU_LIN_B

1U

LIN Instance B.

Brief: The following are instances available for LIN module.

7.6.1.19. enum Mcu_LowPowerModeType

Enumerator

Value

Description

MCU_IDLE_MODE

0U

MCU Idle mode.

MCU_STANDBY_MODE

1U

MCU Standby mode.

MCU_MODE_MAX

Brief: List of low power modes.

7.6.1.20. enum Mcu_ASysCtlTestNodeType

Enumerator

Value

Description

MCU_ASYSCTL_TEST_NODE_NO_CONN

0U

No test node connected (reset default)

MCU_ASYSCTL_TEST_NODE_VDDCORE

1U

VDDCORE supply rail

MCU_ASYSCTL_TEST_NODE_VDDA

2U

VDDA analog supply

MCU_ASYSCTL_TEST_NODE_VSSA

3U

VSSA analog ground

MCU_ASYSCTL_TEST_NODE_VREFLOA

4U

VREFLO for ADC-A

MCU_ASYSCTL_TEST_NODE_VREFLOB

5U

VREFLO for ADC-B

MCU_ASYSCTL_TEST_NODE_CDAC1H

7U

CDAC1 high output

MCU_ASYSCTL_TEST_NODE_CDAC1L

8U

CDAC1 low output

MCU_ASYSCTL_TEST_NODE_CDAC2H

9U

CDAC2 high output

MCU_ASYSCTL_TEST_NODE_CDAC2L

10U

CDAC2 low output

MCU_ASYSCTL_TEST_NODE_CDAC3H

11U

CDAC3 high output

MCU_ASYSCTL_TEST_NODE_CDAC3L

12U

CDAC3 low output

MCU_ASYSCTL_TEST_NODE_CDAC4H

13U

CDAC4 high output

MCU_ASYSCTL_TEST_NODE_CDAC4L

14U

CDAC4 low output

MCU_ASYSCTL_TEST_NODE_CDAC5H

15U

CDAC5 high output

MCU_ASYSCTL_TEST_NODE_CDAC5L

16U

CDAC5 low output

MCU_ASYSCTL_TEST_NODE_CDAC6H

17U

CDAC6 high output

MCU_ASYSCTL_TEST_NODE_CDAC6L

18U

CDAC6 low output

MCU_ASYSCTL_TEST_NODE_CDAC7H

19U

CDAC7 high output

MCU_ASYSCTL_TEST_NODE_CDAC7L

20U

CDAC7 low output

MCU_ASYSCTL_TEST_NODE_CDAC8H

21U

CDAC8 high output

MCU_ASYSCTL_TEST_NODE_CDAC8L

22U

CDAC8 low output

MCU_ASYSCTL_TEST_NODE_CDAC9H

23U

CDAC9 high output

MCU_ASYSCTL_TEST_NODE_CDAC9L

24U

CDAC9 low output

MCU_ASYSCTL_TEST_NODE_CDAC10H

25U

CDAC10 high output

MCU_ASYSCTL_TEST_NODE_CDAC10L

26U

CDAC10 low output

MCU_ASYSCTL_TEST_NODE_CDAC11H

27U

CDAC11 high output

MCU_ASYSCTL_TEST_NODE_CDAC11L

28U

CDAC11 low output

MCU_ASYSCTL_TEST_NODE_ENZ_CALIB_GAIN_3P3

29U

Enable calibration gain 3.3V

MCU_ASYSCTL_TEST_NODE_MAX

Sentinel — not a valid node

7.6.1.21. typedef Mcu_ClockType

typedef uint8 Mcu_ClockType;

Brief: This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock.

7.6.1.22. typedef Mcu_RawResetType

typedef uint32 Mcu_RawResetType;

Brief: This type specifies the identification (ID) for a RAW reset status returned by Mcu_GetResetRawValue.

7.6.1.23. typedef Mcu_ModeType

typedef uint8 Mcu_ModeType;

Brief: This type specifies the identification (ID) for a MCU low power mode used in Mcu_SetMode.

7.6.1.24. typedef Mcu_RamSectionType

typedef uint8 Mcu_RamSectionType;

Brief: This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection.

7.6.1.25. typedef Mcu_RamConfigPtrType

typedef const Mcu_RamSectionConfigType* Mcu_RamConfigPtrType;

7.6.1.26. typedef Mcu_PeripheralClkRegConfigPtrType

typedef const Mcu_PeripheralClkRegConfigType* Mcu_PeripheralClkRegConfigPtrType;

7.6.1.27. typedef Mcu_PeripheralResetRegConfigPtrType

typedef const Mcu_PeripheralResetRegConfigType* Mcu_PeripheralResetRegConfigPtrType;

7.6.1.28. typedef Mcu_MCanClkConfigPtrType

typedef const Mcu_MCanClkConfigType* Mcu_MCanClkConfigPtrType;

7.6.1.29. typedef Mcu_LinClkConfigPtrType

typedef const Mcu_LinClkConfigType* Mcu_LinClkConfigPtrType;

7.6.1.30. typedef Mcu_ClockConfigPtrType

typedef const Mcu_ClockConfigType* Mcu_ClockConfigPtrType;

7.6.1.31. typedef Mcu_ModeConfigPtrType

typedef const Mcu_ModeConfigType* Mcu_ModeConfigPtrType;

7.6.2. Structures

Name

Brief

Mcu_ConfigType

MCU CONFIG ROOT structure.

Mcu_RamSectionConfigType

Structure for data pre-setting to be initialized.

Mcu_LinClkConfigType

Structure for LIN clock register setting.

Mcu_EthercatClkConfigType

Structure for EtherCat clock setting.

Mcu_MCanClkConfigType

Structure for MCAN clock register setting.

Mcu_CpuTimerClkConfigType

Structure for Cpu Timer clock register setting.

Mcu_ExternalClkOutConfigType

Structure for External Clock Output setting.

Mcu_PeripheralClkRegConfigType

Structure for peripheral clock register setting.

Mcu_PeripheralResetRegConfigType

Structure for peripheral Reset register setting.

Mcu_ClockConfigType

Structure for device clock setting.

Mcu_ModeConfigType

Structure for Mcu low power mode configuration type.

Mcu_PeripheralRegEntryType

Single peripheral configuration register entry.

Mcu_PeripheralConfigType

Peripheral configuration type containing register entries.

Mcu_ASysCtlConfigType

Mcu_CMPSSASysCtlConfigType

7.6.3. Defines

Name

Brief

MCU_SW_MAJOR_VERSION

Driver Implementation Major Version.

MCU_SW_MINOR_VERSION

Driver Implementation Minor Version.

MCU_SW_PATCH_VERSION

Driver Implementation Patch Version.

MCU_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by MCU Driver.

MCU_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by MCU Driver.

MCU_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by MCU Driver.

MCU_VENDOR_ID

Texas Instruments Vendor ID.

MCU_MODULE_ID

MCU Driver Module ID.

MCU_INSTANCE_ID

MCU Instance ID.

MCU_SID_INIT

Service ID for Mcu_Init.

MCU_SID_INIT_RAMSECTION

Service ID for Mcu_InitRamSection.

MCU_SID_INIT_CLOCK

Service ID for Mcu_InitClock.

MCU_SID_DISTRIBUTE_PLL_CLOCK

Service ID for Mcu_DistributePllClock.

MCU_SID_GET_PLL_STATUS

Service ID for Mcu_GetPllStatus.

MCU_SID_GET_RESET_REASON

Service ID for Mcu_GetResetReason.

MCU_SID_GET_RESET_RAW_VALUE

Service ID for Mcu_GetResetRawValue.

MCU_SID_PERFORM_RESET

Service ID for Mcu_PerformReset.

MCU_SID_SET_MODE

Service ID for Mcu_SetMode.

MCU_SID_GET_VERSION_INFO

Service ID for Mcu_GetVersionInfo.

MCU_SID_GET_RAM_STATE

Service ID for Mcu_GetRamState.

MCU_SID_GET_SYS_CLOCK

Service ID for Mcu_GetSystemClock.

MCU_SID_ASY_SELECT_INTERNAL_TEST_NODE

Service ID for Mcu_ASysCtl_SelectInternalTestNode.

MCU_SID_ASY_CONFIG_ADC_GLOBAL_SOC

Service ID for Mcu_ASysCtl_ConfigADCGlobalSOC.

MCU_SID_ASY_FORCE_ADC_GLOBAL_SOC

Service ID for Mcu_ASysCtl_ForceADCGlobalSOC.

MCU_SID_ASYSCTL_COMMIT_LOCK

Service ID for Mcu_ASysCtl_CommitLock.

MCU_SID_SYSCTL_CONFIG_EPWMXLINK

Service ID for Mcu_SysCtl_ConfigEPWMXLink.

MCU_E_PARAM_CONFIG

Mcu_Init config param invalid.

MCU_E_PARAM_CLOCK

Mcu_InitClock clockid param invalid.

MCU_E_PARAM_MODE

Mcu_SetMode modeid param invalid.

MCU_E_PARAM_RAMSECTION

Mcu_InitRamSection ramSect param invalid.

MCU_E_PLL_NOT_LOCKED

PLL not locked.

MCU_E_UNINIT

API invoked without performing Mcu_Init.

MCU_E_PARAM_POINTER

NULL_PTR passed to MCU driver APIs.

MCU_E_INIT_FAILED

Mcu Initialization failed.

MCU_E_UNINIT_CLOCK

API invoked without performing Mcu_InitClock.

MCU_E_PARAM_TESTNODE

Invalid test node value passed to Mcu_ASysCtl_SelectInternalTestNode.

MCU_E_ALREADY_LOCKED

Error code: Mcu_ASysCtl_CommitLock() called with lock bits that are already committed.

MCU_ERRORRST_MASK

Define indicating invalid raw reset value.

7.6.4. Functions

Return type

Function Name

Brief

void

Mcu_GetVersionInfo(Std_VersionInfoType * versioninfo)

This service provides the version information of MCU module.

void

Mcu_Init(const Mcu_ConfigType * CfgPtr)

This service initializes the MCU driver.

Std_ReturnType

Mcu_InitRamSection(Mcu_RamSectionType RamSection)

This service initializes the RAM section wise with default values supplied in configuration set.

Std_ReturnType

Mcu_InitClock(Mcu_ClockType ClockSetting)

This service initializes the PLL and other MCU specific clock options.

Mcu_PllStatusType

Mcu_GetPllStatus(void )

This service provides the lock status of the PLL.

uint32

Mcu_GetSystemClock(void )

This service provides the system clock.

Mcu_ResetType

Mcu_GetResetReason(void )

The service reads the reset reason from the hardware.

Mcu_RawResetType

Mcu_GetResetRawValue(void )

The service reads the raw reset value from the hardware register.

void

Mcu_PerformReset(void )

The service performs a microcontroller reset.

void

Mcu_SetMode(Mcu_ModeType McuMode)

The service activates low power modes.

void

Mcu_ASysCtl_SelectInternalTestNode(Mcu_ASysCtlTestNodeType TestNode)

Selects the internal analog test node connected to the analog test bus.

void

Mcu_ASysCtl_ConfigADCGlobalSOC(uint32 BaseAddr, uint8 AdcSelect)

Configures the ADC Global SOC Force Select register (ADCSOCFRCGBSEL).

void

Mcu_ASysCtl_ForceADCGlobalSOC(uint32 BaseAddr, uint32 SocMask)

Forces the ADC Global SOC trigger register (ADCSOCFRCGB).

void

Mcu_SysCtl_ConfigEPWMXLink(uint32 EPWMXLinkMask)

Configures the EPWM XLINK feature by writing the EPWMXLINKCFG register.

void

Mcu_ASysCtl_CommitLock(Mcu_ASysCtlLockType LockMask)

Commits (locks) the specified ASysCtl registers.

Mcu_RamStateType

Mcu_GetRamState(void )

This service provides the actual status of the microcontroller Ram.

7.6.4.1. function Mcu_GetVersionInfo

void Mcu_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: This service provides the version information of MCU module.

Parameters:

  • versioninfo - Pointer to MCU driver version information.

Returns:

  • None

Return: None

Precondition: This API is available only if MCU_CFG_GET_VERSION_INFO_API is STD_ON

Postcondition: None

7.6.4.2. function Mcu_Init

void Mcu_Init(
    const Mcu_ConfigType * CfgPtr
)

Brief: This service initializes the MCU driver.

This API is used to configure MCU settings for PLL and clock. This API is used to configure RAM section settings and Power mode settings.

Parameters:

  • CfgPtr - Pointer to MCU driver configuration set.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

7.6.4.3. function Mcu_InitRamSection

Std_ReturnType Mcu_InitRamSection(
    Mcu_RamSectionType RamSection
)

Brief: This service initializes the RAM section wise with default values supplied in configuration set.

This service initializes the RAM section wise.

Parameters:

  • RamSection Selects RAM memory section provided in configuration set

Returns:

  • E_OK command has been accepted

  • E_NOT_OK command has not been accepted

Return: Std_ReturnType

Precondition: None

Postcondition: None

7.6.4.4. function Mcu_InitClock

Std_ReturnType Mcu_InitClock(
    Mcu_ClockType ClockSetting
)

Brief: This service initializes the PLL and other MCU specific clock options.

This API is used to initializate clock & PLL This API is used to Set CPU timer clock, XCLKOUT, Ethercat clock, Peripheral clocks, MCAN module clocks

Parameters:

  • ClockSetting Selects clock section details provided in configuration set

Returns:

  • E_OK command has been accepted.

  • E_NOT_OK command has not been accepted

Return: Std_ReturnType

Precondition: This API is available only if MCU_CFG_INIT_CLOCK_API is STD_ON

Postcondition: None

7.6.4.5. function Mcu_GetPllStatus

Mcu_PllStatusType Mcu_GetPllStatus(
    void 
)

Brief: This service provides the lock status of the PLL.

Returns:

  • MCU_PLL_LOCKED PLL is in locked state. MCU_PLL_UNLOCKED: PLL is in unlocked state. MCU_PLL_STATUS_UNDEFINED: Pre-compile McuNoPll is set to true.

Return: Mcu_PllStatusType - PLL Status

Precondition: None

Postcondition: None

7.6.4.6. function Mcu_GetSystemClock

uint32 Mcu_GetSystemClock(
    void 
)

Brief: This service provides the system clock.

Returns:

  • PllSysclk

Return: Mcu_SysClk - System clock

Precondition: None

Postcondition: None

7.6.4.7. function Mcu_GetResetReason

Mcu_ResetType Mcu_GetResetReason(
    void 
)

Brief: The service reads the reset reason from the hardware.

This API reads the reset value from hardware and returns from the list of reset types defined in Mcu_ResetType.

Returns:

  • MCU_POWER_ON_RESET Power On reset

  • MCU_EXTERNAL_RESET External reset

  • MCU_ESM_NMI_WATCHDOG_RESET NMI Watchdog reset

  • MCU_WATCHDOG_RESET Watchdog reset

  • MCU_SW_RESET Simulation of external reset

  • MCU_ESM_RESET ESM reset

  • MCU_RESET_UNDEFINED UNDEFINED reset

Return: Mcu_ResetType - Reset Type

Precondition: None

Postcondition: None

7.6.4.8. function Mcu_GetResetRawValue

Mcu_RawResetType Mcu_GetResetRawValue(
    void 
)

Brief: The service reads the raw reset value from the hardware register.

This API reads the reset value from hardware and returns it.

Returns:

  • Reset raw value

Return: Mcu_RawResetType - Reset raw value

Precondition: None

Postcondition: None

7.6.4.9. function Mcu_PerformReset

void Mcu_PerformReset(
    void 
)

Brief: The service performs a microcontroller reset.

This API perform simulation of external reset only

Returns:

  • None

Return: None

Precondition: This API is available only if MCU_CFG_PERFORM_RESET_API is STD_ON

Postcondition: None

7.6.4.10. function Mcu_SetMode

void Mcu_SetMode(
    Mcu_ModeType McuMode
)

Brief: The service activates low power modes.

This API is used to activate the low power modes IDLE & STANDBY

Parameters:

  • McuMode - ID to select one MCU mode setting from the list provided in configuration set

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

7.6.4.11. function Mcu_ASysCtl_SelectInternalTestNode

void Mcu_ASysCtl_SelectInternalTestNode(
    Mcu_ASysCtlTestNodeType TestNode
)

Brief: Selects the internal analog test node connected to the analog test bus.

This API is used to set the internal test node in ASysCtl

Parameters:

  • TestNode Test node selection value.

Returns:

  • None

Return: None

Precondition: Mcu_Init() must have been called.

Postcondition: INTERNALTESTCTL.TESTSEL reflects the requested node.

7.6.4.12. function Mcu_ASysCtl_ConfigADCGlobalSOC

void Mcu_ASysCtl_ConfigADCGlobalSOC(
    uint32 BaseAddr,
    uint8 AdcSelect
)

Brief: Configures the ADC Global SOC Force Select register (ADCSOCFRCGBSEL).

Writes ADCSOCFRCGBSEL at the given base address with the ADC instance select mask, selecting which ADC instances participate in the global software trigger.

Parameters:

  • BaseAddr Base address of the ADC global register block

  • AdcSelect ADC instance selection mask (e.g. ASYSCTL_ADCSOCFRCGBSEL_ADCA, etc.)

Returns:

  • None

Return: None

Note: This API is a general-purpose ASysCtl service and is available unconditionally (not gated by a feature-specific compile switch). It is intended to be called by any module that requires ADC global SOC instance selection (e.g. Cdd_Adc when CDD_ADC_GLBSW_TRIG_API is STD_ON).

Precondition: Mcu_Init() must have been called.

Postcondition: ADCSOCFRCGBSEL register written with AdcSelect.

7.6.4.13. function Mcu_ASysCtl_ForceADCGlobalSOC

void Mcu_ASysCtl_ForceADCGlobalSOC(
    uint32 BaseAddr,
    uint32 SocMask
)

Brief: Forces the ADC Global SOC trigger register (ADCSOCFRCGB).

Writes ADCSOCFRCGB at the given base address with the SOC mask to simultaneously trigger the selected SOCs across all ADC instances configured via ADCSOCFRCGBSEL.

Parameters:

  • BaseAddr Base address of the ADC global register block

  • SocMask SOC trigger mask (one bit per SOC to trigger)

Returns:

  • None

Return: None

Note: This API is a general-purpose ASysCtl service and is available unconditionally (not gated by a feature-specific compile switch). It is intended to be called by any module that requires ADC global SOC force triggering (e.g. Cdd_Adc when CDD_ADC_GLBSW_TRIG_API is STD_ON).

Precondition: Mcu_Init() must have been called.

Postcondition: ADCSOCFRCGB register written with SocMask.

7.6.4.15. function Mcu_ASysCtl_CommitLock

void Mcu_ASysCtl_CommitLock(
    Mcu_ASysCtlLockType LockMask
)

Brief: Commits (locks) the specified ASysCtl registers.

This function applies the one-time write-lock to ASysCtl registers (ASYSCTL_O_LOCK) for the registers specified by LockMask. Lock bits are irreversible until system reset.

Values of Mcu_ASysCtlLockType can be OR-combined to lock multiple registers:

  • MCU_ASYSCTL_LOCK_TSNSCTL — Temperature Sensor Control

  • MCU_ASYSCTL_LOCK_ANAREFCTL — Analog Reference Control

  • MCU_ASYSCTL_LOCK_VMONCTL — Voltage Monitor Control

  • MCU_ASYSCTL_LOCK_CMPHPMXSEL — CMPSS HP positive mux (CMP1-CMP10)

  • MCU_ASYSCTL_LOCK_CMPLPMXSEL — CMPSS LP positive mux (CMP1-CMP10)

  • MCU_ASYSCTL_LOCK_CMPHNMXSEL — CMPSS HN negative mux

  • MCU_ASYSCTL_LOCK_CMPLNMXSEL — CMPSS LN negative mux

  • MCU_ASYSCTL_LOCK_VREGCTL — Voltage Regulator Control

  • MCU_ASYSCTL_LOCK_CMPHPMXSEL1 — CMPSS HP positive mux (CMP11-CMP12)

  • MCU_ASYSCTL_LOCK_CMPLPMXSEL1 — CMPSS LP positive mux (CMP11-CMP12)

Parameters:

  • LockMask Bitmask of Mcu_ASysCtlLockType values to lock

Returns:

  • None

Return: None

Precondition: Mcu_Init() must be called before calling this function.

Postcondition: Specified ASysCtl registers are locked until next system reset.

7.6.4.16. function Mcu_GetRamState

Mcu_RamStateType Mcu_GetRamState(
    void 
)

Brief: This service provides the actual status of the microcontroller Ram.

This API is not checking actual RAM status. So no actions are performed and returns RAM VALID

Returns:

  • MCU_RAMSTATE_INVALID Invalid Ram status

  • MCU_RAMSTATE_VALID Valid Ram status

Return: Mcu_RamStateType - Ram State Type

Precondition: This API is available only if MCU_CFG_GET_RAM_STATE_API is STD_ON

Postcondition: None