7.3. FLS
7.3.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
ENUM for erase type names. |
|
typedef uint32 |
Type of address type. |
|
typedef uint32 |
Type of length type. |
7.3.1.1. enum Fls_EraseType
Enumerator |
Value |
Description |
|---|---|---|
FLS_SECTOR_ERASE |
0U |
Erase sector. |
FLS_BANK_ERASE |
1U |
Erase bank. |
Brief: ENUM for erase type names.
7.3.1.2. typedef Fls_AddressType
typedef uint32 Fls_AddressType;
Brief: Type of address type.
7.3.1.3. typedef Fls_LengthType
typedef uint32 Fls_LengthType;
Brief: Type of length type.
7.3.2. Structures
Name |
Brief |
|---|---|
FLS Module Flashable Sectors and pages. |
|
7.3.3. Defines
Name |
Brief |
|---|---|
FLS_SW_MAJOR_VERSION |
Defines for FLS Driver version used for compatibility checks. |
FLS_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
FLS_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
FLS_AR_RELEASE_MAJOR_VERSION |
Defines for FLS Driver AUTOSAR version used for compatibility checks. |
FLS_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by FLS Driver. |
FLS_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by FLS Driver. |
FLS_VENDOR_ID |
FLS Driver ID Info. |
FLS_MODULE_ID |
FLS Driver Module ID. |
FLS_INSTANCE_ID |
FLS Driver Instance ID. |
FLS_WRITE_ADDRESS_ALIGNMENT |
|
FLS_E_PARAM_CONFIG |
Flash write address alignment. |
FLS_E_PARAM_ADDRESS |
API service called with wrong parameter. |
FLS_E_PARAM_LENGTH |
API service called with wrong parameter. |
FLS_E_PARAM_DATA |
API service called with wrong parameter. |
FLS_E_UNINIT |
API service used without module initialization. |
FLS_E_BUSY |
APIs called when module is busy. |
FLS_E_PARAM_POINTER |
APIs called with a Null Pointer. |
FLS_E_PARAM_ALIGNMENT |
API service called with wrong parameter. |
FLS_E_VERIFY_ERASE_FAILED |
Runtime Errors WITH HW. |
FLS_E_VERIFY_WRITE_FAILED |
APIs serice Write Verification (Compare) failed. |
FLS_E_TIMEOUT |
APIs Timeout Exceeded. |
FLS_E_ERASE_FAILED |
TRANSIENT FAULTS WITH HW. |
FLS_E_WRITE_FAILED |
Flash Write Failed in HW. |
FLS_E_READ_FAILED |
Flash Read Failed in HW. |
FLS_E_COMPARE_FAILED |
Flash Compare Failediin HW. |
FLS_E_UNEXPECTED_FLASH_ID |
Expected HW ID not matched. |
FLS_E_BLANK_CHECK_FAILED |
Flash Blank Check Failediin HW. |
FLS_SID_INIT |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error. |
FLS_SID_ERASE |
FLS_Erase() API Service ID. |
FLS_SID_WRITE |
FLS_Write() API Service ID. |
FLS_SID_CANCEL |
FLS_Cancel() API Service ID. |
FLS_SID_GET_STATUS |
FLS_GetStatus() API Service ID. |
FLS_SID_GET_JOB_RESULT |
Fls_GetJobResult() API Service ID. |
FLS_SID_READ |
FLS_Read() API Service ID. |
FLS_SID_COMPARE |
FLS_Compare() API Service ID. |
FLS_SID_SET_MODE |
FLS_SetMode() API Service ID. |
FLS_SID_GET_VERSION_INFO |
Fls_GetVersionInfo() API Service ID. |
FLS_SID_BLANK_CHECK |
FLS_BlankCheck() API Service ID. |
FLS_SID_MAIN_FUNCTION |
FLS_MainFunction() API Service ID. |
7.3.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Fls_Init(const Fls_ConfigType * ConfigPtr) |
Initializes the Flash Driver. |
Std_ReturnType |
Fls_Erase(Fls_AddressType TargetAddress, Fls_LengthType Length) |
Erases flash sector(s). |
Std_ReturnType |
Fls_Write(Fls_AddressType TargetAddress, const uint8 * SourceAddressPtr, Fls_LengthType Length) |
Writes one or more complete flash pages. |
Std_ReturnType |
Fls_Read(Fls_AddressType SourceAddress, uint8 * TargetAddressPtr, Fls_LengthType Length) |
Reads from flash memory. |
Std_ReturnType |
Fls_Compare(Fls_AddressType SourceAddress, const uint8 * TargetAddressPtr, Fls_LengthType Length) |
Compares the contents of an area of flash memory with that of an application data buffer. |
Std_ReturnType |
Fls_BlankCheck(Fls_AddressType TargetAddress, Fls_LengthType Length) |
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed. |
MemIf_StatusType |
Fls_GetStatus(void ) |
Returns the driver state. |
Std_ReturnType |
Fls_GetVersionInfo(Std_VersionInfoType * versioninfo) |
Returns the version information of this module. |
MemIf_JobResultType |
Fls_GetJobResult(void ) |
Returns the result of the last job. |
void |
Fls_MainFunction(void ) |
Performs the processing of jobs. |
void |
Fls_Cancel(void ) |
Cancels an ongoing job. |
void |
Fls_SetMode(MemIf_ModeType Mode) |
Sets the flash driver’s operation mode. This is a dummy API which is not supported and added for integration purposes. |
uint32 |
Fls_SetEraseType(Fls_EraseType erasetype) |
Sets the parameters required in application, based on the erase type parameter passed to this function while calling from Application. |
7.3.4.1. function Fls_Init
void Fls_Init(
const Fls_ConfigType * ConfigPtr
)
Brief: Initializes the Flash Driver.
Parameters:
ConfigPtr : Pointer to flash driver configuration set
Return: None
Precondition: None
Postcondition: None
7.3.4.2. function Fls_Erase
Std_ReturnType Fls_Erase(
Fls_AddressType TargetAddress,
Fls_LengthType Length
)
Brief: Erases flash sector(s).
Parameters:
TargetAddress Target address in flash memory. This address offset will be added to the flash memory base address.
Length - Number of bytes to erase
Returns:
E_OK erase command has been accepted
E_NOT_OK erase command has not been accepted
Return: return_value
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.3. function Fls_Write
Std_ReturnType Fls_Write(
Fls_AddressType TargetAddress,
const uint8 * SourceAddressPtr,
Fls_LengthType Length
)
Brief: Writes one or more complete flash pages.
Parameters:
TargetAddress Target address in flash memory. This address offset will be added to the flash memory base address.
SourceAddressPtr Pointer to source address
Length - Number of bytes to write
Returns:
E_OK write command has been accepted
E_NOT_OK write command has not been accepted
Return: Std_ReturnType
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.4. function Fls_Read
Std_ReturnType Fls_Read(
Fls_AddressType SourceAddress,
uint8 * TargetAddressPtr,
Fls_LengthType Length
)
Brief: Reads from flash memory.
Parameters:
SourceAddress Source address
Length - Number of bytes to read
TargetAddressPtr Pointer to target data buffer
Returns:
E_OK read command has been accepted
E_NOT_OK read command has not been accepted
Return: Std_ReturnType
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.5. function Fls_Compare
Std_ReturnType Fls_Compare(
Fls_AddressType SourceAddress,
const uint8 * TargetAddressPtr,
Fls_LengthType Length
)
Brief: Compares the contents of an area of flash memory with that of an application data buffer.
Parameters:
SourceAddress Target address in flash memory. This address offset will be added to the flash memory base address.
TargetAddressPtr Pointer to target data buffer
Length - Number of bytes to compare
Returns:
E_OK compare command has been accepted
E_NOT_OK compare command has not been accepted
Return: Std_ReturnType
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.6. function Fls_BlankCheck
Std_ReturnType Fls_BlankCheck(
Fls_AddressType TargetAddress,
Fls_LengthType Length
)
Brief: The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.
Parameters:
TargetAddress Address in flash memory from which the blank check should be started.
Length - Number of bytes to be checked for erase pattern
Returns:
E_OK request for blank checking has been accepted by the module
E_NOT_OK request for blank checking has not been accepted by the module
Return: Std_ReturnType
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.7. function Fls_GetStatus
MemIf_StatusType Fls_GetStatus(
void
)
Brief: Returns the driver state.
Return: MemIf_StatusType
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
7.3.4.8. function Fls_GetVersionInfo
Std_ReturnType Fls_GetVersionInfo(
Std_VersionInfoType * versioninfo
)
Brief: Returns the version information of this module.
Parameters:
versioninfo Pointer to where to store the version information of this module.
Return: None
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.4.9. function Fls_GetJobResult
MemIf_JobResultType Fls_GetJobResult(
void
)
Brief: Returns the result of the last job.
Return: MemIf_JobResultType
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.4.10. function Fls_MainFunction
void Fls_MainFunction(
void
)
Brief: Performs the processing of jobs.
Return: None
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.4.11. function Fls_Cancel
void Fls_Cancel(
void
)
Brief: Cancels an ongoing job.
Return: None
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.4.12. function Fls_SetMode
void Fls_SetMode(
MemIf_ModeType Mode
)
Brief: Sets the flash driver’s operation mode. This is a dummy API which is not supported and added for integration purposes.
Return: None
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.4.13. function Fls_SetEraseType
uint32 Fls_SetEraseType(
Fls_EraseType erasetype
)
Brief: Sets the parameters required in application, based on the erase type parameter passed to this function while calling from Application.
Parameters:
erasetype
Return: Sector or bank size
Precondition: Preconditions - None
Postcondition: Postconditions - None
7.3.5. Detailed Description
This files defines FLS MCAL configuration structures