5.13. CDD_IPC
5.13.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
CPU cores type. |
|
enum |
IPC Tx processing. |
|
enum |
IPC Instance type. |
|
typedef void(*)(const PduInfoType *PduInfoPtr) |
Notification callback function pointer. |
5.13.1.1. enum Cdd_Ipc_CoreType
Enumerator |
Value |
Description |
|---|---|---|
CDD_IPC_CPU1 |
0U |
CPU1. |
CDD_IPC_CPU2 |
1U |
CPU2. |
CDD_IPC_CPU3 |
2U |
CPU3. |
Brief: CPU cores type.
5.13.1.2. enum Cdd_Ipc_TxProcessingType
Enumerator |
Value |
Description |
|---|---|---|
CDD_IPC_POLLING |
1U |
Polling mode. |
CDD_IPC_INTERRUPT |
2U |
Interrupt mode. |
Brief: IPC Tx processing.
5.13.1.3. enum Cdd_Ipc_InstanceType
Enumerator |
Value |
Description |
|---|---|---|
CDD_IPC_CPU1_L_CPU2_R_INST0 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU2INTIPCSET(0U) |
CPU1 - Local core, CPU2 - Remote core, Instance 1. |
CDD_IPC_CPU1_L_CPU2_R_INST1 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU2INTIPCSET(1U) |
CPU1 - Local core, CPU2 - Remote core, Instance 2. |
CDD_IPC_CPU1_L_CPU2_R_INST2 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU2INTIPCSET(2U) |
CPU1 - Local core, CPU2 - Remote core, Instance 3. |
CDD_IPC_CPU1_L_CPU2_R_INST3 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU2INTIPCSET(3U) |
CPU1 - Local core, CPU2 - Remote core, Instance 4. |
CDD_IPC_CPU1_L_CPU3_R_INST0 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU3INTIPCSET(0U) |
CPU1 - Local core, CPU3 - Remote core, Instance 1. |
CDD_IPC_CPU1_L_CPU3_R_INST1 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU3INTIPCSET(1U) |
CPU1 - Local core, CPU3 - Remote core, Instance 2. |
CDD_IPC_CPU1_L_CPU3_R_INST2 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU3INTIPCSET(2U) |
CPU1 - Local core, CPU3 - Remote core, Instance 3. |
CDD_IPC_CPU1_L_CPU3_R_INST3 |
CPU1IPCSEND_BASE + IPC_O_CPU1TOCPU3INTIPCSET(3U) |
CPU1 - Local core, CPU3 - Remote core, Instance 4. |
CDD_IPC_CPU2_L_CPU1_R_INST0 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU1INTIPCSET(0U) |
CPU2 - Local core, CPU1 - Remote core, Instance 1. |
CDD_IPC_CPU2_L_CPU1_R_INST1 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU1INTIPCSET(1U) |
CPU2 - Local core, CPU1 - Remote core, Instance 2. |
CDD_IPC_CPU2_L_CPU1_R_INST2 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU1INTIPCSET(2U) |
CPU2 - Local core, CPU1 - Remote core, Instance 3. |
CDD_IPC_CPU2_L_CPU1_R_INST3 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU1INTIPCSET(3U) |
CPU2 - Local core, CPU1 - Remote core, Instance 4. |
CDD_IPC_CPU2_L_CPU3_R_INST0 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU3INTIPCSET(0U) |
CPU2 - Local core, CPU3 - Remote core, Instance 1. |
CDD_IPC_CPU2_L_CPU3_R_INST1 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU3INTIPCSET(1U) |
CPU2 - Local core, CPU3 - Remote core, Instance 2. |
CDD_IPC_CPU2_L_CPU3_R_INST2 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU3INTIPCSET(2U) |
CPU2 - Local core, CPU3 - Remote core, Instance 3. |
CDD_IPC_CPU2_L_CPU3_R_INST3 |
CPU2IPCSEND_BASE + IPC_O_CPU2TOCPU3INTIPCSET(3U) |
CPU2 - Local core, CPU3 - Remote core, Instance 4. |
CDD_IPC_CPU3_L_CPU1_R_INST0 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU1INTIPCSET(0U) |
CPU3 - Local core, CPU1 - Remote core, Instance 1. |
CDD_IPC_CPU3_L_CPU1_R_INST1 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU1INTIPCSET(1U) |
CPU3 - Local core, CPU1 - Remote core, Instance 2. |
CDD_IPC_CPU3_L_CPU1_R_INST2 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU1INTIPCSET(2U) |
CPU3 - Local core, CPU1 - Remote core, Instance 3. |
CDD_IPC_CPU3_L_CPU1_R_INST3 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU1INTIPCSET(3U) |
CPU3 - Local core, CPU1 - Remote core, Instance 4. |
CDD_IPC_CP3_L_CPU2_R_INST0 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU2INTIPCSET(0U) |
CPU3 - Local core, CPU2 - Remote core, Instance 1. |
CDD_IPC_CP3_L_CPU2_R_INST1 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU2INTIPCSET(1U) |
CPU3 - Local core, CPU2 - Remote core, Instance 2. |
CDD_IPC_CP3_L_CPU2_R_INST2 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU2INTIPCSET(2U) |
CPU3 - Local core, CPU2 - Remote core, Instance 3. |
CDD_IPC_CP3_L_CPU2_R_INST3 |
CPU3IPCSEND_BASE + IPC_O_CPU3TOCPU2INTIPCSET(3U) |
CPU3 - Local core, CPU2 - Remote core, Instance 4. |
Brief: IPC Instance type.
5.13.1.4. typedef Cdd_Ipc_NotifyType
typedef void(* Cdd_Ipc_NotifyType) (const PduInfoType *PduInfoPtr);
Brief: Notification callback function pointer.
5.13.2. Structures
Name |
Brief |
|---|---|
IPC Tx channel config type. |
|
IPC Tx instance config type. |
|
IPC Rx channel config type. |
|
IPC Rx instance config type. |
|
IPC config type. |
5.13.3. Defines
Name |
Brief |
|---|---|
CDD_IPC_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
CDD_IPC_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
CDD_IPC_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
CDD_IPC_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by CDD_IPC Driver. |
CDD_IPC_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by CDD_IPC Driver. |
CDD_IPC_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by CDD_IPC Driver. |
CDD_IPC_VENDOR_ID |
Texas Instruments Vendor ID. |
CDD_IPC_MODULE_ID |
CDD IPC Driver Module ID. |
CDD_IPC_INSTANCE_ID |
CDD IPC Instance ID. |
CDD_IPC_E_UNINIT |
API service used without module initialization. |
CDD_IPC_E_ALREADY_INITIALIZED |
API Cdd_Ipc_Init service called while the IPC driver has already been initialized. |
CDD_IPC_E_PARAM_VALUE |
API service called with invalid parameter value. |
CDD_IPC_E_PARAM_POINTER |
API service called with invalid data buffer pointer. |
CDD_IPC_E_INVALID_LENGTH |
API service called with invalid data length. |
CDD_IPC_SID_GET_VERSION_INFO |
Cdd_Ipc_GetVersionInfo() API Service ID. |
CDD_IPC_SID_INIT |
Cdd_Ipc_Init() API Service ID. |
CDD_IPC_SID_SYNC |
Cdd_Ipc_Sync() API Service ID. |
CDD_IPC_SID_TRANSMIT |
Cdd_Ipc_Transmit() API Service ID. |
CDD_IPC_SID_MAIN_FUNCTION_READ |
Cdd_Ipc_MainFunction_Read() API Service ID. |
CDD_IPC_IS_TX_INSTANCE_FREE |
Cdd_Ipc_IsTxInstanceFree() API Service ID. |
CDD_IPC_SID_GET_COUNTER |
Cdd_Ipc_GetCounter() API Service ID. |
BIT_MASK_EIGHT |
Bit mask for last 8 bits. |
BIT_MASK_FOUR |
Bit mask for last 4 bits. |
BIT_SHIFT_BY_8 |
Shift bits by 8 bits. |
5.13.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Cdd_Ipc_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr) |
Service to provide the version information of Cdd Ipc module. |
void |
Cdd_Ipc_Init(const Cdd_Ipc_ConfigType * ConfigPtr) |
Service to initialize CDD IPC driver. |
Std_ReturnType |
Cdd_Ipc_Sync(Cdd_Ipc_CoreType RemoteCore) |
Service to synchronise two cores communicating in IPC communication within a preconfigured timeout. |
Std_ReturnType |
Cdd_Ipc_Transmit(PduIdType ChannelId, const PduInfoType * PduInfoPtr) |
Service to request transmission. |
void |
Cdd_Ipc_MainFunction_Read(void ) |
Service to perform the polling of confgured IPC Rx instances. |
boolean |
Cdd_Ipc_IsTxInstanceFree(PduIdType ChannelId) |
Service to check the status of the instance that is configured for transmitting the message in the respective channel. |
uint64 |
Cdd_Ipc_GetCounter(void ) |
Service to read the timestamp counter value. |
5.13.4.1. function Cdd_Ipc_GetVersionInfo
void Cdd_Ipc_GetVersionInfo(
Std_VersionInfoType * VersionInfoPtr
)
Brief: Service to provide the version information of Cdd Ipc module.
Parameters:
VersionInfoPtr is the pointer to CDD IPC driver version information.
Returns:
None
Return: None
Precondition: This API is available only if CDD_IPC_GET_VERSION_INFO_API is STD_ON
Postcondition: None
5.13.4.2. function Cdd_Ipc_Init
void Cdd_Ipc_Init(
const Cdd_Ipc_ConfigType * ConfigPtr
)
Brief: Service to initialize CDD IPC driver.
Parameters:
ConfigPtr is the configuration pointer pointing to a generated configuration variant from plugin
Return: None
Precondition: Preconditions - Driver not already initialized
Postcondition: Postconditions - Driver in initialized state
5.13.4.3. function Cdd_Ipc_Sync
Std_ReturnType Cdd_Ipc_Sync(
Cdd_Ipc_CoreType RemoteCore
)
Brief: Service to synchronise two cores communicating in IPC communication within a preconfigured timeout.
Parameters:
RemoteCore is the symbolic name of the remote core that needs to be synchronized with.
Returns:
E_OK Synchronization is successful.
E_NOT_OK Synchronization failed.
Return: Status of synchronization.
Precondition: None
Postcondition: None
5.13.4.4. function Cdd_Ipc_Transmit
Std_ReturnType Cdd_Ipc_Transmit(
PduIdType ChannelId,
const PduInfoType * PduInfoPtr
)
Brief: Service to request transmission.
Parameters:
ChannelId : When Cdd Ipc is integrated with Autosar Com stack, this parameter is a Pdu identifier used to address the respective channel. When Cdd Ipc is not integrated with Autosar Com stack, this parameter is a channel identifier used to address the respective channel.
PduInfoPtr is the pointer to a struct of type PduInfoType containing the complete data to be transmitted.
Returns:
E_OK Transmit request has been accepted.
E_NOT_OK Transmit request has not been accepted.
Return: Cdd_Ipc_Transmit request is accepted or not
Precondition: None
Postcondition: None
5.13.4.5. function Cdd_Ipc_MainFunction_Read
void Cdd_Ipc_MainFunction_Read(
void
)
Brief: Service to perform the polling of confgured IPC Rx instances.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.13.4.6. function Cdd_Ipc_IsTxInstanceFree
boolean Cdd_Ipc_IsTxInstanceFree(
PduIdType ChannelId
)
Brief: Service to check the status of the instance that is configured for transmitting the message in the respective channel.
Parameters:
ChannelId : When Cdd Ipc is integrated with Autosar Com stack, this parameter is a Pdu identifier used to address the respective channel. When Cdd Ipc is not integrated with Autosar Com stack, this parameter is a channel identifier used to address the respective channel.
Returns:
TRUE Instance is free
FALSE Instance is busy
Return: IPC instance configured for transmitting the PDU is busy or not
Precondition: None
Postcondition: None
5.13.4.7. function Cdd_Ipc_GetCounter
uint64 Cdd_Ipc_GetCounter(
void
)
Brief: Service to read the timestamp counter value.
Return: 64-bit timestamp counter value
Precondition: None
Postcondition: None