5.1. CAN

5.1.1. Types

Base type

Type Name

Brief

enum

Can_ProcessingType

Can Tx/Rx Processing.

enum

Can_ReturnType

Values that can be returned by CAN Driver APIs.

enum

Can_HandleType

Can Handle Type FULL/BASIC.

enum

Can_ControllerInstance

Can Controller Instance ID.

enum

Can_MailboxDirectionType

Can Mailbox direction enum.

enum

Can_Icom_signal_operation_type

Icom signal operation type.

enum

Can_DrvState

Can Driver state.

enum

Can_EventPin

Enum for the event pin.

enum

Can_StandardFilterType

Enum for the Can standard filter selection.

5.1.1.1. enum Can_ProcessingType

Enumerator

Value

Description

CAN_INTERRUPT

0x0U

Interrupt.

CAN_MIXED

0x1U

Mixed

CAN_POLLING

0x2U

Polling.

Brief: Can Tx/Rx Processing.

5.1.1.2. enum Can_ReturnType

Enumerator

Value

Description

CAN_BUSY

2U

Transmit request could not be processed because no transmit object was available.

Brief: Values that can be returned by CAN Driver APIs.

5.1.1.3. enum Can_HandleType

Enumerator

Value

Description

CAN_FULL

0x0U

Full

CAN_BASIC

Basic

Brief: Can Handle Type FULL/BASIC.

5.1.1.4. enum Can_ControllerInstance

Enumerator

Value

Description

CAN_CONTROLLER_INSTANCE_MCANA

0x0U

MCANA Controller Instance.

CAN_CONTROLLER_INSTANCE_MCANB

0x1U

MCANB Controller Instance.

CAN_CONTROLLER_INSTANCE_MCANC

0x2U

MCANC Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAND

0x3U

MCAND Controller Instance.

CAN_CONTROLLER_INSTANCE_MCANE

0x4U

MCANE Controller Instance.

CAN_CONTROLLER_INSTANCE_MCANF

0x5U

MCANF Controller Instance.

Brief: Can Controller Instance ID.

5.1.1.5. enum Can_MailboxDirectionType

Enumerator

Value

Description

CAN_RECEIVE

0x0U

Mailbox is for receive.

CAN_TRANSMIT

Mailbox is for transmit.

Brief: Can Mailbox direction enum.

5.1.1.6. enum Can_Icom_signal_operation_type

Enumerator

Value

Description

AND

0U

AND.

EQUAL

1U

EQUAL.

GREATER

2U

GREATER.

SMALLER

3U

SMALLER.

XOR

4U

XOR.

Brief: Icom signal operation type.

5.1.1.7. enum Can_DrvState

Enumerator

Value

Description

CAN_UNINIT

0U

Can module state when reset/power-up.

CAN_READY

1U

Can module state after initialization.

Brief: Can Driver state.

5.1.1.8. enum Can_EventPin

Enumerator

Value

Description

CAN_EVENT_PIN_0

0x0U

EVENT PIN0.

CAN_EVENT_PIN_1

0x1U

EVENT PIN1.

CAN_EVENT_PIN_NONE

0x2U

EVENT NONE.

Brief: Enum for the event pin.

5.1.1.9. enum Can_StandardFilterType

Enumerator

Value

Description

CAN_RANGE_FILTER

0x0U

Range filter from SFID1 to SFID2 (SFID2 ≥ SFID1)

CAN_DUAL_ID_FILTER

0x1U

Dual ID filter for SFID1 or SFID2.

CAN_CLASSIC_FILTER

0x2U

Classic filter: SFID1 = filter; SFID2 = mask.

CAN_FILTER_DISABLED

0x03

Filter element disabled.

Brief: Enum for the Can standard filter selection.

5.1.2. Structures

Name

Brief

Can_MainFunctionRWPeriodRefType

Can Main Function RW Period Ref Type Identifier.

Can_MaskType

Structure defining the filter mask to be used.

Can_CanConfigType

MCan Controller Specific Configuration.

Can_FdBaudConfigType

Structure defining the CAN FD data phase baud rate configuration.

Can_BaudConfigType

Can Controller Baud Rate Configuration definition.

Can_ControllerType

Can Controller Configuration definition.

Can_HwFilterType

Structure defining the HW filter to be used.

Can_MailboxType

Can mailbox configuration definition.

Can_IcomSignalConfigType

Icom signal config data structure.

Can_IcomRxMessageType

Icom Rx message data structure.

Can_IcomConfigType

Icom data structure containing the overall ICOM configuration data.

Can_ConfigType

External data structure containing the overall initialization data for the CAN driver and SFR settings affecting all controllers.

Can_PeriodicReadBackDataType

Can periodic readback register definition.

5.1.3. Defines

Name

Brief

CAN_SW_MAJOR_VERSION

Driver Implementation Major Version.

CAN_SW_MINOR_VERSION

Driver Implementation Minor Version.

CAN_SW_PATCH_VERSION

Driver Implementation Patch Version.

CAN_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CAN Driver.

CAN_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CAN Driver.

CAN_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CAN Driver.

CAN_VENDOR_ID

CAN Driver ID Info.

CAN_MODULE_ID

CAN Driver Module ID.

CAN_INSTANCE_ID

CAN Instance ID.

CAN_SID_INIT

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error.

CAN_SID_MAINFUNC_WRITE

Service ID - Can_MainFunction_Write().

CAN_SID_SETCTR

Service ID - Can_SetControllerMode().

CAN_SID_DIINT

Service ID - Can_DisableControllerInterrupts().

CAN_SID_ENINT

Service ID - Can_EnableControllerInterrupts().

CAN_SID_WRITE

Service ID - Can_Write().

CAN_SID_GET_VERSION_INFO

Service ID - Can_GetVersionInfo().

CAN_SID_MAINFUNC_READ

Service ID - Can_MainFunction_Read().

CAN_SID_MAINFUNC_BO

Service ID - Can_MainFunction_BusOff().

CAN_SID_MAINFUNC_WU

Service ID - Can_MainFunction_Wakeup().

CAN_SID_CKWAKEUP

Service ID - Can_CheckWakeup().

CAN_SID_MAINFUNC_MODE

Service ID - Can_MainFunction_Mode().

CAN_SID_CHNGBAUDRATE

Service ID - Can_ChangeBaudrate().

CAN_SID_CHKBAUDRATE

Service ID - Can_CheckBaudrate().

CAN_SID_SETBAUDRATE

Service ID - Can_SetBaudRate().

CAN_SID_DEINIT

Service ID - Can_DeInit().

CAN_SID_GETCNTRERRSTATE

Service ID - Can_GetControllerErrorState().

CAN_SID_GETCNTRMODE

Service ID - Can_GetControllerMode().

CAN_SID_PROCESSISR

Service ID - Can_ProcessISR().

CAN_SID_ICOMCONFIG

Service ID - Can_SetIcomConfiguration().

CAN_SID_READBACK

Service ID - Can_PeriodicReadback().

CAN_E_PARAM_POINTER

Error codes returned by Can functions - Development Errors.

CAN_E_PARAM_HANDLE

Invalid Controller Handle.

CAN_E_PARAM_DATA_LENGTH

Invalid length of msg.

CAN_E_PARAM_CONTROLLER

Invalid controller id.

CAN_E_UNINIT

Error due to API invoked without performing Can_Init().

CAN_E_TRANSITION

Error during Controller state transition.

CAN_E_PARAM_BAUDRATE

Invalid Baudrate configuration.

CAN_E_ICOM_CONFIG_INVALID

Invalid ICOM configuration Id.

CAN_E_DATALOST

Error codes returned by Can functions - Run Time Errors.

CAN_ICOM_CONFIG_DISABLE

Icom config disable.

CAN_EXTENDED_ID

Extended id.

CAN_STANDARD_ID

Standard id.

CAN_MIXED_ID

Mixed id.

5.1.4. Functions

Return type

Function Name

Brief

void

Can_GetVersionInfo(Std_VersionInfoType * versioninfo)

Function returns the version information of this module.

void

Can_Init(const Can_ConfigType * Config_Ptr)

This function initializes the configuration.

void

Can_DeInit(void )

This function deinitializes the module.

Std_ReturnType

Can_SetBaudrate(uint8 Controller, const uint16 BaudRateConfigID)

This service shall set the baud rate configuration of the CAN Controller.

Std_ReturnType

Can_SetControllerMode(uint8 Controller, Can_ControllerStateType Transition)

This service performs software triggered state transitions of the CAN controller State machine.

void

Can_DisableControllerInterrupts(uint8 Controller)

This service disables all interrupts.

void

Can_EnableControllerInterrupts(uint8 Controller)

This service enables all allowed interrupts.

Std_ReturnType

Can_CheckWakeup(uint8 Controller)

This service checks if a wakeup has occurred for the given controller.

Std_ReturnType

Can_GetControllerErrorState(uint8 Controller, Can_ErrorStateType * ErrorStatePtr)

This service obtains the error state of the CAN controller.

Std_ReturnType

Can_GetControllerMode(uint8 Controller, Can_ControllerStateType * ControllerModePtr)

This service reports about the current status of the requested CAN controller.

Std_ReturnType

Can_Write(Can_HwHandleType Hth, const Can_PduType * PduInfo)

This service is called by CanIf to pass a CAN message to CanDrv for transmission.

void

Can_MainFunction_Write(uint16 RWFuncID)

This service performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

void

Can_MainFunction_Read(uint16 RWFuncID)

This service performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

void

Can_MainFunction_BusOff(void )

This service performs the polling of bus-off events that are configured statically as ‘to be polled’.

void

Can_MainFunction_Wakeup(void )

This function performs the polling of wake-up events that are configured statically as ‘to be polled’.

void

Can_MainFunction_Mode(void )

This function performs the polling of CAN controller mode transitions.

Std_ReturnType

Can_SetIcomConfiguration(uint8 Controller, IcomConfigIdType ConfigurationId)

This service shall change the Icom Configuration of a CAN controller to the requested one.

void

Can_PeriodicReadback(uint8 Controller, Can_PeriodicReadBackDataType * ReadBackRegisterdata)

This service shall read all the statically configured registers.

5.1.4.1. function Can_GetVersionInfo

void Can_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: Function returns the version information of this module.

This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported.

Parameters:

  • versioninfo Pointer to where to store the version information of this module.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.2. function Can_Init

void Can_Init(
    const Can_ConfigType * Config_Ptr
)

Brief: This function initializes the configuration.

This function initializes the message RAM, which also clears all the message objects, and places the CAN controller in an init state. Write access to the configuration registers is available as a result, allowing the bit timing and message objects to be setup.

Parameters:

  • Config_Ptr Pointer to post-build configuration data.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.3. function Can_DeInit

void Can_DeInit(
    void 
)

Brief: This function deinitializes the module.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.4. function Can_SetBaudrate

Std_ReturnType Can_SetBaudrate(
    uint8 Controller,
    const uint16 BaudRateConfigID
)

Brief: This service shall set the baud rate configuration of the CAN Controller.

This function sets the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.

Parameters:

  • Controller CAN controller, whose baud rate shall be set.

  • BaudRateConfigID references a baud rate configuration by ID.

Returns:

  • E_OK - Service request accepted, setting of (new) baud rate started.

  • E_NOT_OK - Service request not accepted.

Return: Setting the Baudrate successful or failure.

Precondition: None

Postcondition: None

5.1.4.5. function Can_SetControllerMode

Std_ReturnType Can_SetControllerMode(
    uint8 Controller,
    Can_ControllerStateType Transition
)

Brief: This service performs software triggered state transitions of the CAN controller State machine.

The function perfroms the transition of the CAN controller state machine which is software triggered.

Parameters:

  • Controller CAN controller for which the status shall be changed.

  • Transition Transition value to request new CAN controller state.

Returns:

  • E_OK Request accepted.

  • E_NOT_OK Request not accepted i.e. an error occured while requesting an incorrect from one state to other or an incorrect transition.

Return: Setting the controller mode successful/failure.

Precondition: None

Postcondition: None

5.1.4.6. function Can_DisableControllerInterrupts

void Can_DisableControllerInterrupts(
    uint8 Controller
)

Brief: This service disables all interrupts.

This function checks if there is a DET Error and then disables all the interrupts for the controller.

Parameters:

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.7. function Can_EnableControllerInterrupts

void Can_EnableControllerInterrupts(
    uint8 Controller
)

Brief: This service enables all allowed interrupts.

This function checks the total number of interrupts and enables all the interrupts allowed for the controller.

Parameters:

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.8. function Can_CheckWakeup

Std_ReturnType Can_CheckWakeup(
    uint8 Controller
)

Brief: This service checks if a wakeup has occurred for the given controller.

This function checks if the Init is done and checks if wakeup has occured and returns value accordingly for the given controller.

Parameters:

  • Controller to be checked for a wakeup.

Returns:

  • E_OK API call has been accepted.

  • E_NOT_OK API call has not been accepted.

Return: Wakeup occurred or not for a controller

Precondition: None

Postcondition: None

5.1.4.9. function Can_GetControllerErrorState

Std_ReturnType Can_GetControllerErrorState(
    uint8 Controller,
    Can_ErrorStateType * ErrorStatePtr
)

Brief: This service obtains the error state of the CAN controller.

This function gets the error state of the CAN controller.

Parameters:

  • Controller CAN controller, which is requested for ErrorState.

  • ErrorStatePtr Pointer to a memory location, where the error state of the CAN controller will be stored.

Returns:

  • E_OK - Error state request has been accepted.

  • E_NOT_OK - Error state request has not been accepted..

Return: Error state obtained successfully/failed to obtain error state.

Precondition: None

Postcondition: None

5.1.4.10. function Can_GetControllerMode

Std_ReturnType Can_GetControllerMode(
    uint8 Controller,
    Can_ControllerStateType * ControllerModePtr
)

Brief: This service reports about the current status of the requested CAN controller.

This function gets the current status of the CAN controller.

Parameters:

  • Controller CAN controller, which is requested for ErrorState.

  • ControllerModePtr Pointer to a memory location, where the current mode of the CAN controller will be stored.

Returns:

  • E_OK - Controller mode request has been accepted.

  • E_NOT_OK - Controller mode request has not been accepted.

Return: Able/unable to fetch current status of the controller.

Precondition: None

Postcondition: None

5.1.4.11. function Can_Write

Std_ReturnType Can_Write(
    Can_HwHandleType Hth,
    const Can_PduType * PduInfo
)

Brief: This service is called by CanIf to pass a CAN message to CanDrv for transmission.

The function Can_Write first checks if the hardware transmit object is identified and is free. It passes the CAN message to CanDrv for transmission.

Parameters:

  • Hth information which HW-transmit handle shall be used for transmit. Implicitly this is also the information about the controller to use because the Hth numbers are unique inside one hardware unit.

  • PduInfo Pointer to SDU user memory, DLC and Identifier.

Returns:

  • E_OK Write command has been accepted.

  • E_NOT_OK Development error occurred.

  • CAN_BUSY No TX hardware buffer available or pre-emptive call of Can_Write that can’t be implemented re-entrant

Return: Can write command is accepted (or) resulted in an error (or) Controller is busy

Precondition: None

Postcondition: None

5.1.4.12. function Can_MainFunction_Write

void Can_MainFunction_Write(
    uint16 RWFuncID
)

Brief: This service performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. For a TX Mailbox if the controller is active polling of TX confirmation is done.

Parameters:

  • RWFuncID Read/Write period ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.13. function Can_MainFunction_Read

void Can_MainFunction_Read(
    uint16 RWFuncID
)

Brief: This service performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. For a Rx Mailbox if the controller is active polling of Rx indications is done.

Parameters:

  • RWFuncID Read/Write period ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.14. function Can_MainFunction_BusOff

void Can_MainFunction_BusOff(
    void 
)

Brief: This service performs the polling of bus-off events that are configured statically as ‘to be polled’.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. If the controller is active the polling of bus-off events that are configured statically as ‘to be polled’.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.15. function Can_MainFunction_Wakeup

void Can_MainFunction_Wakeup(
    void 
)

Brief: This function performs the polling of wake-up events that are configured statically as ‘to be polled’.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. The polling of wake-up events is done.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.16. function Can_MainFunction_Mode

void Can_MainFunction_Mode(
    void 
)

Brief: This function performs the polling of CAN controller mode transitions.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. The polling of CAN controller mode transitions is done.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.17. function Can_SetIcomConfiguration

Std_ReturnType Can_SetIcomConfiguration(
    uint8 Controller,
    IcomConfigIdType ConfigurationId
)

Brief: This service shall change the Icom Configuration of a CAN controller to the requested one.

Parameters:

  • Controller CAN controller for which the status shall be changed

  • ConfigurationId Requested Configuration

Returns:

  • E_OK CAN driver succeeded in setting a configuration with a valid Configuration id.

  • E_NOT_OK CAN driver failed to set a configuration with a valid Configuration id.

Return: Std_ReturnType

Precondition: None

Postcondition: None

5.1.4.18. function Can_PeriodicReadback

void Can_PeriodicReadback(
    uint8 Controller,
    Can_PeriodicReadBackDataType * ReadBackRegisterdata
)

Brief: This service shall read all the statically configured registers.

Parameters:

  • Controller CAN controller for which the configured registers shall be read

  • ReadBackRegisterdata pointer for the read back registers

Returns:

  • None

Return: None

Precondition: None

Postcondition: None