|
F29H85x-SDK
1.03.00.00
|
|
Introduction
Matrix multiply example
Watch Variables
External Connections
Steps to Run the Example
- When using CCS projects to build, import the CCS project and build it using the CCS project menu (see CCS Build Project).
- When using makefiles to build, note the required combination and build using make command (see Makefile based Build)
- Launch a CCS debug session and run the executable, see Build, Load and Run
- Pick the project build configuration, build and run the example
- It will print statements as it executes the example, along with Pass/Fail information and number of cycles