Introduction
This example demonstrates the usage of FreeRTOS binary semaphores. A timer interrupt is setup, which posts a binary sempahore. One task runs freely, while another task pends on the binary semaphore to begin execcution
Watch Variables
- Task1_count: # times Task 1 is executed
- Task2_count: # times Task 2 is executed
External Connections
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see CCS Build Project).
- Establish connections as mentioned in External Connections section.
- Launch a CCS debug session and run the executable, see Build, Load and Run
- Place breakpoints to verify task entry and execution