SYSCTL Module¶
System Control (SysCtl) determines the overall operation of the device. The API provides functions to configure the clocking of the device, the set of peripherals that are enabled, the windowed watchdog, the NMI watchdog, and low-power modes. It also provides functions to handle and obtain information about resets and missing clock detection failures.
-
group
sysctl_api
Defines
-
SYSCTL_WD_CHKBITS
0x0028U¶
-
SYSCTL_WD_ENRSTKEY
0x0055U¶
-
SYSCTL_WD_RSTKEY
0x00AAU¶
-
SYSCTL_PERIPH_REG_M
0x001FU¶
-
SYSCTL_PERIPH_REG_S
0x0000U¶
-
SYSCTL_PERIPH_BIT_M
0x1F00U¶
-
SYSCTL_PERIPH_BIT_S
0x0008U¶
-
SYSCTL_REG_KEY
0xA5A50000U¶
-
SYSCTL_PLL_KEY
0XCAFE0000U¶
-
SYSCTL_TYPE_LOCK_S
0xFU¶
-
SYSCTL_LPM_IDLE
0x0000U¶
-
SYSCTL_LPM_STANDBY
0x0001U¶
-
SYSCTL_LPM_HALT
0x0002U¶
-
SYSCTL_LPM_HIB
0x0003U¶
-
SYSCTL_DEFAULT_OSC_FREQ
10000000U¶
-
SYSCTL_SYNCSELECT_SYNCIN_M
SYSCTL_SYNCSELECT_EPWM4SYNCIN_M¶
-
SYSCTL_BOOT_ROM_STATUS
0x002CU¶
-
SYSCTL_BOOT_ROM_POR
0x8000U¶
-
SYSCTL_BOOT_ROM_XRS
0x4000U¶
-
Device_cal
((void (*)(void))((uintptr_t)0x070282))¶
-
SYSCTL_SYSDIV_M
0x00001F80U¶
-
SYSCTL_SYSDIV_S
7U¶
-
SYSCTL_SYSDIV
(x) ((((x) / 2U) << SYSCTL_SYSDIV_S) & SYSCTL_SYSDIV_M)¶ Macro to format system clock divider value. x must be 1 or even values up to 126.
-
SYSCTL_IMULT_M
0x0000007FU¶
-
SYSCTL_IMULT_S
0U¶
-
SYSCTL_IMULT
(x) (((x) << SYSCTL_IMULT_S) & SYSCTL_IMULT_M)¶ Macro to format integer multiplier value. x is a number from 1 to 127.
-
SYSCTL_FMULT_M
0x00006000U¶
-
SYSCTL_FMULT_S
13U¶
-
SYSCTL_FMULT_NONE
0x00000000U¶ No fractional multiplier.
-
SYSCTL_FMULT_0
0x00000000U¶ No fractional multiplier.
-
SYSCTL_FMULT_1_4
0x00002000U¶ Fractional multiplier of 0.25.
-
SYSCTL_FMULT_1_2
0x00004000U¶ Fractional multiplier of 0.50.
-
SYSCTL_FMULT_3_4
0x00006000U¶ Fractional multiplier of 0.75.
-
SYSCTL_OSCSRC_M
0x00030000U¶
-
SYSCTL_OSCSRC_S
16U¶
-
SYSCTL_OSCSRC_OSC2
0x00000000U¶ Internal oscillator INTOSC2.
-
SYSCTL_OSCSRC_XTAL
0x00010000U¶ External oscillator (XTAL) in crystal mode.
-
SYSCTL_OSCSRC_OSC1
0x00020000U¶ Internal oscillator INTOSC1.
-
SYSCTL_PLL_ENABLE
0x80000000U¶ Enable PLL.
-
SYSCTL_PLL_DISABLE
0x00000000U¶ Disable PLL.
-
SYSCTL_AUXPLL_DIV_1
0x00000000U¶ Auxiliary PLL divide by 1.
-
SYSCTL_AUXPLL_DIV_2
0x00000080U¶ Auxiliary PLL divide by 2.
-
SYSCTL_AUXPLL_DIV_4
0x00000100U¶ Auxiliary PLL divide by 4.
-
SYSCTL_AUXPLL_DIV_8
0x00000180U¶ Auxiliary PLL divide by 8.
-
SYSCTL_AUXPLL_IMULT
(x) SYSCTL_IMULT((x))¶ Macro to format integer multiplier value. x is a number from 1 to 127.
-
SYSCTL_AUXPLL_FMULT_NONE
0x00000000U¶ No fractional multiplier.
-
SYSCTL_AUXPLL_FMULT_0
0x00000000U¶ No fractional multiplier.
-
SYSCTL_AUXPLL_FMULT_1_4
0x00002000U¶ Fractional multiplier - 0.25.
-
SYSCTL_AUXPLL_FMULT_1_2
0x00004000U¶ Fractional multiplier - 0.50.
-
SYSCTL_AUXPLL_FMULT_3_4
0x00006000U¶ Fractional multiplier - 0.75.
-
SYSCTL_AUXPLL_OSCSRC_OSC2
0x00000000U¶ Internal oscillator INTOSC2 as auxiliary clock input.
-
SYSCTL_AUXPLL_OSCSRC_XTAL
0x00010000U¶ External oscillator (XTAL) as auxiliary clock input.
-
SYSCTL_AUXPLL_OSCSRC_AUXCLKIN
0x00020000U¶ AUXCLKIN (from GPIO) as auxiliary clock input.
-
SYSCTL_AUXPLL_ENABLE
0x80000000U¶ Enable AUXPLL.
-
SYSCTL_AUXPLL_DISABLE
0x00000000U¶ Disable AUXPLL.
-
SYSCTL_SEC_MASTER_CLA
0x0U¶ Configure CLA as the secondary master.
-
SYSCTL_SEC_MASTER_DMA
0x1U¶ Configure DMA as the secondary master.
-
SYSCTL_NMI_NMIINT
0x1U¶ NMI Interrupt Flag.
-
SYSCTL_NMI_CLOCKFAIL
0x2U¶ Clock Fail Interrupt Flag.
-
SYSCTL_NMI_RAMUNCERR
0x4U¶ RAM Uncorrectable Error NMI Flag.
-
SYSCTL_NMI_FLUNCERR
0x8U¶ Flash Uncorrectable Error NMI Flag.
-
SYSCTL_NMI_CPU1HWBISTERR
0x10U¶ HW BIST Error NMI Flag.
-
SYSCTL_NMI_CLBNMI
0x100U¶ Configurable Logic Block NMI Flag.
-
SYSCTL_CAUSE_POR
0x00000001U¶ Power-on reset.
-
SYSCTL_CAUSE_XRS
0x00000002U¶ External reset pin.
-
SYSCTL_CAUSE_WDRS
0x00000004U¶ Watchdog reset.
-
SYSCTL_CAUSE_NMIWDRS
0x00000008U¶ NMI watchdog reset.
-
SYSCTL_CAUSE_SCCRESET
0x00000100U¶ SCCRESETn by DCSM.
-
SYSCTL_ADCSOC_SRC_PWM1SOCA
0x1U¶ ePWM1 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM2SOCA
0x2U¶ ePWM2 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM3SOCA
0x4U¶ ePWM3 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM4SOCA
0x8U¶ ePWM4 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM5SOCA
0x10U¶ ePWM5 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM6SOCA
0x20U¶ ePWM6 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM7SOCA
0x40U¶ ePWM7 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM8SOCA
0x80U¶ ePWM8 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM9SOCA
0x100U¶ ePWM9 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM10SOCA
0x200U¶ ePWM10 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM11SOCA
0x400U¶ ePWM11 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM12SOCA
0x800U¶ ePWM12 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM1SOCB
0x10000U¶ ePWM1 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM2SOCB
0x20000U¶ ePWM2 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM3SOCB
0x40000U¶ ePWM3 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM4SOCB
0x80000U¶ ePWM4 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM5SOCB
0x100000U¶ ePWM5 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM6SOCB
0x200000U¶ ePWM6 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM7SOCB
0x400000U¶ ePWM7 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM8SOCB
0x800000U¶ ePWM8 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM9SOCB
0x1000000U¶ ePWM9 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM10SOCB
0x2000000U¶ ePWM10 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM11SOCB
0x4000000U¶ ePWM11 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM12SOCB
0x8000000U¶ ePWM12 SOCB for ADCSOCBO
Enums
-
enum
SysCtl_PeripheralPCLOCKCR
¶ The following are values that can be passed to SysCtl_enablePeripheral() and SysCtl_disablePeripheral() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_PERIPH_CLK_CLA1
= 0x0000¶ CLA1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_DMA
= 0x0200¶ DMA clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER0
= 0x0300¶ CPUTIMER0 clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER1
= 0x0400¶ CPUTIMER1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER2
= 0x0500¶ CPUTIMER2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_HRPWM
= 0x1000¶ HRPWM clock.
-
enumerator
SYSCTL_PERIPH_CLK_TBCLKSYNC
= 0x1200¶ TBCLKSYNC clock.
-
enumerator
SYSCTL_PERIPH_CLK_EMIF1
= 0x0001¶ EMIF1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EMIF2
= 0x0101¶ EMIF2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM1
= 0x0002¶ EPWM1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM2
= 0x0102¶ EPWM2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM3
= 0x0202¶ EPWM3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM4
= 0x0302¶ EPWM4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM5
= 0x0402¶ EPWM5 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM6
= 0x0502¶ EPWM6 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM7
= 0x0602¶ EPWM7 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM8
= 0x0702¶ EPWM8 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM9
= 0x0802¶ EPWM9 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM10
= 0x0902¶ EPWM10 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM11
= 0x0A02¶ EPWM11 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM12
= 0x0B02¶ EPWM12 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP1
= 0x0003¶ ECAP1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP2
= 0x0103¶ ECAP2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP3
= 0x0203¶ ECAP3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP4
= 0x0303¶ ECAP4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP5
= 0x0403¶ ECAP5 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP6
= 0x0503¶ ECAP6 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EQEP1
= 0x0004¶ EQEP1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EQEP2
= 0x0104¶ EQEP2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EQEP3
= 0x0204¶ EQEP3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SD1
= 0x0006¶ SD1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SD2
= 0x0106¶ SD2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCIA
= 0x0007¶ SCI_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCIB
= 0x0107¶ SCI_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCIC
= 0x0207¶ SCI_C clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCID
= 0x0307¶ SCI_D clock.
-
enumerator
SYSCTL_PERIPH_CLK_SPIA
= 0x0008¶ SPI_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_SPIB
= 0x0108¶ SPI_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_SPIC
= 0x0208¶ SPI_C clock.
-
enumerator
SYSCTL_PERIPH_CLK_I2CA
= 0x0009¶ I2C_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_I2CB
= 0x0109¶ I2C_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_CANA
= 0x000A¶ CAN_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_CANB
= 0x010A¶ CAN_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_MCBSPA
= 0x000B¶ MCBSP_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_MCBSPB
= 0x010B¶ MCBSP_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_USBA
= 0x100B¶ USB_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_UPPA
= 0x000C¶ UPP_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCA
= 0x000D¶ ADC_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCB
= 0x010D¶ ADC_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCC
= 0x020D¶ ADC_C clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCD
= 0x030D¶ ADC_D clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS1
= 0x000E¶ CMPSS1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS2
= 0x010E¶ CMPSS2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS3
= 0x020E¶ CMPSS3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS4
= 0x030E¶ CMPSS4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS5
= 0x040E¶ CMPSS5 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS6
= 0x050E¶ CMPSS6 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS7
= 0x060E¶ CMPSS7 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS8
= 0x070E¶ CMPSS8 clock.
-
enumerator
SYSCTL_PERIPH_CLK_DACA
= 0x1010¶ DAC_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_DACB
= 0x1110¶ DAC_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_DACC
= 0x1210¶ DAC_C clock.
-
enumerator
-
enum
SysCtl_PeripheralSOFTPRES
¶ The following are values that can be passed to SysCtl_resetPeripheral() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_PERIPH_RES_CPU1CLA1
= 0x0000¶ Reset CPU1_CLA1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EMIF1
= 0x0001¶ Reset EMIF1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EMIF2
= 0x0101¶ Reset EMIF2 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM1
= 0x0002¶ Reset EPWM1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM2
= 0x0102¶ Reset EPWM2 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM3
= 0x0202¶ Reset EPWM3 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM4
= 0x0302¶ Reset EPWM4 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM5
= 0x0402¶ Reset EPWM5 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM6
= 0x0502¶ Reset EPWM6 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM7
= 0x0602¶ Reset EPWM7 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM8
= 0x0702¶ Reset EPWM8 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM9
= 0x0802¶ Reset EPWM9 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM10
= 0x0902¶ Reset EPWM10 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM11
= 0x0A02¶ Reset EPWM11 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM12
= 0x0B02¶ Reset EPWM12 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP1
= 0x0003¶ Reset ECAP1 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP2
= 0x0103¶ Reset ECAP2 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP3
= 0x0203¶ Reset ECAP3 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP4
= 0x0303¶ Reset ECAP4 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP5
= 0x0403¶ Reset ECAP5 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP6
= 0x0503¶ Reset ECAP6 clock.
-
enumerator
SYSCTL_PERIPH_RES_EQEP1
= 0x0004¶ Reset EQEP1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EQEP2
= 0x0104¶ Reset EQEP2 clock.
-
enumerator
SYSCTL_PERIPH_RES_EQEP3
= 0x0204¶ Reset EQEP3 clock.
-
enumerator
SYSCTL_PERIPH_RES_SD1
= 0x0006¶ Reset SD1 clock.
-
enumerator
SYSCTL_PERIPH_RES_SD2
= 0x0106¶ Reset SD2 clock.
-
enumerator
SYSCTL_PERIPH_RES_SCIA
= 0x0007¶ Reset SCI_A clock.
-
enumerator
SYSCTL_PERIPH_RES_SCIB
= 0x0107¶ Reset SCI_B clock.
-
enumerator
SYSCTL_PERIPH_RES_SCIC
= 0x0207¶ Reset SCI_C clock.
-
enumerator
SYSCTL_PERIPH_RES_SCID
= 0x0307¶ Reset SCI_D clock.
-
enumerator
SYSCTL_PERIPH_RES_SPIA
= 0x0008¶ Reset SPI_A clock.
-
enumerator
SYSCTL_PERIPH_RES_SPIB
= 0x0108¶ Reset SPI_B clock.
-
enumerator
SYSCTL_PERIPH_RES_SPIC
= 0x0208¶ Reset SPI_C clock.
-
enumerator
SYSCTL_PERIPH_RES_I2CA
= 0x0009¶ Reset I2C_A clock.
-
enumerator
SYSCTL_PERIPH_RES_I2CB
= 0x0109¶ Reset I2C_B clock.
-
enumerator
SYSCTL_PERIPH_RES_MCBSPA
= 0x000B¶ Reset MCBSP_A clock.
-
enumerator
SYSCTL_PERIPH_RES_MCBSPB
= 0x010B¶ Reset MCBSP_B clock.
-
enumerator
SYSCTL_PERIPH_RES_USBA
= 0x100B¶ Reset USB_A clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCA
= 0x000D¶ Reset ADC_A clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCB
= 0x010D¶ Reset ADC_B clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCC
= 0x020D¶ Reset ADC_C clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCD
= 0x030D¶ Reset ADC_D clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS1
= 0x000E¶ Reset CMPSS1 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS2
= 0x010E¶ Reset CMPSS2 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS3
= 0x020E¶ Reset CMPSS3 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS4
= 0x030E¶ Reset CMPSS4 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS5
= 0x040E¶ Reset CMPSS5 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS6
= 0x050E¶ Reset CMPSS6 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS7
= 0x060E¶ Reset CMPSS7 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS8
= 0x070E¶ Reset CMPSS8 clock.
-
enumerator
SYSCTL_PERIPH_RES_DACA
= 0x1010¶ Reset DAC_A clock.
-
enumerator
SYSCTL_PERIPH_RES_DACB
= 0x1110¶ Reset DAC_B clock.
-
enumerator
SYSCTL_PERIPH_RES_DACC
= 0x1210¶ Reset DAC_C clock.
-
enumerator
-
enum
SysCtl_WDPrescaler
¶ The following are values that can be passed to SysCtl_setWatchdogPrescaler() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_WD_PRESCALE_1
= 1¶ WDCLK = PREDIVCLK / 1.
-
enumerator
SYSCTL_WD_PRESCALE_2
= 2¶ WDCLK = PREDIVCLK / 2.
-
enumerator
SYSCTL_WD_PRESCALE_4
= 3¶ WDCLK = PREDIVCLK / 4.
-
enumerator
SYSCTL_WD_PRESCALE_8
= 4¶ WDCLK = PREDIVCLK / 8.
-
enumerator
SYSCTL_WD_PRESCALE_16
= 5¶ WDCLK = PREDIVCLK / 16.
-
enumerator
SYSCTL_WD_PRESCALE_32
= 6¶ WDCLK = PREDIVCLK / 32.
-
enumerator
SYSCTL_WD_PRESCALE_64
= 7¶ WDCLK = PREDIVCLK / 64.
-
enumerator
-
enum
SysCtl_WDMode
¶ The following are values that can be passed to SysCtl_setWatchdogMode() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_WD_MODE_RESET
¶ Watchdog can generate a reset signal.
-
enumerator
SYSCTL_WD_MODE_INTERRUPT
¶ Watchdog can generate an interrupt signal; reset signal is disabled.
-
enumerator
-
enum
SysCtl_LSPCLKPrescaler
¶ The following are values that can be passed to SysCtl_setLowSpeedClock() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_LSPCLK_PRESCALE_1
= 0¶ LSPCLK = SYSCLK / 1.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_2
= 1¶ LSPCLK = SYSCLK / 2.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_4
= 2¶ LSPCLK = SYSCLK / 4 (default)
-
enumerator
SYSCTL_LSPCLK_PRESCALE_6
= 3¶ LSPCLK = SYSCLK / 6.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_8
= 4¶ LSPCLK = SYSCLK / 8.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_10
= 5¶ LSPCLK = SYSCLK / 10.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_12
= 6¶ LSPCLK = SYSCLK / 12.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_14
= 7¶ LSPCLK = SYSCLK / 14.
-
enumerator
-
enum
SysCtl_EPWMCLKDivider
¶ The following are values that can be passed to SysCtl_setEPWMClockDivider() as the divider parameter.
Values:
-
enumerator
SYSCTL_EPWMCLK_DIV_1
¶ EPWMCLK = PLLSYSCLK / 1.
-
enumerator
SYSCTL_EPWMCLK_DIV_2
¶ EPWMCLK = PLLSYSCLK / 2.
-
enumerator
-
enum
SysCtl_EMIF1CLKDivider
¶ The following are values that can be passed to SysCtl_setEMIF1ClockDivider() as the divider parameter.
Values:
-
enumerator
SYSCTL_EMIF1CLK_DIV_1
¶ EMIF1CLK = PLLSYSCLK / 1.
-
enumerator
SYSCTL_EMIF1CLK_DIV_2
¶ EMIF1CLK = PLLSYSCLK / 2.
-
enumerator
-
enum
SysCtl_EMIF2CLKDivider
¶ The following are values that can be passed to SysCtl_setEMIF2ClockDivider() as the divider parameter.
Values:
-
enumerator
SYSCTL_EMIF2CLK_DIV_1
¶ EMIF2CLK = PLLSYSCLK / 1.
-
enumerator
SYSCTL_EMIF2CLK_DIV_2
¶ EMIF2CLK = PLLSYSCLK / 2.
-
enumerator
-
enum
SysCtl_ClockOut
¶ The following are values that can be passed to SysCtl_selectClockOutSource() as the source parameter.
Values:
-
enumerator
SYSCTL_CLOCKOUT_PLLSYS
= 0U¶ PLL System Clock post SYSCLKDIV.
-
enumerator
SYSCTL_CLOCKOUT_PLLRAW
= 1U¶ PLL Raw Clock.
-
enumerator
SYSCTL_CLOCKOUT_SYSCLK
= 2U¶ CPU System Clock.
-
enumerator
SYSCTL_CLOCKOUT_INTOSC1
= 5U¶ Internal Oscillator 1.
-
enumerator
SYSCTL_CLOCKOUT_INTOSC2
= 6U¶ Internal Oscillator 2.
-
enumerator
SYSCTL_CLOCKOUT_XTALOSC
= 7U¶ External Oscillator.
-
enumerator
-
enum
SysCtl_SyncInput
¶ The following values define the syncInput parameter for SysCtl_setSyncInputConfig().
Values:
-
enumerator
SYSCTL_SYNC_IN_EPWM4
= 0¶ Sync input to EPWM4.
-
enumerator
SYSCTL_SYNC_IN_EPWM7
= 3¶ Sync input to EPWM7.
-
enumerator
SYSCTL_SYNC_IN_EPWM10
= 6¶ Sync input to EPWM10.
-
enumerator
SYSCTL_SYNC_IN_ECAP1
= 9¶ Sync input to ECAP1.
-
enumerator
SYSCTL_SYNC_IN_ECAP4
= 12¶ Sync input to ECAP4.
-
enumerator
-
enum
SysCtl_SyncInputSource
¶ The following values define the syncSrc parameter for SysCtl_setSyncInputConfig(). Note that some of these are only valid for certain values of syncInput. See device technical reference manual for info on time-base counter synchronization for details.
Values:
-
enumerator
SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT
= 0¶ EPWM1SYNCOUT.
-
enumerator
SYSCTL_SYNC_IN_SRC_EPWM4SYNCOUT
= 1¶ EPWM4SYNCOUT.
-
enumerator
SYSCTL_SYNC_IN_SRC_EPWM7SYNCOUT
= 2¶ EPWM7SYNCOUT.
-
enumerator
SYSCTL_SYNC_IN_SRC_EPWM10SYNCOUT
= 3¶ EPWM10SYNCOUT.
-
enumerator
SYSCTL_SYNC_IN_SRC_ECAP1SYNCOUT
= 4¶ ECAP1SYNCOUT.
-
enumerator
SYSCTL_SYNC_IN_SRC_EXTSYNCIN1
= 5¶ EXTSYNCIN1Valid for all values of syncInput.
-
enumerator
SYSCTL_SYNC_IN_SRC_EXTSYNCIN2
= 6¶ EXTSYNCIN2Valid for all values of syncInput.
-
enumerator
-
enum
SysCtl_SyncOutputSource
¶ The following values define the syncSrc parameter for SysCtl_setSyncOutputConfig().
Values:
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT
¶ EPWM1SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM4SYNCOUT
¶ EPWM4SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM7SYNCOUT
¶ EPWM7SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM10SYNCOUT
¶ EPWM10SYNCOUT –> EXTSYNCOUT.
-
enumerator
-
enum
SysCtl_DeviceParametric
¶ The following values define the parametric parameter for SysCtl_getDeviceParametric().
Values:
-
enumerator
SYSCTL_DEVICE_QUAL
¶ Device Qualification Status.
-
enumerator
SYSCTL_DEVICE_PINCOUNT
¶ Device Pin Count.
-
enumerator
SYSCTL_DEVICE_INSTASPIN
¶ Device InstaSPIN Feature Set.
-
enumerator
SYSCTL_DEVICE_FLASH
¶ Device Flash size (KB)
-
enumerator
SYSCTL_DEVICE_PARTID
¶ Device Part ID Format Revision.
-
enumerator
SYSCTL_DEVICE_FAMILY
¶ Device Family.
-
enumerator
SYSCTL_DEVICE_PARTNO
¶ Device Part Number.
-
enumerator
SYSCTL_DEVICE_CLASSID
¶ Device Class ID.
-
enumerator
-
enum
SysCtl_XClkDivider
¶ The following are values that can be passed to SysCtl_setXClk() as divider parameter.
Values:
-
enumerator
SYSCTL_XCLKOUT_DIV_1
= 0¶ XCLKOUT = XCLKOUT / 1.
-
enumerator
SYSCTL_XCLKOUT_DIV_2
= 1¶ XCLKOUT = XCLKOUT / 2.
-
enumerator
SYSCTL_XCLKOUT_DIV_4
= 2¶ XCLKOUT = XCLKOUT / 4.
-
enumerator
SYSCTL_XCLKOUT_DIV_8
= 3¶ XCLKOUT = XCLKOUT / 8.
-
enumerator
-
enum
SysCtl_AuxPLLClkDivider
¶ The following are values that can be passed to SysCtl_setAuxPLLClk() as divider parameter.
Values:
-
enumerator
SYSCTL_AUXPLLCLK_DIV_1
¶ AUXPLL clock = AUXPLL clock / 1.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_2
¶ AUXPLL clock = AUXPLL clock / 2.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_4
¶ AUXPLL clock = AUXPLL clock / 4.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_8
¶ AUXPLL clock = AUXPLL clock / 8.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_3
¶ AUXPLL clock = AUXPLL clock / 3.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_5
¶ AUXPLL clock = AUXPLL clock / 5.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_6
¶ AUXPLL clock = AUXPLL clock / 6.
-
enumerator
SYSCTL_AUXPLLCLK_DIV_7
¶ AUXPLL clock = AUXPLL clock / 7.
-
enumerator
-
enum
SysCtl_Cputimer2ClkDivider
¶ The following are values that can be passed to SysCtl_setCputimer2Clk() as divider parameter.
Values:
-
enumerator
SYSCTL_TMR2CLKPRESCALE_1
¶ Cputimer2 clock = Cputimer2 clock / 1.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_2
¶ Cputimer2 clock = Cputimer2 clock / 2.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_4
¶ Cputimer2 clock = Cputimer2 clock / 4.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_8
¶ Cputimer2 clock = Cputimer2 clock / 8.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_16
¶ Cputimer2 clock = Cputimer2 clock / 16.
-
enumerator
-
enum
SysCtl_Cputimer2ClkSource
¶ The following are values that can be passed to SysCtl_setCputimer2Clk() as source parameter.
Values:
-
enumerator
SYSCTL_TMR2CLKSRCSEL_SYSCLK
= 0U¶ System Clock.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_INTOSC1
= 1U¶ Internal Oscillator 1.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_INTOSC2
= 2U¶ Internal Oscillator 2.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_XTAL
= 3U¶ Crystal oscillator.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_AUXPLLCLK
= 6U¶ Aux PLL CLock.
-
enumerator
Functions
-
void
SysCtl_deviceCal
(void)¶ Wrapper function for Device_cal function
- Return
None.
- Parameters
None
: This is a wrapper function for the Device_cal function available in the OTP memory. The function saves and restores the core registers which are being used by the Device_cal function
-
void
SysCtl_resetPeripheral
(SysCtl_PeripheralSOFTPRES peripheral)¶ Resets a peripheral
This function uses the SOFTPRESx registers to reset a specified peripheral. Module registers will be returned to their reset states.
- Parameters
peripheral
: is the peripheral to reset.
- Note
This includes registers containing trim values.The peripheral software reset needed by CPU2 can be communicated to CPU1 via IPC for all shared peripherals.
- Return
None.
-
void
SysCtl_enablePeripheral
(SysCtl_PeripheralPCLOCKCR peripheral)¶ Enables a peripheral.
Peripherals are enabled with this function. At power-up, all peripherals are disabled; they must be enabled in order to operate or respond to register reads/writes.
- Parameters
peripheral
: is the peripheral to enable.
- Note
Note that there should be atleast 5 cycles delay between enabling the peripheral clock and accessing the peripheral registers. The delay should be added by the user if the peripheral is accessed immediately after this function call. Use asm(” RPT #5 || NOP”); to add 5 cycle delay post this function call.
- Return
None.
-
void
SysCtl_disablePeripheral
(SysCtl_PeripheralPCLOCKCR peripheral)¶ Disables a peripheral.
Peripherals are disabled with this function. Once disabled, they will not operate or respond to register reads/writes.
- Parameters
peripheral
: is the peripheral to disable.
- Return
None.
-
void
SysCtl_resetDevice
(void)¶ Resets the device.
This function performs a watchdog reset of the device.
- Return
This function does not return.
-
uint32_t
SysCtl_getResetCause
(void)¶ Gets the reason for a reset.
This function will return the reason(s) for a reset. Since the reset reasons are sticky until either cleared by software or an external reset, multiple reset reasons may be returned if multiple resets have occurred. The reset reason will be a logical OR of
SYSCTL_CAUSE_POR - Power-on reset
SYSCTL_CAUSE_XRS - External reset pin
SYSCTL_CAUSE_WDRS - Watchdog reset
SYSCTL_CAUSE_NMIWDRS - NMI watchdog reset
SYSCTL_CAUSE_SCCRESET - SCCRESETn reset from DCSM
- Note
If you re-purpose the reserved boot ROM RAM, the POR and XRS reset statuses won’t be accurate.
- Return
Returns the reason(s) for a reset.
-
void
SysCtl_clearResetCause
(uint32_t rstCauses)¶ Clears reset reasons.
This function clears the specified sticky reset reasons. Once cleared, another reset for the same reason can be detected, and a reset for a different reason can be distinguished (instead of having two reset causes set). If the reset reason is used by an application, all reset causes should be cleared after they are retrieved with
SysCtl_getResetCause().- Parameters
rstCauses
: are the reset causes to be cleared; must be a logical OR of SYSCTL_CAUSE_POR, SYSCTL_CAUSE_XRS, SYSCTL_CAUSE_WDRS, SYSCTL_CAUSE_NMIWDRS, and/or SYSCTL_CAUSE_SCCRESET.
- Note
Some reset causes are cleared by the boot ROM.
- Return
None.
-
void
SysCtl_setLowSpeedClock
(SysCtl_LSPCLKPrescaler prescaler)¶ Sets the low speed peripheral clock rate prescaler.
This function configures the clock rate of the low speed peripherals. The
prescaler parameter is the value by which the SYSCLK rate is divided to get the LSPCLK rate. For example, a prescaler of SYSCTL_LSPCLK_PRESCALE_4 will result in a LSPCLK rate that is a quarter of the SYSCLK rate.- Parameters
prescaler
: is the LSPCLK rate relative to SYSCLK
- Return
None.
-
void
SysCtl_setEPWMClockDivider
(SysCtl_EPWMCLKDivider divider)¶ Sets the ePWM clock divider.
This function configures the clock rate of the EPWMCLK. The
divider parameter is the value by which the SYSCLK rate is divided to get the EPWMCLK rate. For example, SYSCTL_EPWMCLK_DIV_2 will select an EPWMCLK rate that is half the PLLSYSCLK rate.- Parameters
divider
: is the value by which PLLSYSCLK is divided
- Return
None.
-
void
SysCtl_setEMIF1ClockDivider
(SysCtl_EMIF1CLKDivider divider)¶ Sets the EMIF1 clock divider.
This function configures the clock rate of the EMIF1CLK. The
divider parameter is the value by which the SYSCLK rate is divided to get the EMIF1CLK rate. For example, SYSCTL_EMIF1CLK_DIV_2 will select an EMIF1CLK rate that is half the PLLSYSCLK (or CPU1.SYSCLK on a dual core device) rate.- Parameters
divider
: is the value by which PLLSYSCLK (or CPU1.SYSCLK on a dual core device) is divided
- Return
None.
-
void
SysCtl_setEMIF2ClockDivider
(SysCtl_EMIF2CLKDivider divider)¶ Sets the EMIF2 clock divider.
This function configures the clock rate of the EMIF2CLK. The
divider parameter is the value by which the SYSCLK rate is divided to get the EMIF2CLK rate. For example, SYSCTL_EMIF2CLK_DIV_2 will select an EMIF2CLK rate that is half the PLLSYSCLK (or CPU1.SYSCLK on a dual core device) rate.- Parameters
divider
: is the value by which PLLSYSCLK (or CPU1.SYSCLK on a dual core device) is divided
- Return
None.
-
void
SysCtl_selectClockOutSource
(SysCtl_ClockOut source)¶ Selects a clock source to mux to an external GPIO pin (XCLKOUT).
This function configures the specified clock source to be muxed to an external clock out (XCLKOUT) GPIO pin. The
source parameter may take a value of one of the following values:SYSCTL_CLOCKOUT_PLLSYS
SYSCTL_CLOCKOUT_PLLRAW
SYSCTL_CLOCKOUT_SYSCLK
SYSCTL_CLOCKOUT_INTOSC1
SYSCTL_CLOCKOUT_INTOSC2
SYSCTL_CLOCKOUT_XTALOSC
- Parameters
source
: is the internal clock source to be configured.
- Return
None.
-
uint16_t
SysCtl_getExternalOscCounterValue
(void)¶ Gets the external oscillator counter value.
This function returns the X1 clock counter value. When the return value reaches 0x3FF, it freezes. Before switching from INTOSC2 to an external oscillator (XTAL), an application should call this function to make sure the counter is saturated.
- Return
Returns the value of the 10-bit X1 clock counter.
-
void
SysCtl_turnOnOsc
(uint32_t oscSource)¶ Turns on the specified oscillator sources.
This function turns on the oscillator specified by the
oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.- Parameters
oscSource
: is the oscillator source to be configured.
- Note
SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.
- Return
None.
-
void
SysCtl_turnOffOsc
(uint32_t oscSource)¶ Turns off the specified oscillator sources.
This function turns off the oscillator specified by the
oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.- Parameters
oscSource
: is the oscillator source to be configured.
- Note
SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.
- Return
None.
-
void
SysCtl_enterIdleMode
(void)¶ Enters IDLE mode.
This function puts the device into IDLE mode. The CPU clock is gated while all peripheral clocks are left running. Any enabled interrupt will wake the CPU up from IDLE mode.
- Return
None.
-
void
SysCtl_enterStandbyMode
(void)¶ Enters STANDBY mode.
This function puts the device into STANDBY mode. This will gate both the CPU clock and any peripheral clocks derived from SYSCLK. The watchdog is left active, and an NMI or an optional watchdog interrupt will wake the CPU subsystem from STANDBY mode.
GPIOs may be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().
The CPU will receive an interrupt (WAKEINT) on wakeup.
- Return
None.
-
void
SysCtl_enterHaltMode
(void)¶ Enters HALT mode.
This function puts the device into HALT mode. This will gate almost all systems and clocks and allows for the power-down of oscillators and analog blocks. The watchdog may be left clocked to produce a reset. See SysCtl_enableWatchdogInHalt() to enable this. GPIOs should be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().
The CPU will receive an interrupt (WAKEINT) on wakeup.
- Return
None.
-
void
SysCtl_enterHibernateMode
(void)¶ Enters Hibernate mode.
This function puts the device into Hibernate mode. Hibernate (HIB) is a global low-power mode that gates the supply voltages to most of the system. This mode affects both CPU subsystems. HIB is essentially a controlled power-down with remote wakeup capability, and can be used to save power during long periods of inactivity.
To wake the device from HIB mode:
Assert the dedicated GPIOHIBWAKE pin (GPIO41) low to enable the power-up of the device clock sources.
Assert GPIOHIBWAKE pin high again. This triggers the power-up of the rest of the device.
- Return
None.
-
void
SysCtl_enableLPMWakeupPin
(uint32_t pin)¶ Enables a pin to wake up the device from the following mode(s):
STANDBY
HALT
This function connects a pin to the LPM circuit, allowing an event on the pin to wake up the device when when it is in following mode(s):
STANDBY
HALT
- Parameters
pin
: is the identifying number of the pin.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are capable of being connected to the LPM circuit.
- Return
None.
-
void
SysCtl_disableLPMWakeupPin
(uint32_t pin)¶ Disables a pin to wake up the device from the following mode(s):
STANDBY
HALT
This function disconnects a pin to the LPM circuit, disallowing an event on the pin to wake up the device when when it is in following mode(s):
STANDBY
HALT
- Parameters
pin
: is the identifying number of the pin.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are valid.
- Return
None.
-
void
SysCtl_setStandbyQualificationPeriod
(uint16_t cycles)¶ Sets the number of cycles to qualify an input on waking from STANDBY mode.
This function sets the number of OSCCLK clock cycles used to qualify the selected inputs when waking from STANDBY mode. The
cycles parameter should be passed a cycle count between 2 and 65 cycles inclusive.- Parameters
cycles
: is the number of OSCCLK cycles.
- Return
None.
-
void
SysCtl_enableWatchdogStandbyWakeup
(void)¶ Enable the device to wake from STANDBY mode upon a watchdog interrupt.
- Note
In order to use this option, you must configure the watchdog to generate an interrupt using SysCtl_setWatchdogMode().
- Return
None.
-
void
SysCtl_disableWatchdogStandbyWakeup
(void)¶ Disable the device from waking from STANDBY mode upon a watchdog interrupt.
- Return
None.
-
void
SysCtl_enableWatchdogInHalt
(void)¶ Enable the watchdog to run while in HALT mode.
This function configures the watchdog to continue to run while in HALT mode. Additionally, INTOSC1 and INTOSC2 are not powered down when the system enters HALT mode. By default the watchdog is gated when the system enters HALT.
- Return
None.
-
void
SysCtl_disableWatchdogInHalt
(void)¶ Disable the watchdog from running while in HALT mode.
This function gates the watchdog when the system enters HALT mode. INTOSC1 and INTOSC2 will be powered down. This is the default behavior of the device.
- Return
None.
-
void
SysCtl_setWatchdogMode
(SysCtl_WDMode mode)¶ Configures whether the watchdog generates a reset or an interrupt signal.
This function configures the action taken when the watchdog counter reaches its maximum value. When the
mode parameter is SYSCTL_WD_MODE_INTERRUPT, the watchdog is enabled to generate a watchdog interrupt signal and disables the generation of a reset signal. This will allow the watchdog module to wake up the device from IDLE or STANDBY if desired (see SysCtl_enableWatchdogStandbyWakeup()).- Parameters
mode
: is a flag to select the watchdog mode.
When the mode parameter is SYSCTL_WD_MODE_RESET, the watchdog will be put into reset mode and generation of a watchdog interrupt signal will be disabled. This is how the watchdog is configured by default.
- Note
Check the status of the watchdog interrupt using SysCtl_isWatchdogInterruptActive() before calling this function. If the interrupt is still active, switching from interrupt mode to reset mode will immediately reset the device.
- Return
None.
-
bool
SysCtl_isWatchdogInterruptActive
(void)¶ Gets the status of the watchdog interrupt signal.
This function returns the status of the watchdog interrupt signal. If the interrupt is active, this function will return true. If false, the interrupt is NOT active.
- Note
Make sure to call this function to ensure that the interrupt is not active before making any changes to the configuration of the watchdog to prevent any unexpected behavior. For instance, switching from interrupt mode to reset mode while the interrupt is active will immediately reset the device.
- Return
true if the interrupt is active and false if it is not.
-
void
SysCtl_disableWatchdog
(void)¶ Disables the watchdog.
This function disables the watchdog timer. Note that the watchdog timer is enabled on reset.
- Return
None.
-
void
SysCtl_enableWatchdog
(void)¶ Enables the watchdog.
This function enables the watchdog timer. Note that the watchdog timer is enabled on reset.
- Return
None.
-
void
SysCtl_serviceWatchdog
(void)¶ Services the watchdog.
This function resets the watchdog.
- Return
None.
-
void
SysCtl_enableWatchdogReset
(void)¶ Writes the first key to enter the watchdog reset.
This function writes the first key to enter the watchdog reset.
- Return
None.
-
void
SysCtl_resetWatchdog
(void)¶ Writes the second key to reset the watchdog.
This function writes the second key to reset the watchdog.
- Return
None.
-
void
SysCtl_setWatchdogPrescaler
(SysCtl_WDPrescaler prescaler)¶ Sets up watchdog clock (WDCLK) prescaler.
This function sets up the watchdog clock (WDCLK) prescaler. The
prescaler parameter divides INTOSC1 down to WDCLK.- Parameters
prescaler
: is the value that configures the watchdog clock relative to the value from the pre-divider.
- Return
None.
-
uint16_t
SysCtl_getWatchdogCounterValue
(void)¶ Gets the watchdog counter value.
- Return
Returns the current value of the 8-bit watchdog counter. If this count value overflows, a watchdog output pulse is generated.
-
bool
SysCtl_getWatchdogResetStatus
(void)¶ Gets the watchdog reset status.
This function returns the watchdog reset status. If this function returns true, that indicates that a watchdog reset generated the last reset condition. Otherwise, it was an external device or power-up reset condition.
- Return
Returns true if the watchdog generated the last reset condition.
-
void
SysCtl_clearWatchdogResetStatus
(void)¶ Clears the watchdog reset status.
This function clears the watchdog reset status. To check if it was set first, see SysCtl_getWatchdogResetStatus().
- Return
None.
-
void
SysCtl_setWatchdogWindowValue
(uint16_t value)¶ Set the minimum threshold value for windowed watchdog
This function sets the minimum threshold value used to define the lower limit of the windowed watchdog functionality.
- Parameters
value
: is the value to set the window threshold
- Return
None.
-
void
SysCtl_clearWatchdogOverride
(void)¶ Clears the watchdog override.
This function clears the watchdog override and locks the watchdog timer module to remain in its prior state which could be either enable /disable. The watchdog timer will remain in this state until the next system reset.
- Return
None.
-
void
SysCtl_enableNMIGlobalInterrupt
(void)¶ Enable the NMI Global interrupt bit
Note: This bit should be set after the device security related initialization is complete.
- Return
None.
-
bool
SysCtl_getNMIStatus
(void)¶ Read NMI interrupts.
Read the current state of NMI interrupt.
- Return
true if NMI interrupt is triggered, false if not.
-
uint16_t
SysCtl_getNMIFlagStatus
(void)¶ Read NMI Flags.
Read the current state of individual NMI interrupts
- Return
Value of NMIFLG register. These defines are provided to decode the value:
SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
-
bool
SysCtl_isNMIFlagSet
(uint32_t nmiFlags)¶ Check if the individual NMI interrupts are set.
Check if interrupt flags corresponding to the passed in bit mask are asserted.
- Parameters
nmiFlags
: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
- Return
true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.
-
void
SysCtl_clearNMIStatus
(uint32_t nmiFlags)¶ Function to clear individual NMI interrupts.
Clear NMI interrupt flags that correspond with the passed in bit mask.
- Parameters
nmiFlags
: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
Note: The NMI Interrupt flag is always cleared by default and therefore doesn’t have to be included in the bit mask.
- Return
None.
-
void
SysCtl_clearAllNMIFlags
(void)¶ Clear all the NMI Flags that are currently set.
- Return
None.
-
void
SysCtl_forceNMIFlags
(uint32_t nmiFlags)¶ Function to force individual NMI interrupt fail flags
- Return
None.
- Parameters
nmiFlags
: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
-
uint16_t
SysCtl_getNMIWatchdogCounter
(void)¶ Gets the NMI watchdog counter value.
Note: The counter is clocked at the SYSCLKOUT rate.
- Return
Returns the NMI watchdog counter register’s current value.
-
void
SysCtl_setNMIWatchdogPeriod
(uint16_t wdPeriod)¶ Sets the NMI watchdog period value.
This function writes to the NMI watchdog period register that holds the value to which the NMI watchdog counter is compared. When the two registers match, a reset is generated. By default, the period is 0xFFFF.
- Parameters
wdPeriod
: is the 16-bit value at which a reset is generated.
- Note
If a value smaller than the current counter value is passed into the wdPeriod parameter, a NMIRSn will be forced.
- Return
None.
-
uint16_t
SysCtl_getNMIWatchdogPeriod
(void)¶ Gets the NMI watchdog period value.
- Return
Returns the NMI watchdog period register’s current value.
-
uint32_t
SysCtl_getNMIShadowFlagStatus
(void)¶ Read NMI Shadow Flags.
Read the current state of individual NMI interrupts
- Return
Value of NMISHDFLG register. These defines are provided to decode the value:
SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
-
bool
SysCtl_isNMIShadowFlagSet
(uint32_t nmiFlags)¶ Check if the individual NMI shadow flags are set.
Check if interrupt flags corresponding to the passed in bit mask are asserted.
- Parameters
nmiFlags
: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag
- Return
true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.
-
void
SysCtl_enableMCD
(void)¶ Enable the missing clock detection (MCD) Logic
- Return
None.
-
void
SysCtl_disableMCD
(void)¶ Disable the missing clock detection (MCD) Logic
- Return
None.
-
bool
SysCtl_isMCDClockFailureDetected
(void)¶ Get the missing clock detection Failure Status
- Note
A failure means the oscillator clock is missing
- Return
Returns true if a failure is detected or false if a failure isn’t detected
-
void
SysCtl_resetMCD
(void)¶ Reset the missing clock detection logic after clock failure
- Return
None.
-
void
SysCtl_connectMCDClockSource
(void)¶ Re-connect missing clock detection clock source to stop simulating clock failure
- Return
None.
-
void
SysCtl_disconnectMCDClockSource
(void)¶ Disconnect missing clock detection clock source to simulate clock failure. This is for testing the MCD functionality.
- Return
None.
-
void
SysCtl_setSyncInputConfig
(SysCtl_SyncInput syncInput, SysCtl_SyncInputSource syncSrc)¶ Configures the sync input source for the ePWM and eCAP signals.
This function configures the sync input source for the ePWM and eCAP modules. The
syncInput parameter is the sync input being configured. It should be passed a value of SYSCTL_SYNC_IN_XXXX, where XXXX is the ePWM or eCAP instance the sync signal is entering.- Parameters
syncInput
: is the sync input being configuredsyncSrc
: is sync input source selection.
The syncSrc parameter is the sync signal selected as the source of the sync input. It should be passed a value of SYSCTL_SYNC_IN_SRC_XXXX, XXXX is a sync signal coming from an ePWM, eCAP or external sync output. where For example, a syncInput value of SYSCTL_SYNC_IN_ECAP1 and a syncSrc value of SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT will make the EPWM1SYNCOUT signal drive eCAP1’s SYNCIN signal.
Note that some syncSrc values are only valid for certain values of syncInput. See device technical reference manual for details on time-base counter synchronization.
- Return
None.
-
void
SysCtl_setSyncOutputConfig
(SysCtl_SyncOutputSource syncSrc)¶ Configures the sync output source.
This function configures the sync output source from the ePWM modules. The
syncSrc parameter is a value SYSCTL_SYNC_OUT_SRC_XXXX, where XXXX is a sync signal coming from an ePWM such as SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT- Parameters
syncSrc
: is sync output source selection.
- Return
None.
-
void
SysCtl_enableExtADCSOCSource
(uint32_t adcsocSrc)¶ Enables ePWM SOC signals to drive an external (off-chip) ADCSOC signal.
This function configures which ePWM SOC signals are enabled as a source for either ADCSOCAO or ADCSOCBO. The
adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.- Parameters
adcsocSrc
: is a bit field of the selected signals to be enabled
- Return
None.
-
void
SysCtl_disableExtADCSOCSource
(uint32_t adcsocSrc)¶ Disables ePWM SOC signals from driving an external ADCSOC signal.
This function configures which ePWM SOC signals are disabled as a source for either ADCSOCAO or ADCSOCBO. The
adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.- Parameters
adcsocSrc
: is a bit field of the selected signals to be disabled
- Return
None.
-
void
SysCtl_lockExtADCSOCSelect
(void)¶ Locks the SOC Select of the Trig X-BAR.
This function locks the external ADC SOC select of the Trig X-BAR.
- Return
None.
-
void
SysCtl_selectSecMaster
(uint16_t periFrame1Config, uint16_t periFrame2Config)¶ Configures whether the dual ported bridge is connected with DMA or CLA as the secondary master.
One of the following values can be passed as parameter.
SYSCTL_SEC_MASTER_CLA SYSCTL_SEC_MASTER_DMA- Parameters
periFrame1Config
: indicates whether CLA or DMA is configured as secondary master on peripheral frame 1.periFrame2Config
: indicates whether CLA or DMA is configured as secondary master on peripheral frame 2.
- Return
None.
-
void
SysCtl_lockSyncSelect
(void)¶ Locks the Sync Select of the Trig X-BAR.
This function locks Sync Input and Output Select of the Trig X-BAR.
- Return
None.
-
uint32_t
SysCtl_getDeviceRevision
(void)¶ Get the Device Silicon Revision ID
This function returns the silicon revision ID for the device.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Returns the silicon revision ID value.
-
uint16_t
SysCtl_getEfuseError
(void)¶ Gets the error status of the Efuse
The function provides both the Efuse Autoload & the Efuse Self Test Error Status.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Fuse Error status.
-
void
SysCtl_setXClk
(SysCtl_XClkDivider divider)¶ Sets up XCLK divider.
This function sets up the XCLK divider. There is only one divider that scales INTOSC1 to XCLK.
- Parameters
divider
: is the value that configures the divider.
The divider parameter can have one enumerated value from SysCtl_XClkDivider
- Return
None.
-
void
SysCtl_setPLLSysClk
(uint16_t divider)¶ Sets up PLLSYSCLK divider.
This function sets up the PLLSYSCLK divider. There is only one divider that scales PLLSYSCLK to generate the system clock.
- Parameters
divider
: is the value that configures the divider.
The divider parameter can have one value from the set below: 0x0 = /1 0x1 = /2 0x2 = /4 (default on reset) 0x3 = /6 0x4 = /8 …… 0x3F =/126
- Return
None.
- Note
Please make sure to check if the PLL is locked and valid using the SysCtl_isPLLValid() before setting the divider.
-
void
SysCtl_setAuxPLLClk
(SysCtl_AuxPLLClkDivider divider)¶ Sets up AUXPLLCLK divider.
This function sets up the AUXPLLCLK divider. There is only one divider that scales AUXPLLCLK to generate the system clock.
- Parameters
divider
: is the value that configures the divider.
The divider parameter can have one enumerated value from SysCtl_AuxPLLClkDivider
- Return
None.
- Note
Please make sure to check if the PLL is locked and valid using the SysCtl_isPLLValid() before setting the divider.
-
void
SysCtl_setCputimer2Clk
(SysCtl_Cputimer2ClkDivider divider, SysCtl_Cputimer2ClkSource source)¶ Sets up CPU Timer 2 CLK source & divider.
This function sets up the CPU Timer 2 CLK divider based on the source that is selected. There is only one divider that scales the “source” to CPU Timer 2 CLK.
- Parameters
divider
: is the value that configures the divider.source
: is the source for the clock divider
The divider parameter can have one enumerated value from SysCtl_Cputimer2ClkDivider The source parameter can have one enumerated value from SysCtl_Cputimer2ClkSource
- Return
None.
-
uint32_t
SysCtl_getPIEVErrAddr
(void)¶ Gets the PIE Vector Fetch Error Handler Routine Address.
The function indicates the address of the PIE Vector Fetch Error handler routine.
- Return
Error Handler Address.
- Note
Its the responsibility of user to initialize this register. If this register is not initialized, a default error handler at address 0x3fffbe will get executed.
-
uint32_t
SysCtl_isPresentUSBPHY
(void)¶ Check if the Internal PHY is present or not for the USB module
Provides the USB module Internal PHY presence
- Note
This API is applicable only for the CPU1 subsystem.
- Return
true if Internal USB PHY Module is present false if Internal USB PHY Module is not present
-
void
SysCtl_delay
(uint32_t count)¶ Delays for a fixed number of cycles.
This function generates a constant length delay using assembly code. The loop takes 5 cycles per iteration plus 9 cycles of overhead.
- Parameters
count
: is the number of delay loop iterations to perform.
- Note
If count is equal to zero, the loop will underflow and run for a very long time.
- Return
None.
-
uint32_t
SysCtl_getClock
(uint32_t clockInHz)¶ Calculates the system clock frequency (SYSCLK).
This function determines the frequency of the system clock based on the frequency of the oscillator clock source (from
clockInHz) and the PLL and clock divider configuration registers.- Parameters
clockInHz
: is the frequency of the oscillator clock source (OSCCLK).
- Return
Returns the system clock frequency. If a missing clock is detected, the function will return the INTOSC1 frequency. This needs to be corrected and cleared (see SysCtl_resetMCD()) before trying to call this function again.
-
uint32_t
SysCtl_getAuxClock
(uint32_t clockInHz)¶ Calculates the system auxiliary clock frequency (AUXPLLCLK).
This function determines the frequency of the auxiliary clock based on the frequency of the oscillator clock source (from
clockInHz) and the AUXPLL and clock divider configuration registers.- Parameters
clockInHz
: is the frequency of the oscillator clock source (AUXOSCCLK).
- Return
Returns the auxiliary clock frequency.
-
bool
SysCtl_setClock
(uint32_t config)¶ Configures the clocking of the device.
This function configures the clocking of the device. The input crystal frequency, oscillator to be used, use of the PLL, and the system clock divider are all configured with this function.
- Parameters
config
: is the required configuration of the device clocking.
The config parameter is the OR of several different values, many of which are grouped into sets where only one can be chosen.
The system clock divider is chosen with the macro SYSCTL_SYSDIV(x) where x is either 1 or an even value up to 126.
The use of the PLL is chosen with either SYSCTL_PLL_ENABLE or SYSCTL_PLL_DISABLE.
The integer multiplier is chosen SYSCTL_IMULT(x) where x is a value from 1 to 127.
The fractional multiplier is chosen with either SYSCTL_FMULT_0, SYSCTL_FMULT_1_4, SYSCTL_FMULT_1_2, or SYSCTL_FMULT_3_4.
The oscillator source chosen with SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.
This function uses the watchdog as a monitor for the PLL. The user watchdog settings will be modified and restored upon completion. Make sure that the WDOVERRIDE bit isn’t set before calling this function. Re-lock attempt is carried out if either SLIP condition occurs or SYSCLK to input clock ratio is off by 10%.
This function uses the following resources to support PLL initialization:
Watchdog
CPU Timer 1
CPU Timer 2
- Note
See your device errata for more details about locking the PLL.
- Return
Returns false if a missing clock error is detected. This needs to be cleared (see SysCtl_resetMCD()) before trying to call this function again. Otherwise, returns true.
-
void
SysCtl_selectXTAL
(void)¶ Configures the external oscillator for the clocking of the device.
This function configures the external oscillator (XTAL) to be used for the clocking of the device in crystal mode. It follows the procedure to turn on the oscillator, wait for it to power up, and select it as the source of the system clock.
Please note that this function blocks while it waits for the XTAL to power up. If the XTAL does not manage to power up properly, the function will loop for a long time. It is recommended that you modify this function to add an appropriate timeout and error-handling procedure.
- Return
None.
-
void
SysCtl_selectOscSource
(uint32_t oscSource)¶ Selects the oscillator to be used for the clocking of the device.
This function configures the oscillator to be used in the clocking of the device. The
oscSource parameter may take a value of SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.- Parameters
oscSource
: is the oscillator source to be configured.
- See
- Return
None.
-
void
SysCtl_selectOscSourceAuxPLL
(uint32_t oscSource)¶ Selects the oscillator to be used for the AUXPLL.
This function configures the oscillator to be used in the clocking of the AUXPLL. The
oscSource parameter may take a value of SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.- Parameters
oscSource
: is the oscillator source to be configured.
- See
- Return
None.
-
uint32_t
SysCtl_getLowSpeedClock
(uint32_t clockInHz)¶ Calculates the low-speed peripheral clock frequency (LSPCLK).
This function determines the frequency of the low-speed peripheral clock based on the frequency of the oscillator clock source (from
clockInHz) and the PLL and clock divider configuration registers.- Parameters
clockInHz
: is the frequency of the oscillator clock source (OSCCLK).
- Return
Returns the low-speed peripheral clock frequency.
-
uint16_t
SysCtl_getDeviceParametric
(SysCtl_DeviceParametric parametric)¶ Get the device part parametric value
This function gets the device part parametric value.
- Parameters
parametric
: is the requested device parametric value
The parametric parameter can have one the following enumerated values:
SYSCTL_DEVICE_QUAL - Device Qualification Status
SYSCTL_DEVICE_PINCOUNT - Device Pin Count
SYSCTL_DEVICE_INSTASPIN - Device InstaSPIN Feature Set
SYSCTL_DEVICE_FLASH - Device Flash size (KB)
SYSCTL_DEVICE_PARTID - Device Part ID Format Revision
SYSCTL_DEVICE_FAMILY - Device Family
SYSCTL_DEVICE_PARTNO - Device Part Number
SYSCTL_DEVICE_CLASSID - Device Class ID
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Returns the specified parametric value.
-
void
SysCtl_setAuxClock
(uint32_t config)¶ Configures the auxiliary PLL for clocking USB.
This function configures the clock source for auxiliary PLL, the integer multiplier, fractional multiplier and divider.
- Parameters
config
: is the required configuration of the device clocking.
The config parameter is the OR of several different values, many of which are grouped into sets where only one can be chosen.
The system clock divider is chosen with one of the following macros: SYSCTL_AUXPLL_DIV_1, SYSCTL_AUXPLL_DIV_2, SYSCTL_AUXPLL_DIV_4, SYSCTL_AUXPLL_DIV_8
The use of the PLL is chosen with either SYSCTL_AUXPLL_ENABLE or SYSCTL_AUXPLL_DISABLE.
The integer multiplier is chosen with SYSCTL_AUXPLL_IMULT(x) where x is a value from 1 to 127.
The oscillator source chosen with one of SYSCTL_AUXPLL_OSCSRC_OSC2, SYSCTL_AUXPLL_OSCSRC_XTAL, SYSCTL_AUXPLL_OSCSRC_AUXCLKIN,
- Note
This function uses CPU Timer 2 to monitor a successful lock of the AUXPLL. For this function to properly detect the PLL startup SYSCLK >= 2*AUXPLLCLK after the AUXPLL is selected as the clocking source. User configuration of CPU Timer 2 will be backed up and restored.
- Note
See your device errata for more details about locking the PLL.
- Return
None.
-
Many of the functions provided by the SysCtl API are related to device clocking. The most important of these functions is SysCtl_setClock() which will configure which oscillator is to be used, configure the PLL, and configure the system clock divider. SysCtl_getClock() is a complementary function to this one that will, given the frequency of the oscillator source used, read back the configuration of the PLL and clock divider and calculate the system clock frequency. A similar pair of functions is provided for the low-speed peripheral clock, SysCtl_setLowSpeedClock() and SysCtl_getLowSpeedClock().
The ability to enable (turn on the module clock), disable (gate off the module clock), and perform a software reset on most of the peripherals on a device is provided by SysCtl_enablePeripheral(), SysCtl_disablePeripheral(), and SysCtl_resetPeripheral() respectively.
The device’s windowed watchdog is enabled and disabled by SysCtl_enableWatchdog() and SysCtl_disableWatchdog() respectively. The watchdog can be serviced by SysCtl_serviceWatchdog(). Several functions are also provided to configure the watchdog’s clock and windowed functionality.
This section will give further details of these functions and each of the others used for the configuration of SysCtl.
The code for this module is contained in driverlib/sysctl.c, with driverlib/sysctl.h containing the API declarations for use by applications.