Functions | |
void | initEPWM_aux_trip (uint32_t aux_pwm_base, EPWM_DigitalCompareTripInput system_trip_source, uint16_t trip_delay) |
Defines the initialization steps for an auxiliary PWM output. More... | |
void | configEPWMDelayTrip (uint32_t base1, EPWM_DigitalCompareTripInput aux_trip_source) |
Configures the delay trip action for inner switches(PWMxB). More... | |
void initEPWM_aux_trip | ( | uint32_t | aux_pwm_base, |
EPWM_DigitalCompareTripInput | system_trip_source, | ||
uint16_t | trip_delay | ||
) |
Defines the initialization steps for an auxiliary PWM output.
Another EPWMxA will be used as auxiliary trip signal for inner switches, with the dead-band insertion for the auxiliary PWM action at the system trip event.
aux_pwm_base | PWM base register for the auxiliary PWM output |
system_trip_source | Trip input for the system trip event |
trip_delay | Customized delay timing with rising edge delay |
Definition at line 45 of file type4_pwm_protection_source.h.
void configEPWMDelayTrip | ( | uint32_t | base1, |
EPWM_DigitalCompareTripInput | aux_trip_source | ||
) |
Configures the delay trip action for inner switches(PWMxB).
base1 | PWM base register for inner switches |
aux_trip_source | Trip input for the auxiliary PWM output |
Definition at line 129 of file type4_pwm_protection_source.h.