UART2MSP432E4 Object. More...
#include <UART2MSP432E4.h>
Data Fields | |
struct { | |
bool opened:1 | |
UART2_Mode readMode | |
UART2_Mode writeMode | |
UART2_ReadReturnMode readReturnMode:1 | |
bool txEnabled:1 | |
} | state |
HwiP_Handle | hwi |
int32_t | rxStatus |
int32_t | txStatus |
void * | userArg |
UDMAMSP432E4_Handle | udmaHandle |
unsigned char * | readBuf |
size_t | readSize |
uint32_t | nReadTransfers |
size_t | readCount |
size_t | rxSize |
size_t | bytesRead |
SemaphoreP_Handle | readSem |
UART2_Callback | readCallback |
const unsigned char * | writeBuf |
size_t | writeSize |
uint32_t | nWriteTransfers |
size_t | writeCount |
size_t | txSize |
size_t | bytesWritten |
SemaphoreP_Handle | writeSem |
UART2_Callback | writeCallback |
unsigned int | powerMgrId |
UART2MSP432E4 Object.
The application must not access any member variables of this structure!
bool UART2MSP432E4_Object::opened |
UART2_Mode UART2MSP432E4_Object::readMode |
UART2_Mode UART2MSP432E4_Object::writeMode |
UART2_ReadReturnMode UART2MSP432E4_Object::readReturnMode |
bool UART2MSP432E4_Object::txEnabled |
struct { ... } UART2MSP432E4_Object::state |
HwiP_Handle UART2MSP432E4_Object::hwi |
int32_t UART2MSP432E4_Object::rxStatus |
int32_t UART2MSP432E4_Object::txStatus |
void* UART2MSP432E4_Object::userArg |
UDMAMSP432E4_Handle UART2MSP432E4_Object::udmaHandle |
unsigned char* UART2MSP432E4_Object::readBuf |
size_t UART2MSP432E4_Object::readSize |
uint32_t UART2MSP432E4_Object::nReadTransfers |
size_t UART2MSP432E4_Object::readCount |
size_t UART2MSP432E4_Object::rxSize |
size_t UART2MSP432E4_Object::bytesRead |
SemaphoreP_Handle UART2MSP432E4_Object::readSem |
UART2_Callback UART2MSP432E4_Object::readCallback |
const unsigned char* UART2MSP432E4_Object::writeBuf |
size_t UART2MSP432E4_Object::writeSize |
uint32_t UART2MSP432E4_Object::nWriteTransfers |
size_t UART2MSP432E4_Object::writeCount |
size_t UART2MSP432E4_Object::txSize |
size_t UART2MSP432E4_Object::bytesWritten |
SemaphoreP_Handle UART2MSP432E4_Object::writeSem |
UART2_Callback UART2MSP432E4_Object::writeCallback |
unsigned int UART2MSP432E4_Object::powerMgrId |