The definition of a UART2 function table that contains the required set of functions to control a specific UART2 driver implementation. More...
#include <UART2.h>
The definition of a UART2 function table that contains the required set of functions to control a specific UART2 driver implementation.
UART2_CloseFxn UART2_FxnTable::closeFxn |
Function to close the specified peripheral
UART2_OpenFxn UART2_FxnTable::openFxn |
Function to open the specified peripheral
UART2_ReadFxn UART2_FxnTable::readFxn |
Function to read from the specified peripheral
UART2_ReadCancelFxn UART2_FxnTable::readCancelFxn |
Function to cancel a read from the specified peripheral
UART2_WriteFxn UART2_FxnTable::writeFxn |
Function to write from the specified peripheral
UART2_WriteCancelFxn UART2_FxnTable::writeCancelFxn |
Function to cancel a write from the specified peripheral
UART2_FlushRxFxn UART2_FxnTable::flushRxFxn |
Function to flush the RX FIFO