Data Fields
SPIMSP432E4DMA_Object Struct Reference

#include <SPIMSP432E4DMA.h>

Collaboration diagram for SPIMSP432E4DMA_Object:
Collaboration graph
[legend]

Data Fields

HwiP_Handle hwiHandle
 
SemaphoreP_Handle transferComplete
 
SPI_CallbackFxn transferCallbackFxn
 
UDMAMSP432E4_Handle dmaHandle
 
SPI_TransactionheadPtr
 
SPI_TransactiontailPtr
 
size_t framesQueued
 
size_t framesTransferred
 
size_t priTransferSize
 
size_t altTransferSize
 
uint32_t bitRate
 
uint32_t dataSize
 
uint32_t transferTimeout
 
uint32_t activeChannel
 
uint32_t busyBit
 
uint16_t rxScratchBuf
 
SPI_Mode spiMode
 
SPI_TransferMode transferMode
 
uint8_t format
 
bool isOpen
 

Field Documentation

§ hwiHandle

HwiP_Handle SPIMSP432E4DMA_Object::hwiHandle

§ transferComplete

SemaphoreP_Handle SPIMSP432E4DMA_Object::transferComplete

§ transferCallbackFxn

SPI_CallbackFxn SPIMSP432E4DMA_Object::transferCallbackFxn

§ dmaHandle

UDMAMSP432E4_Handle SPIMSP432E4DMA_Object::dmaHandle

§ headPtr

SPI_Transaction* SPIMSP432E4DMA_Object::headPtr

§ tailPtr

SPI_Transaction* SPIMSP432E4DMA_Object::tailPtr

§ framesQueued

size_t SPIMSP432E4DMA_Object::framesQueued

§ framesTransferred

size_t SPIMSP432E4DMA_Object::framesTransferred

§ priTransferSize

size_t SPIMSP432E4DMA_Object::priTransferSize

§ altTransferSize

size_t SPIMSP432E4DMA_Object::altTransferSize

§ bitRate

uint32_t SPIMSP432E4DMA_Object::bitRate

§ dataSize

uint32_t SPIMSP432E4DMA_Object::dataSize

§ transferTimeout

uint32_t SPIMSP432E4DMA_Object::transferTimeout

§ activeChannel

uint32_t SPIMSP432E4DMA_Object::activeChannel

§ busyBit

uint32_t SPIMSP432E4DMA_Object::busyBit

§ rxScratchBuf

uint16_t SPIMSP432E4DMA_Object::rxScratchBuf

§ spiMode

SPI_Mode SPIMSP432E4DMA_Object::spiMode

§ transferMode

SPI_TransferMode SPIMSP432E4DMA_Object::transferMode

§ format

uint8_t SPIMSP432E4DMA_Object::format

§ isOpen

bool SPIMSP432E4DMA_Object::isOpen

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale