Data Fields
SDFatFS_Object Struct Reference

SDFatFS Object The application must not access any member variables of this structure! More...

#include <SDFatFS.h>

Collaboration diagram for SDFatFS_Object:
Collaboration graph
[legend]

Data Fields

uint_fast32_t driveNum
 
DSTATUS diskState
 
FATFS filesystem
 
SD_Handle sdHandle
 

Detailed Description

SDFatFS Object The application must not access any member variables of this structure!

Field Documentation

§ driveNum

uint_fast32_t SDFatFS_Object::driveNum

§ diskState

DSTATUS SDFatFS_Object::diskState

§ filesystem

FATFS SDFatFS_Object::filesystem

§ sdHandle

SD_Handle SDFatFS_Object::sdHandle

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale