Data Fields
PWMMSP432E4_Status Struct Reference

PWMMSP432E4_Status. More...

#include <PWMMSP432E4.h>

Data Fields

uint32_t pwmDuties [(8)]
 
uint32_t genPeriods [(4)]
 
uint8_t prescalar
 
uint8_t activeOutputs
 

Detailed Description

PWMMSP432E4_Status.

The application must not access any member variables of this structure!

Field Documentation

§ pwmDuties

uint32_t PWMMSP432E4_Status::pwmDuties[(8)]

§ genPeriods

uint32_t PWMMSP432E4_Status::genPeriods[(4)]

§ prescalar

uint8_t PWMMSP432E4_Status::prescalar

§ activeOutputs

uint8_t PWMMSP432E4_Status::activeOutputs

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale