Data Fields
Display_Params Struct Reference

Display Parameters. More...

#include <Display.h>

Data Fields

Display_LineClearMode lineClearMode
 

Detailed Description

Display Parameters.

Display parameters are used with the Display_open() call. Default values for these parameters are set using Display_Params_init().

See also
Display_Params_init()

Field Documentation

§ lineClearMode

Display_LineClearMode Display_Params::lineClearMode

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale