MSP432E4 ADCBuf_Params Parameter Extensions. More...
#include <ADCBufMSP432E4.h>
Data Fields | |
ADCBufMSP432E4_SamplingDuration | samplingDuration |
MSP432E4 ADCBuf_Params Parameter Extensions.
To use non-default MSP432E4 specific parameters when calling ADCBuf_open(), a pointer to an instance of this structure must be specified in ADCBuf_Params.custom. Alternatively, these values can be set using the ADCBuf_control() function after calling ADCBuf_open().
ADCBufMSP432E4_SamplingDuration ADCBufMSP432E4_ParamsExtension::samplingDuration |
ADC sampling duration, ADCBufMSP432E4_SamplingDuration