Data Structures | Macros | Typedefs | Variables
UARTMSP432E4.h File Reference

Detailed Description

UART driver implementation for a MSP432E4 UART controller.

============================================================================

The UART header file should be included in an application as follows:

Refer to UART.h for a complete description of APIs & example of use.


#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/devices/msp432e4/inc/msp432.h>
#include <ti/devices/msp432e4/driverlib/gpio.h>
#include <ti/devices/msp432e4/driverlib/pin_map.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/gpio/GPIOMSP432E4.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/utils/RingBuf.h>
Include dependency graph for UARTMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  UARTMSP432E4_FxnSet
 Complement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only. More...
 
struct  UARTMSP432E4_HWAttrs
 UARTMSP432E4 Hardware attributes. More...
 
struct  UARTMSP432E4_Object
 UARTMSP432E4 Object. More...
 

Macros

#define UARTMSP432E4_PIN_UNASSIGNED   0xFFFFFFFF
 Indicates a pin is not being used. More...
 
#define UARTMSP432E4_FLOWCTRL_NONE   0
 No hardware flow control. More...
 
#define UARTMSP432E4_FLOWCTRL_HARDWARE   1
 Hardware flow control. More...
 
#define UARTMSP432E4_PA0_U0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_U0RX)
 PA0 is used for UART0 RX. More...
 
#define UARTMSP432E4_PA1_U0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_U0TX)
 PA1 is used for UART0 RX. More...
 
#define UARTMSP432E4_PH1_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 1, GPIO_PH1_U0CTS)
 PH1 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PM4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTM, 4, GPIO_PM4_U0CTS)
 PM4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PB4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_U0CTS)
 PB4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PE6_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 6, GPIO_PE6_U0CTS)
 PE6 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PG4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_U0CTS)
 PG4 is used for UART0 CTS. More...
 
#define UARTMSP432E4_PH0_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 0, GPIO_PH0_U0RTS)
 PH0 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PB5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_U0RTS)
 PB5 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PE7_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 7, GPIO_PE7_U0RTS)
 PE7 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PG5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_U0RTS)
 PG5 is used for UART0 RTS. More...
 
#define UARTMSP432E4_PB0_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_U1RX)
 PB0 is used for UART1 RX. More...
 
#define UARTMSP432E4_PQ4_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 4, GPIO_PQ4_U1RX)
 PQ4 is used for UART1 RX. More...
 
#define UARTMSP432E4_PR5_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 5, GPIO_PR5_U1RX)
 PR5 is used for UART1 RX. More...
 
#define UARTMSP432E4_PB1_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_U1TX)
 PB1 is used for UART1 TX. More...
 
#define UARTMSP432E4_PQ5_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 5, GPIO_PQ5_U1TX)
 PQ5 is used for UART1 TX. More...
 
#define UARTMSP432E4_PR6_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 6, GPIO_PR6_U1TX)
 PR6 is used for UART1 TX. More...
 
#define UARTMSP432E4_PP3_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 3, GPIO_PP3_U1CTS)
 PP3 is used for UART1 CTS. More...
 
#define UARTMSP432E4_PN1_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 1, GPIO_PN1_U1CTS)
 PN1 is used for UART1 CTS. More...
 
#define UARTMSP432E4_PE0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 0, GPIO_PE0_U1RTS)
 PE0 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PN0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 0, GPIO_PN0_U1RTS)
 PN0 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PN7_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U1RTS)
 PN7 is used for UART1 RTS. More...
 
#define UARTMSP432E4_PA6_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 6, GPIO_PA6_U2RX)
 PA6 is used for UART2 RX. More...
 
#define UARTMSP432E4_PD4_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 4, GPIO_PD4_U2RX)
 PD4 is used for UART2 RX. More...
 
#define UARTMSP432E4_PA7_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 7, GPIO_PA7_U2TX)
 PA7 is used for UART2 TX. More...
 
#define UARTMSP432E4_PD5_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 5, GPIO_PD5_U2TX)
 PD5 is used for UART2 TX. More...
 
#define UARTMSP432E4_PN3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 3, GPIO_PN3_U2CTS)
 PN3 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PD7_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 7, GPIO_PD7_U2CTS)
 PD7 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PJ3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 3, GPIO_PJ3_U2CTS)
 PJ3 is used for UART2 CTS. More...
 
#define UARTMSP432E4_PN2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 2, GPIO_PN2_U2RTS)
 PN2 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PD6_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 6, GPIO_PD6_U2RTS)
 PD6 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PJ2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 2, GPIO_PJ2_U2RTS)
 PJ2 is used for UART2 RTS. More...
 
#define UARTMSP432E4_PA4_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_U3RX)
 PA4 is used for UART3 RX. More...
 
#define UARTMSP432E4_PJ0_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 0, GPIO_PJ0_U3RX)
 PJ0 is used for UART3 RX. More...
 
#define UARTMSP432E4_PA5_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_U3TX)
 PA5 is used for UART3 TX. More...
 
#define UARTMSP432E4_PJ1_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 1, GPIO_PJ1_U3TX)
 PJ1 is used for UART3 TX. More...
 
#define UARTMSP432E4_PP5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 5, GPIO_PP5_U3CTS)
 PP5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PN5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 5, GPIO_PN5_U3CTS)
 PN5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PJ5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 5, GPIO_PJ5_U3CTS)
 PJ5 is used for UART3 CTS. More...
 
#define UARTMSP432E4_PP4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 4, GPIO_PP4_U3RTS)
 PP4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PN4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 4, GPIO_PN4_U3RTS)
 PN4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PJ4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 4, GPIO_PJ4_U3RTS)
 PJ4 is used for UART3 RTS. More...
 
#define UARTMSP432E4_PA2_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_U4RX)
 PA2 is used for UART4 RX. More...
 
#define UARTMSP432E4_PK0_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 0, GPIO_PK0_U4RX)
 PK0 is used for UART4 RX. More...
 
#define UARTMSP432E4_PR1_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 1, GPIO_PR1_U4RX)
 PR1 is used for UART4 RX. More...
 
#define UARTMSP432E4_PA3_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_U4TX)
 PA3 is used for UART4 TX. More...
 
#define UARTMSP432E4_PK1_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 1, GPIO_PK1_U4TX)
 PK1 is used for UART4 TX. More...
 
#define UARTMSP432E4_PR0_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 0, GPIO_PR0_U4TX)
 PR0 is used for UART4 TX. More...
 
#define UARTMSP432E4_PK3_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 3, GPIO_PK3_U4CTS)
 PK3 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PJ7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 7, GPIO_PJ7_U4CTS)
 PJ7 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PN7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U4CTS)
 PN7 is used for UART4 CTS. More...
 
#define UARTMSP432E4_PK2_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 2, GPIO_PK2_U4RTS)
 PK2 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PJ6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 6, GPIO_PJ6_U4RTS)
 PJ6 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PN6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 6, GPIO_PN6_U4RTS)
 PN6 is used for UART4 RTS. More...
 
#define UARTMSP432E4_PC6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 6, GPIO_PC6_U5RX)
 PC6 is used for UART5 RX. More...
 
#define UARTMSP432E4_PH6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U5RX)
 PH6 is used for UART5 RX. More...
 
#define UARTMSP432E4_PC7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 7, GPIO_PC7_U5TX)
 PC7 is used for UART5 TX. More...
 
#define UARTMSP432E4_PH7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U5TX)
 PH7 is used for UART5 TX. More...
 
#define UARTMSP432E4_PP0_U6RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 0, GPIO_PP0_U6RX)
 PP0 is used for UART6 RX. More...
 
#define UARTMSP432E4_PP1_U6TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 1, GPIO_PP1_U6TX)
 PP1 is used for UART6 TX. More...
 
#define UARTMSP432E4_PC4_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 4, GPIO_PC4_U7RX)
 PC4 is used for UART7 RX. More...
 
#define UARTMSP432E4_PH6_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U7RX)
 PH6 is used for UART7 RX. More...
 
#define UARTMSP432E4_PC5_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 5, GPIO_PC5_U7TX)
 PC5 is used for UART7 TX. More...
 
#define UARTMSP432E4_PH7_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U7TX)
 PH7 is used for UART7 TX. More...
 

Typedefs

typedef void(* UARTMSP432E4_ErrorCallback) (UART_Handle handle, uint32_t error)
 The definition of an optional callback function used by the UART driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs. More...
 
typedef struct UARTMSP432E4_ObjectUARTMSP432E4_Handle
 

Variables

const UART_FxnTable UARTMSP432E4_fxnTable
 

Macro Definition Documentation

§ UARTMSP432E4_PIN_UNASSIGNED

#define UARTMSP432E4_PIN_UNASSIGNED   0xFFFFFFFF

Indicates a pin is not being used.

If hardware flow control is not being used, the UART CTS and RTS pins should be set to UARTMSP432E4_PIN_UNASSIGNED.

§ UARTMSP432E4_FLOWCTRL_NONE

#define UARTMSP432E4_FLOWCTRL_NONE   0

No hardware flow control.

§ UARTMSP432E4_FLOWCTRL_HARDWARE

#define UARTMSP432E4_FLOWCTRL_HARDWARE   1

Hardware flow control.

§ UARTMSP432E4_PA0_U0RX

#define UARTMSP432E4_PA0_U0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_U0RX)

PA0 is used for UART0 RX.

§ UARTMSP432E4_PA1_U0TX

#define UARTMSP432E4_PA1_U0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_U0TX)

PA1 is used for UART0 RX.

§ UARTMSP432E4_PH1_U0CTS

#define UARTMSP432E4_PH1_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 1, GPIO_PH1_U0CTS)

PH1 is used for UART0 CTS.

§ UARTMSP432E4_PM4_U0CTS

#define UARTMSP432E4_PM4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTM, 4, GPIO_PM4_U0CTS)

PM4 is used for UART0 CTS.

§ UARTMSP432E4_PB4_U0CTS

#define UARTMSP432E4_PB4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_U0CTS)

PB4 is used for UART0 CTS.

§ UARTMSP432E4_PE6_U0CTS

#define UARTMSP432E4_PE6_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 6, GPIO_PE6_U0CTS)

PE6 is used for UART0 CTS.

§ UARTMSP432E4_PG4_U0CTS

#define UARTMSP432E4_PG4_U0CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_U0CTS)

PG4 is used for UART0 CTS.

§ UARTMSP432E4_PH0_U0RTS

#define UARTMSP432E4_PH0_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 0, GPIO_PH0_U0RTS)

PH0 is used for UART0 RTS.

§ UARTMSP432E4_PB5_U0RTS

#define UARTMSP432E4_PB5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_U0RTS)

PB5 is used for UART0 RTS.

§ UARTMSP432E4_PE7_U0RTS

#define UARTMSP432E4_PE7_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 7, GPIO_PE7_U0RTS)

PE7 is used for UART0 RTS.

§ UARTMSP432E4_PG5_U0RTS

#define UARTMSP432E4_PG5_U0RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_U0RTS)

PG5 is used for UART0 RTS.

§ UARTMSP432E4_PB0_U1RX

#define UARTMSP432E4_PB0_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_U1RX)

PB0 is used for UART1 RX.

§ UARTMSP432E4_PQ4_U1RX

#define UARTMSP432E4_PQ4_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 4, GPIO_PQ4_U1RX)

PQ4 is used for UART1 RX.

§ UARTMSP432E4_PR5_U1RX

#define UARTMSP432E4_PR5_U1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 5, GPIO_PR5_U1RX)

PR5 is used for UART1 RX.

§ UARTMSP432E4_PB1_U1TX

#define UARTMSP432E4_PB1_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_U1TX)

PB1 is used for UART1 TX.

§ UARTMSP432E4_PQ5_U1TX

#define UARTMSP432E4_PQ5_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 5, GPIO_PQ5_U1TX)

PQ5 is used for UART1 TX.

§ UARTMSP432E4_PR6_U1TX

#define UARTMSP432E4_PR6_U1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 6, GPIO_PR6_U1TX)

PR6 is used for UART1 TX.

§ UARTMSP432E4_PP3_U1CTS

#define UARTMSP432E4_PP3_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 3, GPIO_PP3_U1CTS)

PP3 is used for UART1 CTS.

§ UARTMSP432E4_PN1_U1CTS

#define UARTMSP432E4_PN1_U1CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 1, GPIO_PN1_U1CTS)

PN1 is used for UART1 CTS.

§ UARTMSP432E4_PE0_U1RTS

#define UARTMSP432E4_PE0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 0, GPIO_PE0_U1RTS)

PE0 is used for UART1 RTS.

§ UARTMSP432E4_PN0_U1RTS

#define UARTMSP432E4_PN0_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 0, GPIO_PN0_U1RTS)

PN0 is used for UART1 RTS.

§ UARTMSP432E4_PN7_U1RTS

#define UARTMSP432E4_PN7_U1RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U1RTS)

PN7 is used for UART1 RTS.

§ UARTMSP432E4_PA6_U2RX

#define UARTMSP432E4_PA6_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 6, GPIO_PA6_U2RX)

PA6 is used for UART2 RX.

§ UARTMSP432E4_PD4_U2RX

#define UARTMSP432E4_PD4_U2RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 4, GPIO_PD4_U2RX)

PD4 is used for UART2 RX.

§ UARTMSP432E4_PA7_U2TX

#define UARTMSP432E4_PA7_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 7, GPIO_PA7_U2TX)

PA7 is used for UART2 TX.

§ UARTMSP432E4_PD5_U2TX

#define UARTMSP432E4_PD5_U2TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 5, GPIO_PD5_U2TX)

PD5 is used for UART2 TX.

§ UARTMSP432E4_PN3_U2CTS

#define UARTMSP432E4_PN3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 3, GPIO_PN3_U2CTS)

PN3 is used for UART2 CTS.

§ UARTMSP432E4_PD7_U2CTS

#define UARTMSP432E4_PD7_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 7, GPIO_PD7_U2CTS)

PD7 is used for UART2 CTS.

§ UARTMSP432E4_PJ3_U2CTS

#define UARTMSP432E4_PJ3_U2CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 3, GPIO_PJ3_U2CTS)

PJ3 is used for UART2 CTS.

§ UARTMSP432E4_PN2_U2RTS

#define UARTMSP432E4_PN2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 2, GPIO_PN2_U2RTS)

PN2 is used for UART2 RTS.

§ UARTMSP432E4_PD6_U2RTS

#define UARTMSP432E4_PD6_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 6, GPIO_PD6_U2RTS)

PD6 is used for UART2 RTS.

§ UARTMSP432E4_PJ2_U2RTS

#define UARTMSP432E4_PJ2_U2RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 2, GPIO_PJ2_U2RTS)

PJ2 is used for UART2 RTS.

§ UARTMSP432E4_PA4_U3RX

#define UARTMSP432E4_PA4_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_U3RX)

PA4 is used for UART3 RX.

§ UARTMSP432E4_PJ0_U3RX

#define UARTMSP432E4_PJ0_U3RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 0, GPIO_PJ0_U3RX)

PJ0 is used for UART3 RX.

§ UARTMSP432E4_PA5_U3TX

#define UARTMSP432E4_PA5_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_U3TX)

PA5 is used for UART3 TX.

§ UARTMSP432E4_PJ1_U3TX

#define UARTMSP432E4_PJ1_U3TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 1, GPIO_PJ1_U3TX)

PJ1 is used for UART3 TX.

§ UARTMSP432E4_PP5_U3CTS

#define UARTMSP432E4_PP5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 5, GPIO_PP5_U3CTS)

PP5 is used for UART3 CTS.

§ UARTMSP432E4_PN5_U3CTS

#define UARTMSP432E4_PN5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 5, GPIO_PN5_U3CTS)

PN5 is used for UART3 CTS.

§ UARTMSP432E4_PJ5_U3CTS

#define UARTMSP432E4_PJ5_U3CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 5, GPIO_PJ5_U3CTS)

PJ5 is used for UART3 CTS.

§ UARTMSP432E4_PP4_U3RTS

#define UARTMSP432E4_PP4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 4, GPIO_PP4_U3RTS)

PP4 is used for UART3 RTS.

§ UARTMSP432E4_PN4_U3RTS

#define UARTMSP432E4_PN4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 4, GPIO_PN4_U3RTS)

PN4 is used for UART3 RTS.

§ UARTMSP432E4_PJ4_U3RTS

#define UARTMSP432E4_PJ4_U3RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 4, GPIO_PJ4_U3RTS)

PJ4 is used for UART3 RTS.

§ UARTMSP432E4_PA2_U4RX

#define UARTMSP432E4_PA2_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_U4RX)

PA2 is used for UART4 RX.

§ UARTMSP432E4_PK0_U4RX

#define UARTMSP432E4_PK0_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 0, GPIO_PK0_U4RX)

PK0 is used for UART4 RX.

§ UARTMSP432E4_PR1_U4RX

#define UARTMSP432E4_PR1_U4RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 1, GPIO_PR1_U4RX)

PR1 is used for UART4 RX.

§ UARTMSP432E4_PA3_U4TX

#define UARTMSP432E4_PA3_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_U4TX)

PA3 is used for UART4 TX.

§ UARTMSP432E4_PK1_U4TX

#define UARTMSP432E4_PK1_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 1, GPIO_PK1_U4TX)

PK1 is used for UART4 TX.

§ UARTMSP432E4_PR0_U4TX

#define UARTMSP432E4_PR0_U4TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 0, GPIO_PR0_U4TX)

PR0 is used for UART4 TX.

§ UARTMSP432E4_PK3_U4CTS

#define UARTMSP432E4_PK3_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 3, GPIO_PK3_U4CTS)

PK3 is used for UART4 CTS.

§ UARTMSP432E4_PJ7_U4CTS

#define UARTMSP432E4_PJ7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 7, GPIO_PJ7_U4CTS)

PJ7 is used for UART4 CTS.

§ UARTMSP432E4_PN7_U4CTS

#define UARTMSP432E4_PN7_U4CTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 7, GPIO_PN7_U4CTS)

PN7 is used for UART4 CTS.

§ UARTMSP432E4_PK2_U4RTS

#define UARTMSP432E4_PK2_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 2, GPIO_PK2_U4RTS)

PK2 is used for UART4 RTS.

§ UARTMSP432E4_PJ6_U4RTS

#define UARTMSP432E4_PJ6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTJ, 6, GPIO_PJ6_U4RTS)

PJ6 is used for UART4 RTS.

§ UARTMSP432E4_PN6_U4RTS

#define UARTMSP432E4_PN6_U4RTS   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 6, GPIO_PN6_U4RTS)

PN6 is used for UART4 RTS.

§ UARTMSP432E4_PC6_U5RX

#define UARTMSP432E4_PC6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 6, GPIO_PC6_U5RX)

PC6 is used for UART5 RX.

§ UARTMSP432E4_PH6_U5RX

#define UARTMSP432E4_PH6_U5RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U5RX)

PH6 is used for UART5 RX.

§ UARTMSP432E4_PC7_U5TX

#define UARTMSP432E4_PC7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 7, GPIO_PC7_U5TX)

PC7 is used for UART5 TX.

§ UARTMSP432E4_PH7_U5TX

#define UARTMSP432E4_PH7_U5TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U5TX)

PH7 is used for UART5 TX.

§ UARTMSP432E4_PP0_U6RX

#define UARTMSP432E4_PP0_U6RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 0, GPIO_PP0_U6RX)

PP0 is used for UART6 RX.

§ UARTMSP432E4_PP1_U6TX

#define UARTMSP432E4_PP1_U6TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 1, GPIO_PP1_U6TX)

PP1 is used for UART6 TX.

§ UARTMSP432E4_PC4_U7RX

#define UARTMSP432E4_PC4_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 4, GPIO_PC4_U7RX)

PC4 is used for UART7 RX.

§ UARTMSP432E4_PH6_U7RX

#define UARTMSP432E4_PH6_U7RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 6, GPIO_PH6_U7RX)

PH6 is used for UART7 RX.

§ UARTMSP432E4_PC5_U7TX

#define UARTMSP432E4_PC5_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTC, 5, GPIO_PC5_U7TX)

PC5 is used for UART7 TX.

§ UARTMSP432E4_PH7_U7TX

#define UARTMSP432E4_PH7_U7TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTH, 7, GPIO_PH7_U7TX)

PH7 is used for UART7 TX.

Typedef Documentation

§ UARTMSP432E4_ErrorCallback

typedef void(* UARTMSP432E4_ErrorCallback) (UART_Handle handle, uint32_t error)

The definition of an optional callback function used by the UART driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs.

Parameters
UART_HandleUART_Handle
errorThe current value of the receive status register. Please refer to the device data sheet to interpret this value.

§ UARTMSP432E4_Handle

Variable Documentation

§ UARTMSP432E4_fxnTable

const UART_FxnTable UARTMSP432E4_fxnTable
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale