Data Structures | Enumerations | Functions | Variables
TimerMSP432E4.h File Reference

Detailed Description

Timer driver interface for MSP432E4 devices.


Operation

This driver implements half and full width general purpose timers for the MSP432E4 device. For MSP432E4 devices, the system clock is 120 MHz and a 16-bit timer has an 8-bit prescaler. The desired period may not always be achieved due to hardware limitations, such as the aforementioned. The timer resolution is limited to 8.33ns due to the 120 MHz clock. A timer period no greater than 546,133us can be achieved when operating in 16-bit mode. Similarly, a period no greater than 35,791,394us can be achieved when operating in 32-bit mode. The same time constraints apply to the 16-bit timer when attempting to use a frequency less than 5 Hertz. For additional details, refer to the device's technical reference manual.

The timer always operates in count down mode. When using a half width timer, an 8-bit prescaler will be implemented by the driver if necessary. If the timer is operating in Timer_FREE_RUNNING, the timer will count down from the specified period to 0 before restarting.

When using a half width timer, Timer_getCount() will return the value of the counter in bits 15:0 and bits 23:16 will contain the current free-running value of the prescaler. Bits 31:24 are always 0. When using a full width timer, Timer_getCount() will return the the value of the 32-bit timer.

Timer_ONESHOT_CALLBACK is non-blocking. After Timer_start() is called, the calling thread will continue execution. When the timer interrupt is triggered, the specified callback function will be called. The timer will not generate another interrupt unless Timer_start() is called again. Calling Timer_stop() or Timer_close() after Timer_start() but, before the timer interrupt, will prevent the specified callback from ever being invoked.

Timer_ONESHOT_BLOCKING is a blocking call. A semaphore is used to block the calling thead's execution until the timer generates an interrupt. If Timer_stop() is called, the calling thread will become unblocked immediately. The behavior of the timer in this mode is similar to a sleep function.

Timer_CONTINUOUS_CALLBACK is non-blocking. After Timer_start() is called, the calling thread will continue execution. When the timer interrupt is treiggered, the specified callback function will be called. The timer is automatically restarted and will continue to periodically generate interrupts until Timer_stop() is called.

Timer_FREE_RUNNING is non-blocking. After Timer_start() is called, the calling thread will continue execution. The timer will not generate an interrupt in this mode. The timer will count down from the specified period until it reaches 0. The timer will automatically reload the period and start over. The timer will continue running until Timer_stop() is called.

Resource Allocation

Each general purpose timer block contains two timers, Timer A and Timer B, that can be configured to operate independently; or concatenated to operate as one 32-bit timer. This behavior is managed through a set of resource allocation APIs. For example, the TimerMSP432E4_allocateTimerResource API will allocate a timer for exclusive use. Any attempt to allocate this resource in the future will result in a false value being returned from the allocation API. To free a timer resource, the TimerMSP432E4_freeTimerResource is used. The application is not responsible for calling these allocation APIs directly.


#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/Timer.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
Include dependency graph for TimerMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  TimerMSP432E4_HWAttrs
 TimerMSP432E4 Hardware Attributes. More...
 
struct  TimerMSP432E4_Object
 TimerMSP432E4_Object. More...
 

Enumerations

enum  TimerMSP432E4_SubTimer { TimerMSP432E4_timer16A = 0x0001, TimerMSP432E4_timer16B = 0x0002, TimerMSP432E4_timer32 = 0x0003 }
 

Functions

bool TimerMSP432E4_allocateTimerResource (uint32_t baseAddress, TimerMSP432E4_SubTimer subTimer)
 Function to allocate a timer peripheral. More...
 
void TimerMSP432E4_freeTimerResource (uint32_t baseAddress, TimerMSP432E4_SubTimer subTimer)
 Function to de-allocate a timer peripheral. More...
 

Variables

const Timer_FxnTable TimerMSP432E4_fxnTable
 

Enumeration Type Documentation

§ TimerMSP432E4_SubTimer

Enumerator
TimerMSP432E4_timer16A 

Half width timer A

TimerMSP432E4_timer16B 

Half width timer B

TimerMSP432E4_timer32 

Full width timer

Function Documentation

§ TimerMSP432E4_allocateTimerResource()

bool TimerMSP432E4_allocateTimerResource ( uint32_t  baseAddress,
TimerMSP432E4_SubTimer  subTimer 
)

Function to allocate a timer peripheral.

This function is intended to be used by any driver which implements a timer hardware peripheral. Calling this function will enable power to the timer peripheral specified by the parameter, baseAddress.

Parameters
baseAddressThe base address of a timer hardware peripheral.
subTimerThe TimerMSP432E4_subTimer to be allocated.
Returns
A bool returning true if the timer resource was successfully allocated. If the base address is not valid or if the resource is not available, false is returned.
See also
TimerMSP432E4_freeTimerResource()

§ TimerMSP432E4_freeTimerResource()

void TimerMSP432E4_freeTimerResource ( uint32_t  baseAddress,
TimerMSP432E4_SubTimer  subTimer 
)

Function to de-allocate a timer peripheral.

This function is intended to be used by any driver which implements a timer hardware peripheral. Calling this function will disable power to the timer peripheral specified by the parameter, baseAddress, if and only if the timer peripheral is no longer in use.

Precondition
A successful call to TimerMSP432E4_allocateTimerResource() using the baseAddress and subTimer must have been made prior to calling this API.
Parameters
baseAddressThe base address of a timer hardware peripheral.
subTimerThe TimerMSP432E4_subTimer to be freed.
See also
TimerMSP432E4_allocateTimerResource()

Variable Documentation

§ TimerMSP432E4_fxnTable

const Timer_FxnTable TimerMSP432E4_fxnTable
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale