Data Structures | Variables
NVSMSP432E4.h File Reference

Detailed Description

NVS driver implementation for MSP432E4 devices.

============================================================================

This NVS driver implementation is designed to work with FLASH memory on MSP432E4 devices. FLASH memory sectors on these devices are 16 kilobytes in size.

The NVS header file should be included in an application as follows:


#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
Include dependency graph for NVSMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  NVSMSP432E4_HWAttrs
 NVSMSP432E4 attributes. More...
 
struct  NVSMSP432E4_Object
 

Variables

const NVS_FxnTable NVSMSP432E4_fxnTable
 

Variable Documentation

§ NVSMSP432E4_fxnTable

const NVS_FxnTable NVSMSP432E4_fxnTable
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale