AESCCMMSP432E4.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2018-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
108 #ifndef ti_drivers_aesccm_AESCCMMSP432E4__include
109 #define ti_drivers_aesccm_AESCCMMSP432E4__include
110 
111 #include <stdint.h>
112 #include <stdbool.h>
113 
114 #include <ti/drivers/AESCCM.h>
115 
116 #ifdef __cplusplus
117 extern "C" {
118 #endif
119 
126 typedef struct {
127  uint8_t intPriority;
142 
145 /*
146  * AESCCMMSP432E4 context object
147  * The application must not access any member variables of this structure.
148  */
149 typedef struct {
150  bool isOpen;
151  int_fast16_t returnStatus;
152  AESCCM_OperationType operationType;
153  AESCCM_ReturnBehavior returnBehavior;
154  uint32_t accessTimeout;
155  AESCCM_CallbackFxn callbackFxn;
156  AESCCM_Operation *operation;
157 } AESCCMMSP432E4_Object;
158 
161 #ifdef __cplusplus
162 }
163 #endif
164 
165 #endif /* ti_drivers_aesccm_AESCCMMSP432E4__include */
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a me...
Definition: AESCCM.h:463
Hardware-specific configuration attributes.
Definition: AESCCMMSP432E4.h:126
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_Operation *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:537
uint8_t intPriority
Definition: AESCCMMSP432E4.h:127
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:517
AESCCM_ReturnBehavior
The way in which CCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESCCM.h:434
AESCCM driver header.
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale