Network Services API  2.75.00.17
Data Fields
SlNetSock_Winsize_t Struct Reference

The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_Winsize_t:
Collaboration graph

Data Fields

uint32_t winSize
 

Detailed Description

The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option.

Field Documentation

§ winSize

uint32_t SlNetSock_Winsize_t::winSize

receive window size for tcp sockets


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale