Network Services API  2.75.00.17
Data Fields
SlNetSock_SockAddrStorage_t Struct Reference

Generic socket address type to hold either IPv4 or IPv6 address. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_SockAddrStorage_t:
Collaboration graph

Data Fields

uint16_t ss_family
 
uint8_t pad [26]
 

Detailed Description

Generic socket address type to hold either IPv4 or IPv6 address.

Field Documentation

§ ss_family

uint16_t SlNetSock_SockAddrStorage_t::ss_family

§ pad

uint8_t SlNetSock_SockAddrStorage_t::pad[26]

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale