Network Services API  2.75.00.17
Data Fields
SlNetSock_SecAttribNode_t Struct Reference

Secure socket attribute context. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_SecAttribNode_t:
Collaboration graph

Data Fields

SlNetSockSecAttrib_e attribName
 
uint8_t * attribBuff
 
uint16_t attribBuffLen
 
struct SlNetSock_SecAttribNode_tnext
 

Detailed Description

Secure socket attribute context.

Field Documentation

§ attribName

SlNetSockSecAttrib_e SlNetSock_SecAttribNode_t::attribName

Security attribute name

§ attribBuff

uint8_t* SlNetSock_SecAttribNode_t::attribBuff

Security attribute buffer

§ attribBuffLen

uint16_t SlNetSock_SecAttribNode_t::attribBuffLen

Security attribute buffer length

§ next

struct SlNetSock_SecAttribNode_t* SlNetSock_SecAttribNode_t::next

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale