Network Services API  2.75.00.17
Data Fields
SlNetSock_SdSet_t Struct Reference

The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_SdSet_t:
Collaboration graph

Data Fields

uint32_t sdSetBitmap [((32)+(uint8_t) 31)/(uint8_t) 32]
 

Detailed Description

The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function.

< The select socket array manager

Field Documentation

§ sdSetBitmap

uint32_t SlNetSock_SdSet_t::sdSetBitmap[((32)+(uint8_t) 31)/(uint8_t) 32]

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale