Network Services API  2.75.00.17
Data Fields
SlNetSock_SackPermitted_t Struct Reference

The SlNetSock_SackPermitted_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_SackPermitted_t:
Collaboration graph

Data Fields

uint32_t sackPermittedEnabled
 

Detailed Description

The SlNetSock_SackPermitted_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option.

Field Documentation

§ sackPermittedEnabled

uint32_t SlNetSock_SackPermitted_t::sackPermittedEnabled

0 = disabled;1 = enabled; default = 0


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale