Network Services API  2.75.00.17
Data Fields
SlNetSock_Nonblocking_t Struct Reference

The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_Nonblocking_t:
Collaboration graph

Data Fields

uint32_t nonBlockingEnabled
 

Detailed Description

The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option.

Field Documentation

§ nonBlockingEnabled

uint32_t SlNetSock_Nonblocking_t::nonBlockingEnabled

0 = disabled, 1 = enabled, default = 1


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale