Network Services API  2.75.00.17
Data Fields
SlNetSock_NonIpBoundary_t Struct Reference

The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_NonIpBoundary_t:
Collaboration graph

Data Fields

int32_t nonIpBoundaryEnabled
 

Detailed Description

The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option.

Field Documentation

§ nonIpBoundaryEnabled

int32_t SlNetSock_NonIpBoundary_t::nonIpBoundaryEnabled

0 = keep IP boundary; 1 = don`t keep ip boundary; default = 0;


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale