Network Services API  2.75.00.17
Data Fields
SlNetSock_NoPush_t Struct Reference

The SlNetSock_NoPush_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_NoPush_t:
Collaboration graph

Data Fields

uint32_t noPushEnabled
 

Detailed Description

The SlNetSock_NoPush_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option.

Field Documentation

§ noPushEnabled

uint32_t SlNetSock_NoPush_t::noPushEnabled

0 = disabled;1 = enabled; default = 0


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale