Network Services API  2.75.00.17
Data Fields
SlNetSock_MaxSeg_t Struct Reference

The SlNetSock_MaxSeg_t structure is used in SLNETSOCK_TCP_MAXSEG TCP level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_MaxSeg_t:
Collaboration graph

Data Fields

uint32_t maxSeg
 

Detailed Description

The SlNetSock_MaxSeg_t structure is used in SLNETSOCK_TCP_MAXSEG TCP level option.

Field Documentation

§ maxSeg

uint32_t SlNetSock_MaxSeg_t::maxSeg

Maximum TCP segment size. Default = 536


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale