Network Services API  2.75.00.17
Data Fields
SlNetSock_MaxRtt_t Struct Reference

The SlNetSock_MaxRtt_t structure is used in SLNETSOCK_TCP_MAXRTT TCP level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_MaxRtt_t:
Collaboration graph

Data Fields

uint32_t maxRtt
 

Detailed Description

The SlNetSock_MaxRtt_t structure is used in SLNETSOCK_TCP_MAXRTT TCP level option.

Field Documentation

§ maxRtt

uint32_t SlNetSock_MaxRtt_t::maxRtt

Maximum TCP Round Trip Time value allowed; Default = 360000000


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale