Network Services API  2.75.00.17
Data Fields
SlNetSock_Keepalive_t Struct Reference

The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_Keepalive_t:
Collaboration graph

Data Fields

uint32_t keepaliveEnabled
 

Detailed Description

The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option.

Field Documentation

§ keepaliveEnabled

uint32_t SlNetSock_Keepalive_t::keepaliveEnabled

0 = disabled;1 = enabled; default = 1


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale