Network Services API  2.75.00.17
Data Fields
SlNetSock_IpV6Mreq_t Struct Reference

The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP and SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_IpV6Mreq_t:
Collaboration graph

Data Fields

SlNetSock_In6Addr_t ipv6mr_multiaddr
 
uint32_t ipv6mr_interface
 

Detailed Description

The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP and SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option.

Field Documentation

§ ipv6mr_multiaddr

SlNetSock_In6Addr_t SlNetSock_IpV6Mreq_t::ipv6mr_multiaddr

IPv6 multicast address of group

§ ipv6mr_interface

uint32_t SlNetSock_IpV6Mreq_t::ipv6mr_interface

should be 0 to choose the default multicast interface


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale