Network Services API  2.75.00.17
Data Fields
SlNetSock_AddrIn_t Struct Reference

SlNetSock IPv4 address, Internet style. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_AddrIn_t:
Collaboration graph

Data Fields

uint16_t sin_family
 
uint16_t sin_port
 
SlNetSock_InAddr_t sin_addr
 
int8_t sin_zero [8]
 

Detailed Description

SlNetSock IPv4 address, Internet style.

Field Documentation

§ sin_family

uint16_t SlNetSock_AddrIn_t::sin_family

Internet Protocol (AF_INET).

§ sin_port

uint16_t SlNetSock_AddrIn_t::sin_port

Address port (16 bits).

§ sin_addr

SlNetSock_InAddr_t SlNetSock_AddrIn_t::sin_addr

Internet address (32 bits).

§ sin_zero

int8_t SlNetSock_AddrIn_t::sin_zero[8]

Not used.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale