Network Developers Kit API  3.76.00.05
Data Fields
_ci_ipnet Struct Reference

#include <netcfg.h>

Collaboration diagram for _ci_ipnet:
Collaboration graph

Data Fields

uint32_t NetType
 
uint32_t IPAddr
 
uint32_t IPMask
 
void * hBind
 
char Domain [64]
 

Field Documentation

§ NetType

uint32_t _ci_ipnet::NetType

§ IPAddr

uint32_t _ci_ipnet::IPAddr

§ IPMask

uint32_t _ci_ipnet::IPMask

§ hBind

void* _ci_ipnet::hBind

§ Domain

char _ci_ipnet::Domain[64]

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale