Network Services API  2.70.01.02
Data Fields
SlNetSock_AddrIn6_t Struct Reference

SlNetSock IPv6 address, Internet style. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_AddrIn6_t:
Collaboration graph

Data Fields

uint16_t sin6_family
 
uint16_t sin6_port
 
uint32_t sin6_flowinfo
 
SlNetSock_In6Addr_t sin6_addr
 
uint32_t sin6_scope_id
 

Detailed Description

SlNetSock IPv6 address, Internet style.

Field Documentation

§ sin6_family

uint16_t SlNetSock_AddrIn6_t::sin6_family

SLNETSOCK_AF_INET6

§ sin6_port

uint16_t SlNetSock_AddrIn6_t::sin6_port

Transport layer port.

§ sin6_flowinfo

uint32_t SlNetSock_AddrIn6_t::sin6_flowinfo

IPv6 flow information.

§ sin6_addr

SlNetSock_In6Addr_t SlNetSock_AddrIn6_t::sin6_addr

IPv6 address.

§ sin6_scope_id

uint32_t SlNetSock_AddrIn6_t::sin6_scope_id

set of interfaces for a scope.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale